[{"term":"Libraries_BA","id":0,"type":"QUICKLINKS"},{"term":"Instructions","id":1,"type":"QUICKLINKS"},{"term":"WAGO-I/O-PRO","id":2,"type":"QUICKLINKS"},{"term":"Building","id":3,"type":"QUICKLINKS"},{"term":"221","id":4,"type":"QUICKLINKS"}]

Protection Against Corrosion

18 September 2019

The Galvanizer

New methods developed by using hot-dip simulators: The WAGO I/O SYSTEM functions as the central communication system.

Zinc is a particular material that shifts the expiration date of iron far in the future. It safely protects steel from corrosion, so that galvanized components do not rust. This is because zinc and iron form an inseparable elemental compound – the common ferro-zinc alloy. However, this method employs poisonous and potentially explosive gas atmospheres at high temperatures. This consequently demands a process control system that is quite sophisticated to guarantee safety. The task of constantly refining these processes falls to Surtec Research and their hot-dip simulators. The engineers from Falk Steuerungssysteme use the space-saving, easily integrated WAGO 750 I/O SYSTEM in the automation systems for the simulators.

Hot-dip galvanizing is not a new process. The earliest industrial examples extend back into the mid-1800s. However, even after more than 150 years of refinements, improvements to the process still make sense. Due to the increased strength of the steel sheets used in automotive manufacturing, in particular, they are now considerably thinner. Yet the demands placed on the corrosion protection have only increased. “Modern automobile steels are only coated under certain circumstances, due to the variety and characteristics of their alloy components,” explains Björn Beißner, Project Manager at Falk. Safely coping with these challenges on an industrial scale means prior testing of new alloys, gas atmospheres, temperature curves and processes at a laboratory scale. Surtec Research, headquartered in Düsseldorf, builds annealing and hot-dip simulators for this purpose (www.surtec-research.com), and Falk Steuerungssysteme from Stadthagen in Lower Saxony develops and programs the entire automation system. The essential challenge consists in transforming the continuous passage process, found in galvanizing systems, into a dip process, so that the lab results can be transferred into production on a one-to-one basis.

{"container":false,"catalogVersion":"de-wagoContentCatalog/Online","lastExportedVersion":1,"type":"Quote Component","dynamicVisibility":true,"cloneable":true,"uuid":"eyJpdGVtSWQiOiJjb21wXzAwMDA4NjU5IiwiY2F0YWxvZ0lkIjoiZGUtd2Fnb0NvbnRlbnRDYXRhbG9nIiwiY2F0YWxvZ1ZlcnNpb24iOiJPbmxpbmUifQ==","ignoreOnTransfer":false,"uid":"comp_00008659","quote":"Using the WAGO I/O SYSTEM, we can collect all of the data provided by the sensors, switches, and actuators in the system.","modifiedtime":"2025-08-04T01:26:15+0000","children":[],"onlyOneRestrictionMustApply":true,"lastLoad":1754270774980,"visible":true,"wagoColumnComponent":[],"imagePosition":"LEFT","availableLanguages":"AVAILABLE","passepartout":true,"restrictions":[],"searchable":true,"lead":"<p>Björn Beißner, Falk Project Manager</p>","typeCode":"WagoQuoteTeaserComponent","slots":["eyJpdGVtSWQiOiJjc18wMDAwN05KUyIsImNhdGFsb2dJZCI6ImRlLXdhZ29Db250ZW50Q2F0YWxvZyIsImNhdGFsb2dWZXJzaW9uIjoiT25saW5lIn0="],"itemtype":"WagoQuoteTeaserComponent","restricted":false,"name":"quote_bjoern-beißner","synchronizationBlocked":false,"containers":[],"creationtime":"2020-07-21T19:55:31+0000","actions":[],"contentVersion":1,"parents":[]}

WAGO as Central Connection Network

Current pressure and temperature measurements at different areas of the hot-dip simulator represent just one example.

The WAGO I/O SYSTEM functions in the hot-dip simulators as a communication network, it forms both the cornerstone for the entire signal processing system, and also provides functional safety in the ATEX area – all in a very limited space. Falk uses a Siemens Failsafe PLC from the S7-1500 series as the sequence controller for drive control and other purposes, but primarily for the safety technology. A powerful, industrial PC is used as a second control unit to process all of the higher-level functions. These include test procedures and measured value administration with a sampling rate of 10 milliseconds.

The hot-dip simulator consistently functions at high temperatures during the annealing of the metal samples and also during the subsequent immersion (also known as dipping) of the workpiece in the liquid zinc alloy. The annealing phase is decisively important during galvanizing, as a precisely defined oxide coating must be formed on the steel surface.

According to Beißner, “An initial, precise pre-oxidation of the material surface is required for reliable coating.” In addition to temperature and dwell time, the composition of the gases in the hermetically-sealed annealing and coating zone is also extremely important. The use of highly explosive hydrogen or reactive and poisonous carbon monoxide emphasizes the importance of the Ex protection and safety technology incorporated into these systems. It is precisely at this point that Falk Steuerungssysteme relies on the comprehensive tool kit of solutions contained in the WAGO 750 I/O System. Operating errors must be safely avoided, due to to enormous potential risks. Malfunctions or defective components should similarly be prevented from causing accidents in the lab set up. The safety measures involved in the system are so extensive that even the screw connections between the crucible holding the liquid zinc and the induction furnace located above it are protected from unperceived access by an electronically-secured cover.

Safety and Ex as a Functional Unit

“Pressure switches monitor overpressure in the molten metal bath. This way, we ensure that no oxygen penetrates into the system,” explains Project Manager Beißner. “We run the system at a constant overpressure.” It should be obvious from this statement that the safety technology is not limited to the hot-dip simulator. Instead, the failsafe components are installed throughout the hazardous areas, as well. “Demands have risen for our customers in Ex protection – up to a completely intrinsically safe design,” states Beißner.

This is yet another advantage of WAGO technology in comparison to the control systems that Falk used in the past, which relied on the classic disconnect terminal blocks. The combined failsafe Ex i modules from WAGO save enormous amounts of space and are, according to Beißner’s experience, “… more compact than other alternatives. In addition, there is less to wire, which offers real advantages for the carriage-mounted control cabinets.” These control cabinets are subjected to a very strict height limitation. Background: There is a carriage for changing the molten metal baths in the hermetically-sealed crucibles – and they have to fit under the simulator.

{"container":false,"catalogVersion":"de-wagoContentCatalog/Online","lastExportedVersion":1,"type":"Quote Component","dynamicVisibility":true,"cloneable":true,"uuid":"eyJpdGVtSWQiOiJjb21wXzAwMDA4NjVFIiwiY2F0YWxvZ0lkIjoiZGUtd2Fnb0NvbnRlbnRDYXRhbG9nIiwiY2F0YWxvZ1ZlcnNpb24iOiJPbmxpbmUifQ==","ignoreOnTransfer":false,"uid":"comp_0000865E","quote":"... more compact than other alternatives. In addition, there is less to wire, which offers real advantages for the carriage-mounted control cabinets.","modifiedtime":"2025-08-04T01:26:15+0000","children":[],"onlyOneRestrictionMustApply":true,"lastLoad":1754270775554,"visible":true,"wagoColumnComponent":[],"imagePosition":"LEFT","availableLanguages":"AVAILABLE","passepartout":true,"restrictions":[],"searchable":true,"lead":"<p>Björn Beißner, Falk Project Manager</p>","typeCode":"WagoQuoteTeaserComponent","slots":["eyJpdGVtSWQiOiJjc18wMDAwN05KUyIsImNhdGFsb2dJZCI6ImRlLXdhZ29Db250ZW50Q2F0YWxvZyIsImNhdGFsb2dWZXJzaW9uIjoiT25saW5lIn0="],"itemtype":"WagoQuoteTeaserComponent","restricted":false,"name":"quote_beißner","synchronizationBlocked":false,"containers":[],"creationtime":"2020-07-21T19:55:32+0000","actions":[],"contentVersion":1,"parents":[]}

Product Overview

[{"code":"750-663/000-003","name":"Intrinsically safe 4-channel digital input; 24 VDC; PROFIsafe V2.0 iPar","url":"/io-systems/intrinsically-safe-4-channel-digital-input/p/750-663_000-003","description":null,"purchasable":true,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w5ODQzNDd8aW1hZ2UvanBlZ3xhR1U1TDJnMk1pOHhOVEEyT1RFd05ETTBNVEF5TWd8NzFkN2Q5ODgzYzFiM2Q1MmM3NmU2MjE4OTljYzc5MGMwNjE5NDJhOWZhMDlkN2M2YWQ4NTExMTQzMzhiOTE1OQ","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNjY3NjB8aW1hZ2UvanBlZ3xhRE5qTDJneE1TOHhOVEEyT1RFd05UWTFNVGMwTWk4eU1EQXdYekF5TURBd01ERTFNREF3TTJSak5tVXdNREF4TURCaU5sOUVSUzVxY0djfGY3NWNkZDA2OGUzOWE3NWE5NWI1YmEzN2JiZjIwZDMwNWRlZmQ1NGVkZTg2NGQ3OTc5ZDI0ZGEwNzBkYWRlOGI","altText":"2000_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNjY3NjB8aW1hZ2UvanBlZ3xhRE5qTDJneE1TOHhOVEEyT1RFd05UWTFNVGMwTWk4eU1EQXdYekF5TURBd01ERTFNREF3TTJSak5tVXdNREF4TURCaU5sOUVSUzVxY0djfGY3NWNkZDA2OGUzOWE3NWE5NWI1YmEzN2JiZjIwZDMwNWRlZmQ1NGVkZTg2NGQ3OTc5ZDI0ZGEwNzBkYWRlOGI","altText":"2000_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNjY3NjB8aW1hZ2UvanBlZ3xhRE5qTDJneE1TOHhOVEEyT1RFd05UWTFNVGMwTWk4eU1EQXdYekF5TURBd01ERTFNREF3TTJSak5tVXdNREF4TURCaU5sOUVSUzVxY0djfGY3NWNkZDA2OGUzOWE3NWE5NWI1YmEzN2JiZjIwZDMwNWRlZmQ1NGVkZTg2NGQ3OTc5ZDI0ZGEwNzBkYWRlOGI","altText":"2000_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNjY3NjB8aW1hZ2UvanBlZ3xhRE5qTDJneE1TOHhOVEEyT1RFd05UWTFNVGMwTWk4eU1EQXdYekF5TURBd01ERTFNREF3TTJSak5tVXdNREF4TURCaU5sOUVSUzVxY0djfGY3NWNkZDA2OGUzOWE3NWE5NWI1YmEzN2JiZjIwZDMwNWRlZmQ1NGVkZTg2NGQ3OTc5ZDI0ZGEwNzBkYWRlOGI","altText":"2000_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNjY3NjB8aW1hZ2UvanBlZ3xhREJpTDJneFlpOHhOVEEyT1RFd05Ua3hNemc0Tmk4eE5EUXdYekF5TURBd01ERTFNREF3TTJSak5tVXdNREF4TURCaU5sOUVSUzVxY0djfDRkZGNmMTA0MDRhNTNhN2NmMzhlMjEyYTc4NWRiY2Y2ZjRmMjY2NDQyZDY4N2JmNjBkMTFiNTQ4MDZlNWZkOTg","altText":"1440_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNjY3NjB8aW1hZ2UvanBlZ3xhRFEwTDJnM01DOHhOVEEyT1RFd05qTXdOekV3TWk4eE1qZ3dYekF5TURBd01ERTFNREF3TTJSak5tVXdNREF4TURCaU5sOUVSUzVxY0djfDk4MzlhNjg5Yjg1NTc0Zjc4YjEzYWFmZTA1ZDRmNTY3YjE2NWNiNTVhODQ0ODM5ZjVjN2ZhNmUzOTgwNDVhMmU","altText":"1280_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMjI5Mzl8aW1hZ2UvanBlZ3xhR015TDJnM055OHhOVEEyT1RFd05qVTJPVEkwTmk4eE1ESTBYekF5TURBd01ERTFNREF3TTJSak5tVXdNREF4TURCaU5sOUVSUzVxY0djfDFhYTBkNDlmMTNiOTg1ZWJjMDRjNzk4Y2Q3YTdhZjM4ODg0MzNjMTQ3NTdlNzJjYjAyZWI2ODRjOTAzNTg2ODg","altText":"1024_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w4MzA3NHxpbWFnZS9qcGVnfGFEVXlMMmc0TWk4eE5UQTJPVEV3TmpnNU5qa3lOaTgzTmpoZk1ESXdNREF3TVRVd01EQXpaR00yWlRBd01ERXdNR0kyWDBSRkxtcHdad3w0Mzg3YTc1YTUwNDFmN2U5M2NlMjI5NTI0ODU4MmRlZjEyN2EwMmU2MjliZmQyYWQ4NjY3MmI1ZjgyMjgzMzNi","altText":"768_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0Mjg1N3xpbWFnZS9qcGVnfGFHTmxMMmhrTUM4eE5UQTJPVEV3TnpBNU16VXpOQzgwT0RCZk1ESXdNREF3TVRVd01EQXpaR00yWlRBd01ERXdNR0kyWDBSRkxtcHdad3wwYzIzMTg1MWZmNDJjYWUzYmNhODVmMmRjYmNjOTc4OGZiMjlmNzFkMTRhZjYzOTg3N2VlM2FkOGQzODlhNWY4","altText":"480_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTkzfGltYWdlL2pwZWd8YURRMUwyaGtZUzh4TlRBMk9URXdOek15TWpreE1DOHlNREJmTURJd01EQXdNVFV3TURBelpHTTJaVEF3TURFd01HSTJYMFJGTG1wd1p3fDdiNTZiOWQ4MjUzNmU4N2E2ZjJlN2RiY2Q5OWY4YzI1MGY2NWIyMWMxZDRlN2M0Y2YwYzE4NTA3OTU4Y2RmY2Y","altText":"200_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTkzfGltYWdlL2pwZWd8YURRMUwyaGtZUzh4TlRBMk9URXdOek15TWpreE1DOHlNREJmTURJd01EQXdNVFV3TURBelpHTTJaVEF3TURFd01HSTJYMFJGTG1wd1p3fDdiNTZiOWQ4MjUzNmU4N2E2ZjJlN2RiY2Q5OWY4YzI1MGY2NWIyMWMxZDRlN2M0Y2YwYzE4NTA3OTU4Y2RmY2Y","altText":"200_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTkzfGltYWdlL2pwZWd8YURRMUwyaGtZUzh4TlRBMk9URXdOek15TWpreE1DOHlNREJmTURJd01EQXdNVFV3TURBelpHTTJaVEF3TURFd01HSTJYMFJGTG1wd1p3fDdiNTZiOWQ4MjUzNmU4N2E2ZjJlN2RiY2Q5OWY4YzI1MGY2NWIyMWMxZDRlN2M0Y2YwYzE4NTA3OTU4Y2RmY2Y","altText":"200_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_020000150003dc6e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-020000150003dc6e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w1NDY1fGltYWdlL2pwZWd8YUdZekwyaGpNaTh4TlRBMk9URXdPREV3T1RNME1pOHhNakJmTURJd01EQXdNVFV3TURBelpHTTJaVEF3TURFd01HSTJYMFJGTG1wd1p3fGEwMzQwMmI5NWJmNzI0ODVjY2E4NTA3MWI0YjIxY2RiOTJmODdlMDliNWVjM2ZhMzdlNTc1ODc3N2ZlZDAzZTU","altText":"120_020000150003dc6e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_020000150003dc6e000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-663/000-003","stock":null,"url":"/io-systems/intrinsically-safe-4-channel-digital-input/p/750-663_000-003","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["750-663/000-003"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821531432","primaryCategoryName":"I/O Systems","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":false,"status":"RELEASED","cancelDate":null,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["I/O Systems"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"familyCategoryContentPages":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Intrinsically safe 4-channel digital input","primaryImageUrl":null,"productGroup":null,"nameEn":"Intrinsically safe 4-channel digital input; 24 VDC; PROFIsafe V2.0 iPar","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51264981","stockArticle":true,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"showFamily":false,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Digital input","productColor":null,"highlightStatus":null,"downloadData":null,"contentPageData":null,"eventData":null,"pointOfServiceData":null,"faqQuestionData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"jobAdvertisementTileData":null,"productVideos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-667/000-003","name":"Fail-safe 4/4 channel digital input/output; 24 VDC; 2 A; PROFIsafe V2.0 iPar","url":"/io-systems/fail-safe-4-4-channel-digital-input-output/p/750-667_000-003","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3wxMTM1NDc3fGltYWdlL2pwZWd8YURaaEwyZ3pNaTh4TlRBM05EZzFNRGM1T1RZME5nfDNiOThiYTA0ZGMxZjJjZTY4MDRjZDRhNzhjZGI1ZDc2YTEwYjc1YTIyZmRiODgyNjE1OTZkNjcwZjc0ZjQzOTE","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTg5NDd8aW1hZ2UvanBlZ3xhR1JtTDJneU5TOHhOVEEzTkRnMU1USTFPRE01T0M4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMVl6SXdNREF4TURCaU5sOUVSUzVxY0djfGQyOGMxMTI1NDBlOTExY2FkM2EwZjc4YjY3YzNmOGJkMDgyNzg0YmY1NGZlYWRhYWI3ZTRiNjk5YWU1ZWVkMDk","altText":"2000_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTg5NDd8aW1hZ2UvanBlZ3xhR1JtTDJneU5TOHhOVEEzTkRnMU1USTFPRE01T0M4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMVl6SXdNREF4TURCaU5sOUVSUzVxY0djfGQyOGMxMTI1NDBlOTExY2FkM2EwZjc4YjY3YzNmOGJkMDgyNzg0YmY1NGZlYWRhYWI3ZTRiNjk5YWU1ZWVkMDk","altText":"2000_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTg5NDd8aW1hZ2UvanBlZ3xhR1JtTDJneU5TOHhOVEEzTkRnMU1USTFPRE01T0M4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMVl6SXdNREF4TURCaU5sOUVSUzVxY0djfGQyOGMxMTI1NDBlOTExY2FkM2EwZjc4YjY3YzNmOGJkMDgyNzg0YmY1NGZlYWRhYWI3ZTRiNjk5YWU1ZWVkMDk","altText":"2000_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTg5NDd8aW1hZ2UvanBlZ3xhR1JtTDJneU5TOHhOVEEzTkRnMU1USTFPRE01T0M4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMVl6SXdNREF4TURCaU5sOUVSUzVxY0djfGQyOGMxMTI1NDBlOTExY2FkM2EwZjc4YjY3YzNmOGJkMDgyNzg0YmY1NGZlYWRhYWI3ZTRiNjk5YWU1ZWVkMDk","altText":"2000_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTg5NDd8aW1hZ2UvanBlZ3xhR0ZtTDJneVl5OHhOVEEzTkRnMU1UUTFOVEF3Tmk4eE5EUXdYekF5TURBd01EQmxNREF3TXpFMVl6SXdNREF4TURCaU5sOUVSUzVxY0djfGU4ZmY1NTUwYjA4ZTZjNDFhZjY0YjBlZmQ2ZDFjZmY5MDgzNDhhODU0ZDc1NmNhNzUzNzlmNDE5YTBhNjU3ODU","altText":"1440_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTg5NDd8aW1hZ2UvanBlZ3xhRGRtTDJnek15OHhOVEEzTkRnMU1UWTFNVFl4TkM4eE1qZ3dYekF5TURBd01EQmxNREF3TXpFMVl6SXdNREF4TURCaU5sOUVSUzVxY0djfDA5ODk5NWJjY2I4MmU4M2NjNWFmYzkxYWVhNDdjMjg1ODBlMDI4YTM1NzAyODBiYzBhYWUzY2Q0YmU1N2FiMTk","altText":"1280_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDY3MDh8aW1hZ2UvanBlZ3xhR05oTDJnNFlpOHhOVEEzTkRnMU1qRXhNRE0yTmk4eE1ESTBYekF5TURBd01EQmxNREF3TXpFMVl6SXdNREF4TURCaU5sOUVSUzVxY0djfGViMWVhZjFiODQ5YWRhNzAzMTJkYjc1OGQ1YmU2NjBlOTk1MDg3OWI0YTEyMzViYmY3N2UxNjY2NTFkYjE0YjQ","altText":"1024_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5ODMwNHxpbWFnZS9qcGVnfGFEUTJMMmc1Tmk4eE5UQTNORGcxTWpRek9EQTBOaTgzTmpoZk1ESXdNREF3TUdVd01EQXpNVFZqTWpBd01ERXdNR0kyWDBSRkxtcHdad3xlN2JjYWFmOTNiNWRiZGQzZTZlZTUyZjdhNWY0MWNmMDI0ZTQ1NzgzZTdjODg4YTQxMWQ1YzU3NjczNzYzMzhj","altText":"768_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w1MTA1OHxpbWFnZS9qcGVnfGFHUTFMMmhoTUM4eE5UQTNORGcxTWpjMk5UY3lOaTgwT0RCZk1ESXdNREF3TUdVd01EQXpNVFZqTWpBd01ERXdNR0kyWDBSRkxtcHdad3xhYWVjOTkzZWRiMjIzZDg4MzA4YTBhNTM4NWE1ZDc0Nzg2NGVhNzJlYjYyZWZmY2M4NDEyYmUxMDVjZWE3ZTM2","altText":"480_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjI0fGltYWdlL2pwZWd8YURSbUwyaG1NaTh4TlRBM05EZzFNekF5TnpnM01DOHlNREJmTURJd01EQXdNR1V3TURBek1UVmpNakF3TURFd01HSTJYMFJGTG1wd1p3fDlkMTgzZGNiYjViZmRkMTk4ZDU1YTgxYzA0NWNjZmRhNGQ1MmI4MjdjZjY0MjlhMTdkMWE2NDc2MmEyZTI3ODk","altText":"200_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjI0fGltYWdlL2pwZWd8YURSbUwyaG1NaTh4TlRBM05EZzFNekF5TnpnM01DOHlNREJmTURJd01EQXdNR1V3TURBek1UVmpNakF3TURFd01HSTJYMFJGTG1wd1p3fDlkMTgzZGNiYjViZmRkMTk4ZDU1YTgxYzA0NWNjZmRhNGQ1MmI4MjdjZjY0MjlhMTdkMWE2NDc2MmEyZTI3ODk","altText":"200_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjI0fGltYWdlL2pwZWd8YURSbUwyaG1NaTh4TlRBM05EZzFNekF5TnpnM01DOHlNREJmTURJd01EQXdNR1V3TURBek1UVmpNakF3TURFd01HSTJYMFJGTG1wd1p3fDlkMTgzZGNiYjViZmRkMTk4ZDU1YTgxYzA0NWNjZmRhNGQ1MmI4MjdjZjY0MjlhMTdkMWE2NDc2MmEyZTI3ODk","altText":"200_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e000315c2000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000e000315c2000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2MjgyfGltYWdlL2pwZWd8YURrekwyaG1OUzh4TlRBM05EZzFNemMwT0RjMk5pOHhNakJmTURJd01EQXdNR1V3TURBek1UVmpNakF3TURFd01HSTJYMFJGTG1wd1p3fGZkZTkyOGZjZjZlOGIzN2U1YTQ0NmYzYzI2NDJlNWExNGZkZDlhODdmYTQxYzRiOTQ4MGJlNmUzZmY0ZDkwMTI","altText":"120_0200000e000315c2000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000e000315c2000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-667/000-003","stock":null,"url":"/io-systems/fail-safe-4-4-channel-digital-input-output/p/750-667_000-003","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["750-667/000-003"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821038764","primaryCategoryName":"I/O Systems","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":true,"status":"CANCELLED","cancelDate":1688076000000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["I/O Systems"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"familyCategoryContentPages":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Fail-safe 4/4 channel digital input/output","primaryImageUrl":null,"productGroup":null,"nameEn":"Fail-safe 4/4 channel digital input/output; 24 VDC; 2 A; PROFIsafe V2.0 iPar","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51227097","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"showFamily":false,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Digital output","productColor":null,"highlightStatus":null,"downloadData":null,"contentPageData":null,"eventData":null,"pointOfServiceData":null,"faqQuestionData":null,"hideGenerateDatasheetAsPdf":true,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"jobAdvertisementTileData":null,"productVideos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-666/000-003","name":"Fail-safe 4/2 channel digital input/output; 24 VDC; 10 A; PROFIsafe V2.0 iPar","url":"/io-systems/fail-safe-4-2-channel-digital-input-output/p/750-666_000-003","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3wxMTMxNzk2fGltYWdlL2pwZWd8YUdNM0wyaGhNUzh4TlRBM016SXdPVGszTkRneE5BfDNkM2U5OTg4Y2M1OTMyYThmMGZjN2JhM2JhNzI4MmQ0N2I3ZTEwMWEwNGY3Yzc1ZTgxMDAwZjcwYWUzOTI4NGM","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTc5ODN8aW1hZ2UvanBlZ3xhRFUzTDJnMU1TOHhOVEEzTXpJeE1EWXpNREUzTkM4eU1EQXdYekF5TURBd01EQXdNREF3TTJNNE9EZ3dNREF6TURCaU5sOUVSUzVxY0djfGUzNWNkNzAwNWFmMzJkOWJhY2RmZTBlODVlYmRkMjNiNTgyNDFkNTg3NmE1ZDU1YzBmNzgyOWVkYWUwNGRkOWE","altText":"2000_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTc5ODN8aW1hZ2UvanBlZ3xhRFUzTDJnMU1TOHhOVEEzTXpJeE1EWXpNREUzTkM4eU1EQXdYekF5TURBd01EQXdNREF3TTJNNE9EZ3dNREF6TURCaU5sOUVSUzVxY0djfGUzNWNkNzAwNWFmMzJkOWJhY2RmZTBlODVlYmRkMjNiNTgyNDFkNTg3NmE1ZDU1YzBmNzgyOWVkYWUwNGRkOWE","altText":"2000_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTc5ODN8aW1hZ2UvanBlZ3xhRFUzTDJnMU1TOHhOVEEzTXpJeE1EWXpNREUzTkM4eU1EQXdYekF5TURBd01EQXdNREF3TTJNNE9EZ3dNREF6TURCaU5sOUVSUzVxY0djfGUzNWNkNzAwNWFmMzJkOWJhY2RmZTBlODVlYmRkMjNiNTgyNDFkNTg3NmE1ZDU1YzBmNzgyOWVkYWUwNGRkOWE","altText":"2000_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTc5ODN8aW1hZ2UvanBlZ3xhRFUzTDJnMU1TOHhOVEEzTXpJeE1EWXpNREUzTkM4eU1EQXdYekF5TURBd01EQXdNREF3TTJNNE9EZ3dNREF6TURCaU5sOUVSUzVxY0djfGUzNWNkNzAwNWFmMzJkOWJhY2RmZTBlODVlYmRkMjNiNTgyNDFkNTg3NmE1ZDU1YzBmNzgyOWVkYWUwNGRkOWE","altText":"2000_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTc5ODN8aW1hZ2UvanBlZ3xhREF5TDJnMFpTOHhOVEEzTXpJeE1EY3lPRFEzT0M4eE5EUXdYekF5TURBd01EQXdNREF3TTJNNE9EZ3dNREF6TURCaU5sOUVSUzVxY0djfDI2YmYzODdjYWU4NGM0MzUwMDM2MWQ4ODU2NTA5ZTE3NmNlNmIzNDBlODk5M2E1NjUyY2NkZGE0NjExMjYzYjU","altText":"1440_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxOTc5ODN8aW1hZ2UvanBlZ3xhRGN4TDJnME5pOHhOVEEzTXpJeE1EazVNRFl5TWk4eE1qZ3dYekF5TURBd01EQXdNREF3TTJNNE9EZ3dNREF6TURCaU5sOUVSUzVxY0djfDdiZTAzZmExNWFjNTdhNTc3OGYwZWQ0NmVjMzM2MzczM2FmOWFiNWJkOTI3NTYzYWI2MTFlNjJiNDg4ODM0ZmQ","altText":"1280_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDU3MjF8aW1hZ2UvanBlZ3xhRGxsTDJnd1lTOHhOVEEzTXpJeE1USXhPVGs1T0M4eE1ESTBYekF5TURBd01EQXdNREF3TTJNNE9EZ3dNREF6TURCaU5sOUVSUzVxY0djfDY0MWY5Y2NiYWJmZTE0MGMxZjE2ZDA0YjM4NjE0ZTVlMzc4YTJhMzBkOGViMmQzYjMyMmRiNmQxMzllYzJkMDQ","altText":"1024_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5NzgyOXxpbWFnZS9qcGVnfGFHTTFMMmd4TVM4eE5UQTNNekl4TVRRME9UTTNOQzgzTmpoZk1ESXdNREF3TURBd01EQXpZemc0T0RBd01ETXdNR0kyWDBSRkxtcHdad3xmYmNiNzk0NzUyMzJkZWNmZjcyYTJjOWVjYmNmY2YzMjBiMzljNGQzZTExNjZmNDJiMjE0OGQ3NDIzZTQ1ZTEx","altText":"768_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w1MDU5M3xpbWFnZS9qcGVnfGFEazFMMmd4T0M4eE5UQTNNekl4TVRZME5UazRNaTgwT0RCZk1ESXdNREF3TURBd01EQXpZemc0T0RBd01ETXdNR0kyWDBSRkxtcHdad3xkMDI2NmVkNmQ0NTk3ODgyMGVjZGFmYzdiM2E0MDVhYjkxZWNlNTVjZWRkNTBhYWI0MTQyZGNmMzM0MjI4MGFl","altText":"480_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMzfGltYWdlL2pwZWd8YUdaakwyZ3haUzh4TlRBM016SXhNVGd3T1RneU1pOHlNREJmTURJd01EQXdNREF3TURBell6ZzRPREF3TURNd01HSTJYMFJGTG1wd1p3fDRjMzE5NzNmZjUzODA3NzhjZDdmMzcwYjIyNDY2ZWNmYzJiMTMyOTA2ZDY0NzVhYzNhNzE3OGQ2NzQ2ZGVlZDM","altText":"200_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMzfGltYWdlL2pwZWd8YUdaakwyZ3haUzh4TlRBM016SXhNVGd3T1RneU1pOHlNREJmTURJd01EQXdNREF3TURBell6ZzRPREF3TURNd01HSTJYMFJGTG1wd1p3fDRjMzE5NzNmZjUzODA3NzhjZDdmMzcwYjIyNDY2ZWNmYzJiMTMyOTA2ZDY0NzVhYzNhNzE3OGQ2NzQ2ZGVlZDM","altText":"200_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMzfGltYWdlL2pwZWd8YUdaakwyZ3haUzh4TlRBM016SXhNVGd3T1RneU1pOHlNREJmTURJd01EQXdNREF3TURBell6ZzRPREF3TURNd01HSTJYMFJGTG1wd1p3fDRjMzE5NzNmZjUzODA3NzhjZDdmMzcwYjIyNDY2ZWNmYzJiMTMyOTA2ZDY0NzVhYzNhNzE3OGQ2NzQ2ZGVlZDM","altText":"200_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_020000000003c888000300b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-020000000003c888000300b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2MjM2fGltYWdlL2pwZWd8YUdJd0wyZzNOeTh4TlRBM016SXhNak13TVRNME1pOHhNakJmTURJd01EQXdNREF3TURBell6ZzRPREF3TURNd01HSTJYMFJGTG1wd1p3fGQ5OWU0YTllNWVlNTJhOGIzNWE5ZDE4MzczMjcxYzU5NDQxMDYwZDAwMGMwZjA1NjA2NDU1NGJhNzk1MmI5ZWI","altText":"120_020000000003c888000300b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_020000000003c888000300b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-666/000-003","stock":null,"url":"/io-systems/fail-safe-4-2-channel-digital-input-output/p/750-666_000-003","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["750-666/000-003"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821255475","primaryCategoryName":"I/O Systems","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":true,"status":"CANCELLED","cancelDate":1688076000000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["I/O Systems"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"familyCategoryContentPages":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Fail-safe 4/2 channel digital input/output","primaryImageUrl":null,"productGroup":null,"nameEn":"Fail-safe 4/2 channel digital input/output; 24 VDC; 10 A; PROFIsafe V2.0 iPar","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51242294","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"showFamily":false,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Digital output","productColor":null,"highlightStatus":null,"downloadData":null,"contentPageData":null,"eventData":null,"pointOfServiceData":null,"faqQuestionData":null,"hideGenerateDatasheetAsPdf":true,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"jobAdvertisementTileData":null,"productVideos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"753-666/000-003","name":"Fail-safe 4/2 channel digital input/output; 24 VDC; 10 A; PROFIsafe V2.0 iPar","url":"/io-systems/fail-safe-4-2-channel-digital-input-output/p/753-666_000-003","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3wxMTk2OTMzfGltYWdlL2pwZWd8YUdZMUwyZzFaaTh4TlRBNE1UYzNNREU0T0Rnek1BfGIxZDJjNGE4YzE5MDNlYTcyMWE1ZDhmMjUzNTQ0OWM0NmNhMjVkODc1ZTBiZmUyMjE2NTNkYTZjMmI4M2U0N2I","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDgyMTZ8aW1hZ2UvanBlZ3xhR1ZsTDJnMFlpOHhOVEE0TVRjM01EYzBOVGc0Tmk4eU1EQXdYekF5TURBd01EQmlNREF3TURBeU5qUXdNREF5TURCaU5sOUVSUzVxY0djfDIxMjYwMWUyMTFjYzZkNjNiMjY5ZTMwYTMzMzgzMTE1ZjlhYTkzMWJlOWU4OGQzMDYwZDJiYTBjMjhmNmQxZGI","altText":"2000_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDgyMTZ8aW1hZ2UvanBlZ3xhR1ZsTDJnMFlpOHhOVEE0TVRjM01EYzBOVGc0Tmk4eU1EQXdYekF5TURBd01EQmlNREF3TURBeU5qUXdNREF5TURCaU5sOUVSUzVxY0djfDIxMjYwMWUyMTFjYzZkNjNiMjY5ZTMwYTMzMzgzMTE1ZjlhYTkzMWJlOWU4OGQzMDYwZDJiYTBjMjhmNmQxZGI","altText":"2000_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDgyMTZ8aW1hZ2UvanBlZ3xhR1ZsTDJnMFlpOHhOVEE0TVRjM01EYzBOVGc0Tmk4eU1EQXdYekF5TURBd01EQmlNREF3TURBeU5qUXdNREF5TURCaU5sOUVSUzVxY0djfDIxMjYwMWUyMTFjYzZkNjNiMjY5ZTMwYTMzMzgzMTE1ZjlhYTkzMWJlOWU4OGQzMDYwZDJiYTBjMjhmNmQxZGI","altText":"2000_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDgyMTZ8aW1hZ2UvanBlZ3xhR1ZsTDJnMFlpOHhOVEE0TVRjM01EYzBOVGc0Tmk4eU1EQXdYekF5TURBd01EQmlNREF3TURBeU5qUXdNREF5TURCaU5sOUVSUzVxY0djfDIxMjYwMWUyMTFjYzZkNjNiMjY5ZTMwYTMzMzgzMTE1ZjlhYTkzMWJlOWU4OGQzMDYwZDJiYTBjMjhmNmQxZGI","altText":"2000_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDgyMTZ8aW1hZ2UvanBlZ3xhREptTDJnME9DOHhOVEE0TVRjM01EZzNOamsxT0M4eE5EUXdYekF5TURBd01EQmlNREF3TURBeU5qUXdNREF5TURCaU5sOUVSUzVxY0djfGRhODgwNjg2ODhmZDcxNDVhMjMxNTkyNTE1Y2QyMDY2NGUzNWNkNDIyNDY0ODc3MzVlNTJkYjZkMWFiOTE1ODU","altText":"1440_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDgyMTZ8aW1hZ2UvanBlZ3xhRGhpTDJnd05TOHhOVEE0TVRjM01UQXdPREF6TUM4eE1qZ3dYekF5TURBd01EQmlNREF3TURBeU5qUXdNREF5TURCaU5sOUVSUzVxY0djfDExMjI1OTZjZDA0NjgxMzk4NDA5N2JlNGVjNWI0ZWRmMjA5MzdlNGYwMDM2MjQxYTFkZWIzZTM2MDMyOTY2YmU","altText":"1280_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNTM3MTl8aW1hZ2UvanBlZ3xhREZqTDJnd1pDOHhOVEE0TVRjM01USTNNREUzTkM4eE1ESTBYekF5TURBd01EQmlNREF3TURBeU5qUXdNREF5TURCaU5sOUVSUzVxY0djfDQ1MTRlYTEzYjUwNmYwMjQ0NTU4YmNhMmJkZTlkMTJmODk0NDMxNTEwZjAyNTgwYjJkOGM1NmYzZDA4YjBiNzQ","altText":"1024_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMDQyNjJ8aW1hZ2UvanBlZ3xhR1E1TDJneE15OHhOVEE0TVRjM01UUTJOamM0TWk4M05qaGZNREl3TURBd01HSXdNREF3TURJMk5EQXdNREl3TUdJMlgwUkZMbXB3Wnd8ZDIzOThhZTU5YjdmODA4Mzk5ZjM0MmVmOWIyNWY2YTcyYTc5YWE1ZDNkM2E2ZDI0ZDc1NGEwNDQyMWViMzVjZg","altText":"768_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w1NDIxNXxpbWFnZS9qcGVnfGFHRTNMMmd4WkM4eE5UQTRNVGMzTVRjeU9Ea3lOaTgwT0RCZk1ESXdNREF3TUdJd01EQXdNREkyTkRBd01ESXdNR0kyWDBSRkxtcHdad3wyODkyNzcxZTVhYThlMTJjZGNmOWJlMzIzODg2ODkyZGU3M2U1ZTgyYjhmYWIzZmMxNDUyOTI1NzAyMGUyMTgz","altText":"480_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMwfGltYWdlL2pwZWd8YURjNEwyZ3lOQzh4TlRBNE1UYzNNVGt5TlRVek5DOHlNREJmTURJd01EQXdNR0l3TURBd01ESTJOREF3TURJd01HSTJYMFJGTG1wd1p3fDMxNWJkMzIzYTUxODc3YmQ2Y2Q3YzMxNTZkOTlhMWRmYWU5OTQ2YTc1NzNmZWE5OTc2MmE0OWZmNjllNWI0YmI","altText":"200_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMwfGltYWdlL2pwZWd8YURjNEwyZ3lOQzh4TlRBNE1UYzNNVGt5TlRVek5DOHlNREJmTURJd01EQXdNR0l3TURBd01ESTJOREF3TURJd01HSTJYMFJGTG1wd1p3fDMxNWJkMzIzYTUxODc3YmQ2Y2Q3YzMxNTZkOTlhMWRmYWU5OTQ2YTc1NzNmZWE5OTc2MmE0OWZmNjllNWI0YmI","altText":"200_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMwfGltYWdlL2pwZWd8YURjNEwyZ3lOQzh4TlRBNE1UYzNNVGt5TlRVek5DOHlNREJmTURJd01EQXdNR0l3TURBd01ESTJOREF3TURJd01HSTJYMFJGTG1wd1p3fDMxNWJkMzIzYTUxODc3YmQ2Y2Q3YzMxNTZkOTlhMWRmYWU5OTQ2YTc1NzNmZWE5OTc2MmE0OWZmNjllNWI0YmI","altText":"200_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000b00000264000200b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000b00000264000200b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2NDQzfGltYWdlL2pwZWd8YUdVNUwyZzRNeTh4TlRBNE1UYzNNall4TXpZMk1pOHhNakJmTURJd01EQXdNR0l3TURBd01ESTJOREF3TURJd01HSTJYMFJGTG1wd1p3fDkzOWRlOTkwN2Q4MWFmNDMyYjlhOTYyNThjMDdkOTU5ODI3ODUxZDMxYjE4N2JmMDBhZTc5MWUxODBjNzg4OTQ","altText":"120_0200000b00000264000200b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000b00000264000200b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"753-666/000-003","stock":null,"url":"/io-systems/fail-safe-4-2-channel-digital-input-output/p/753-666_000-003","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["753-666/000-003"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821255482","primaryCategoryName":"I/O Systems","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":true,"status":"CANCELLED","cancelDate":1688076000000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["I/O Systems"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"familyCategoryContentPages":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Fail-safe 4/2 channel digital input/output","primaryImageUrl":null,"productGroup":null,"nameEn":"Fail-safe 4/2 channel digital input/output; 24 VDC; 10 A; PROFIsafe V2.0 iPar","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51242295","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"showFamily":false,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Digital output","productColor":null,"highlightStatus":null,"downloadData":null,"contentPageData":null,"eventData":null,"pointOfServiceData":null,"faqQuestionData":null,"hideGenerateDatasheetAsPdf":true,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"jobAdvertisementTileData":null,"productVideos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"753-662/000-003","name":"Fail-safe 8-channel digital input; 24 VDC; PROFIsafe V2.0 iPar","url":"/io-systems/fail-safe-8-channel-digital-input/p/753-662_000-003","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3wxMTk1NTk2fGltYWdlL2pwZWd8YUdGaUwyZ3lZeTh4TlRBNE1qSTBNVGswT1RjeU5nfDUyMjYxNWIwNmZkN2RhOGI1NWFmMzIzZThmZGFhM2IxNDZlOTE5MzI3NjZhYzcwZWRlMTY0M2Q5MDY4OThmZmY","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc5MjJ8aW1hZ2UvanBlZ3xhREkzTDJnNFl5OHhOVEE0TWpJME16RTVORGt4TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJME56Z3dNREF4TURCaU5sOUVSUzVxY0djfGY0MzIwY2FmMzM4NjJiMGNiMjQ0YmJhZmY5YTdiNWFlMzEwMDlhNDYwMWM5NWQ4YWFlZmFmZDFlMjM3ZjY0OTU","altText":"2000_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc5MjJ8aW1hZ2UvanBlZ3xhREkzTDJnNFl5OHhOVEE0TWpJME16RTVORGt4TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJME56Z3dNREF4TURCaU5sOUVSUzVxY0djfGY0MzIwY2FmMzM4NjJiMGNiMjQ0YmJhZmY5YTdiNWFlMzEwMDlhNDYwMWM5NWQ4YWFlZmFmZDFlMjM3ZjY0OTU","altText":"2000_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc5MjJ8aW1hZ2UvanBlZ3xhREkzTDJnNFl5OHhOVEE0TWpJME16RTVORGt4TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJME56Z3dNREF4TURCaU5sOUVSUzVxY0djfGY0MzIwY2FmMzM4NjJiMGNiMjQ0YmJhZmY5YTdiNWFlMzEwMDlhNDYwMWM5NWQ4YWFlZmFmZDFlMjM3ZjY0OTU","altText":"2000_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc5MjJ8aW1hZ2UvanBlZ3xhREkzTDJnNFl5OHhOVEE0TWpJME16RTVORGt4TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJME56Z3dNREF4TURCaU5sOUVSUzVxY0djfGY0MzIwY2FmMzM4NjJiMGNiMjQ0YmJhZmY5YTdiNWFlMzEwMDlhNDYwMWM5NWQ4YWFlZmFmZDFlMjM3ZjY0OTU","altText":"2000_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc5MjJ8aW1hZ2UvanBlZ3xhREEzTDJnNU9TOHhOVEE0TWpJME16VXlNalU1TUM4eE5EUXdYekF5TURBd01EQm1NREF3TVRJME56Z3dNREF4TURCaU5sOUVSUzVxY0djfGZjYzA2NzlkMTg2MDlmZTRhOTk5OGNiOTU0MzJmNjZkMjUxOTkyNjY2MmYxMGU2ZTlkYTBjOGRmNmE1MjBhZDM","altText":"1440_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc5MjJ8aW1hZ2UvanBlZ3xhRGszTDJoaE15OHhOVEE0TWpJME16ZzFNREkzTUM4eE1qZ3dYekF5TURBd01EQm1NREF3TVRJME56Z3dNREF4TURCaU5sOUVSUzVxY0djfDU3MWI3MmE0MWMzMjRlOGI4NTlmNzE5OTY3OGQ0NDFhODFlN2E3YzM3NWM0YzJhNjE2Nzg3NGJiZmE2ZTRiNTU","altText":"1280_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNTM1MTR8aW1hZ2UvanBlZ3xhR1F3TDJobU9DOHhOVEE0TWpJME5ESTBNelE0Tmk4eE1ESTBYekF5TURBd01EQm1NREF3TVRJME56Z3dNREF4TURCaU5sOUVSUzVxY0djfDE1N2Q4YmY5NmQzMGZhY2RlZDJiNDA5ODA5MzA5MGFkZTMyZTdlZTUzYmM3Yzc5YTk4MjdmNTc4ODBmODFiYjU","altText":"1024_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMDQxNzZ8aW1hZ2UvanBlZ3xhREJoTDJobVpDOHhOVEE0TWpJME5EVXpPRE01T0M4M05qaGZNREl3TURBd01HWXdNREF4TWpRM09EQXdNREV3TUdJMlgwUkZMbXB3Wnd8NzU4MGU5YWZjNmI1NDNjZmRmNjliYTIyMjdhOTQ3M2ViODBmY2EyZjY1NDczNjEyZGM5ZTI2Njc5MGJiYmZlZQ","altText":"768_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w1NDIxOXxpbWFnZS9qcGVnfGFHVXpMMmhtTlM4eE5UQTRNakkwTkRjMk56YzNOQzgwT0RCZk1ESXdNREF3TUdZd01EQXhNalEzT0RBd01ERXdNR0kyWDBSRkxtcHdad3wxY2YyMTFjYzg2NDQ5NDM2YjQ3NmMyYjkwMjZiZDBkNDkzOTFhN2Y1NWZkNWUxZGVhMDI1MTNiMzI2OGZjMmI2","altText":"480_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjM4fGltYWdlL2pwZWd8YURFeUwyaGxaaTh4TlRBNE1qSTBORGsyTkRNNE1pOHlNREJmTURJd01EQXdNR1l3TURBeE1qUTNPREF3TURFd01HSTJYMFJGTG1wd1p3fDEzNGMxM2RlZTQ2YjFiYmE2NTljNDRlM2IzOTZjZDAyOTQ3ODM0ZjJmZTY4YjUwNWViZWVmYmY4YjEyZTkxOGI","altText":"200_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjM4fGltYWdlL2pwZWd8YURFeUwyaGxaaTh4TlRBNE1qSTBORGsyTkRNNE1pOHlNREJmTURJd01EQXdNR1l3TURBeE1qUTNPREF3TURFd01HSTJYMFJGTG1wd1p3fDEzNGMxM2RlZTQ2YjFiYmE2NTljNDRlM2IzOTZjZDAyOTQ3ODM0ZjJmZTY4YjUwNWViZWVmYmY4YjEyZTkxOGI","altText":"200_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjM4fGltYWdlL2pwZWd8YURFeUwyaGxaaTh4TlRBNE1qSTBORGsyTkRNNE1pOHlNREJmTURJd01EQXdNR1l3TURBeE1qUTNPREF3TURFd01HSTJYMFJGTG1wd1p3fDEzNGMxM2RlZTQ2YjFiYmE2NTljNDRlM2IzOTZjZDAyOTQ3ODM0ZjJmZTY4YjUwNWViZWVmYmY4YjEyZTkxOGI","altText":"200_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00012478000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000f00012478000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2NDI5fGltYWdlL2pwZWd8YURBNUwyZzVNeTh4TlRBNE1qSTBOVFUxTkRJd05pOHhNakJmTURJd01EQXdNR1l3TURBeE1qUTNPREF3TURFd01HSTJYMFJGTG1wd1p3fDFhYzk2MzU4MDVjMTAzZTA0MjFjY2FiNGQ1NmEzOTNlZWVlNjY0ZWRhZDQ3OGE2OThmMDc4NTBjY2U0NzJkOTg","altText":"120_0200000f00012478000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000f00012478000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"753-662/000-003","stock":null,"url":"/io-systems/fail-safe-8-channel-digital-input/p/753-662_000-003","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["753-662/000-003"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821038788","primaryCategoryName":"I/O Systems","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":true,"status":"CANCELLED","cancelDate":1688076000000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["I/O Systems"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"familyCategoryContentPages":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Fail-safe 8-channel digital input","primaryImageUrl":null,"productGroup":null,"nameEn":"Fail-safe 8-channel digital input; 24 VDC; PROFIsafe V2.0 iPar","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51227099","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"showFamily":false,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Digital input","productColor":null,"highlightStatus":null,"downloadData":null,"contentPageData":null,"eventData":null,"pointOfServiceData":null,"faqQuestionData":null,"hideGenerateDatasheetAsPdf":true,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"jobAdvertisementTileData":null,"productVideos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-665/000-001","name":"Fail-safe 4/4 channel digital input/output; 24 VDC; 0.5 A; PROFIsafe","url":"/io-systems/fail-safe-4-4-channel-digital-input-output/p/750-665_000-001","description":null,"purchasable":true,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3wxMTAxMTk2fGltYWdlL2pwZWd8YUdOaEwyZ3dPQzh4TlRBNE1ERTJOVEkzTnpjeU5nfDM1ZTMwZTU5NWY4YzBhNzhlZGNlYTkxZmM4MmI4N2Y2NDJmZDU5NTRjNDdjZTAwNDZjYjAxY2ZiYjc5MzczOTI","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxODY4MTF8aW1hZ2UvanBlZ3xhRGRoTDJneFl5OHhOVEE0TURFMk5UZ3dNakF4TkM4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMFlUZ3dNREF4TURCaU5sOUVSUzVxY0djfDBlNmQ2NTc2ZjhiZWIzNThiNWU1MGVjOWViNjIwYWE4NjQzMjhlYTA1OGZlODUzNjg4ZjMxNDE4OWVhYjk1YmI","altText":"2000_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxODY4MTF8aW1hZ2UvanBlZ3xhRGRoTDJneFl5OHhOVEE0TURFMk5UZ3dNakF4TkM4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMFlUZ3dNREF4TURCaU5sOUVSUzVxY0djfDBlNmQ2NTc2ZjhiZWIzNThiNWU1MGVjOWViNjIwYWE4NjQzMjhlYTA1OGZlODUzNjg4ZjMxNDE4OWVhYjk1YmI","altText":"2000_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxODY4MTF8aW1hZ2UvanBlZ3xhRGRoTDJneFl5OHhOVEE0TURFMk5UZ3dNakF4TkM4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMFlUZ3dNREF4TURCaU5sOUVSUzVxY0djfDBlNmQ2NTc2ZjhiZWIzNThiNWU1MGVjOWViNjIwYWE4NjQzMjhlYTA1OGZlODUzNjg4ZjMxNDE4OWVhYjk1YmI","altText":"2000_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxODY4MTF8aW1hZ2UvanBlZ3xhRGRoTDJneFl5OHhOVEE0TURFMk5UZ3dNakF4TkM4eU1EQXdYekF5TURBd01EQmxNREF3TXpFMFlUZ3dNREF4TURCaU5sOUVSUzVxY0djfDBlNmQ2NTc2ZjhiZWIzNThiNWU1MGVjOWViNjIwYWE4NjQzMjhlYTA1OGZlODUzNjg4ZjMxNDE4OWVhYjk1YmI","altText":"2000_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxODY4MTF8aW1hZ2UvanBlZ3xhR1UzTDJneU1DOHhOVEE0TURFMk5UazVPRFl5TWk4eE5EUXdYekF5TURBd01EQmxNREF3TXpFMFlUZ3dNREF4TURCaU5sOUVSUzVxY0djfGNkNmNhYWMyNDk2NWEwMTQyNmNiNjk4ZmU1NmE3ZGUxYjNmZGZiMWFjZjc5ODc0ZmU1NTI2ZDZhNjdmYTczNWM","altText":"1440_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxODY4MTF8aW1hZ2UvanBlZ3xhRFkwTDJnMlppOHhOVEE0TURFMk5qRTVOVEl6TUM4eE1qZ3dYekF5TURBd01EQmxNREF3TXpFMFlUZ3dNREF4TURCaU5sOUVSUzVxY0djfGMzNGU5MzExNDUyN2FjZmI0NWIxZmEwODU2MGRhM2Y4NzkwNzhjMTcyNzJlYjdjODI2Y2JlZDMyODQzMmUzMjM","altText":"1280_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzc3ODl8aW1hZ2UvanBlZ3xhRFF5TDJnM1l5OHhOVEE0TURFMk5qVXlNamt4TUM4eE1ESTBYekF5TURBd01EQmxNREF3TXpFMFlUZ3dNREF4TURCaU5sOUVSUzVxY0djfDdiYTM3ZTZmMWVhOWZhOTE3Y2MzNDBmYjg5ZGMxMjg2NjkzYTc0NWMxYzEzYjZlNDAzNTFjMGJkZWRhNWJiZjc","altText":"1024_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5MjQ5OXxpbWFnZS9qcGVnfGFHTXhMMmc0TXk4eE5UQTRNREUyTmpjNE5UQTFOQzgzTmpoZk1ESXdNREF3TUdVd01EQXpNVFJoT0RBd01ERXdNR0kyWDBSRkxtcHdad3wzODVhMGY2MDQ0Mjg5NjlmMTJhNWEwZDMxZmZmMjJkNWQwMTk0YmY5NjcxZDdkYWE1YjcyMGM0Y2E3ODQ1YWY4","altText":"768_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0ODA1NHxpbWFnZS9qcGVnfGFETmlMMmhrTlM4eE5UQTRNREUyTnpBME56RTVPQzgwT0RCZk1ESXdNREF3TUdVd01EQXpNVFJoT0RBd01ERXdNR0kyWDBSRkxtcHdad3w0OTY2N2Q0ZmE5MTJmODc3ZWQxMjc0MWM3NTcyNWU1MDJlZjQ0MWNjZWE3ZjRkN2MwYmZkMWEyZTQzODZlZjMw","altText":"480_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNTAxfGltYWdlL2pwZWd8YUdOaEwyaGtaaTh4TlRBNE1ERTJOek0zTkRnM09DOHlNREJmTURJd01EQXdNR1V3TURBek1UUmhPREF3TURFd01HSTJYMFJGTG1wd1p3fDBlNTQwYjBlODZmOTg3NWNjNGUyOTljNGFkM2UyZWVjNWVkZDUxNzZhM2Q0ZDMxZmQyZmM1NzA4OWQzZGVjNjY","altText":"200_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNTAxfGltYWdlL2pwZWd8YUdOaEwyaGtaaTh4TlRBNE1ERTJOek0zTkRnM09DOHlNREJmTURJd01EQXdNR1V3TURBek1UUmhPREF3TURFd01HSTJYMFJGTG1wd1p3fDBlNTQwYjBlODZmOTg3NWNjNGUyOTljNGFkM2UyZWVjNWVkZDUxNzZhM2Q0ZDMxZmQyZmM1NzA4OWQzZGVjNjY","altText":"200_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNTAxfGltYWdlL2pwZWd8YUdOaEwyaGtaaTh4TlRBNE1ERTJOek0zTkRnM09DOHlNREJmTURJd01EQXdNR1V3TURBek1UUmhPREF3TURFd01HSTJYMFJGTG1wd1p3fDBlNTQwYjBlODZmOTg3NWNjNGUyOTljNGFkM2UyZWVjNWVkZDUxNzZhM2Q0ZDMxZmQyZmM1NzA4OWQzZGVjNjY","altText":"200_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e000314a8000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000e000314a8000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2MDUxfGltYWdlL2pwZWd8YURZNUwyaG1NQzh4TlRBNE1ERTJOemd6TXpZek1DOHhNakJmTURJd01EQXdNR1V3TURBek1UUmhPREF3TURFd01HSTJYMFJGTG1wd1p3fGI2Y2Q1ZTYzNTc1YjQ2YTJlZDFhNGU4NWVmYzJmY2ZiZTQ0MTczMjUzZTAxNmZhNzMzOWRkYTU1ZDRiMjIyZjI","altText":"120_0200000e000314a8000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000e000314a8000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-665/000-001","stock":null,"url":"/io-systems/fail-safe-4-4-channel-digital-input-output/p/750-665_000-001","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["750-665/000-001"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4045454767952","primaryCategoryName":"I/O Systems","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":false,"status":"RELEASED","cancelDate":null,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["I/O Systems"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"familyCategoryContentPages":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Fail-safe 4/4 channel digital input/output","primaryImageUrl":null,"productGroup":null,"nameEn":"Fail-safe 4/4 channel digital input/output; 24 VDC; 0.5 A; PROFIsafe","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51205800","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"showFamily":false,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Digital output","productColor":null,"highlightStatus":null,"downloadData":null,"contentPageData":null,"eventData":null,"pointOfServiceData":null,"faqQuestionData":null,"hideGenerateDatasheetAsPdf":true,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"jobAdvertisementTileData":null,"productVideos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"753-667/000-003","name":"Fail-safe 4/4 channel digital input/output; 24 VDC; 2 A; PROFIsafe V2.0 iPar","url":"/io-systems/fail-safe-4-4-channel-digital-input-output/p/753-667_000-003","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3wxMTk1MDkwfGltYWdlL2pwZWd8YURRMUwyZzNOeTh4TlRBMk56VXlNRGd5TnpReU1nfDgwMzMzNjk5N2I5OGU1ODI0MjE5YWY0ZWQzMzhjMTg4YzRmM2ZjMzk3Mzg0ZDkzNGI3MzVlZDY1NjZlMzE3Mzk","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc3MDh8aW1hZ2UvanBlZ3xhRFEyTDJobE1TOHhOVEEyTnpVeU1UZzBNekl6TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJelpXSXdNREF4TURCaU5sOUVSUzVxY0djfGIzMjUwZTRjNmQxOGE0NGJhNThlZTRiNTVmOWRkYjI5Yjg4MWRjOTBkMjA0MWI3N2U4MDNiNWRhZTFlYTBhZmE","altText":"2000_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc3MDh8aW1hZ2UvanBlZ3xhRFEyTDJobE1TOHhOVEEyTnpVeU1UZzBNekl6TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJelpXSXdNREF4TURCaU5sOUVSUzVxY0djfGIzMjUwZTRjNmQxOGE0NGJhNThlZTRiNTVmOWRkYjI5Yjg4MWRjOTBkMjA0MWI3N2U4MDNiNWRhZTFlYTBhZmE","altText":"2000_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc3MDh8aW1hZ2UvanBlZ3xhRFEyTDJobE1TOHhOVEEyTnpVeU1UZzBNekl6TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJelpXSXdNREF4TURCaU5sOUVSUzVxY0djfGIzMjUwZTRjNmQxOGE0NGJhNThlZTRiNTVmOWRkYjI5Yjg4MWRjOTBkMjA0MWI3N2U4MDNiNWRhZTFlYTBhZmE","altText":"2000_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc3MDh8aW1hZ2UvanBlZ3xhRFEyTDJobE1TOHhOVEEyTnpVeU1UZzBNekl6TUM4eU1EQXdYekF5TURBd01EQm1NREF3TVRJelpXSXdNREF4TURCaU5sOUVSUzVxY0djfGIzMjUwZTRjNmQxOGE0NGJhNThlZTRiNTVmOWRkYjI5Yjg4MWRjOTBkMjA0MWI3N2U4MDNiNWRhZTFlYTBhZmE","altText":"2000_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc3MDh8aW1hZ2UvanBlZ3xhR1UzTDJoalppOHhOVEEyTnpVeU1qQTNNall3Tmk4eE5EUXdYekF5TURBd01EQm1NREF3TVRJelpXSXdNREF4TURCaU5sOUVSUzVxY0djfDBhM2RjYWY4N2Q0MjJjZDU1ZmQyOTI4ZDNlMGQwZDc0NWQ5NGU2MzBiZWM4OWRjMjE1ZjlhYTMyZjg5NWU4NDc","altText":"1440_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMDc3MDh8aW1hZ2UvanBlZ3xhR014TDJoak5TOHhOVEEyTnpVeU1qTTJOelV4T0M4eE1qZ3dYekF5TURBd01EQm1NREF3TVRJelpXSXdNREF4TURCaU5sOUVSUzVxY0djfGE2NzhmYTc0OTRiMjY4YzZmNjBiMzBlOTBiNDQ3YzQ5Nzg3ZTZjNGJiODE1Y2RiNjIwM2RmYTg4OGRjYjZlYzY","altText":"1280_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNTM0MzB8aW1hZ2UvanBlZ3xhR001TDJoaU55OHhOVEEyTnpVeU1qYzVNelV3TWk4eE1ESTBYekF5TURBd01EQm1NREF3TVRJelpXSXdNREF4TURCaU5sOUVSUzVxY0djfDY1NzJjODhlZGE2NjRmZTAyOTZhZmIzMjBmNzk2NjQyNzJiOTk1Nzg4ZWJiMjE3YzczNjViY2UwMTA4OThiNGY","altText":"1024_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMDQxNzJ8aW1hZ2UvanBlZ3xhRE5sTDJnMk15OHhOVEEyTnpVeU16RXlNVEU0TWk4M05qaGZNREl3TURBd01HWXdNREF4TWpObFlqQXdNREV3TUdJMlgwUkZMbXB3Wnd8ODZiNDZlNzczOGY3ZGY2NzZiMDJmZjVlYWQ4NWI2ODhlNTlmNGZjZWMzMzY5N2ZmODNhZTMwZGNjMDY5ZWZmYg","altText":"768_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w1NDIwNnxpbWFnZS9qcGVnfGFEVmhMMmcxTlM4eE5UQTJOelV5TXpVME56RTJOaTgwT0RCZk1ESXdNREF3TUdZd01EQXhNak5sWWpBd01ERXdNR0kyWDBSRkxtcHdad3w2MWQ5OGNkYTJmZWMyYmNiMWMxN2MxY2RkYjk3NDQ1NjBkMzIyYWE3NDMyNWY4ZjEwM2M2MDM0OGMwMWU5Mjg1","altText":"480_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMzfGltYWdlL2pwZWd8YURNekwyZzBaUzh4TlRBMk56VXlNemMzTmpVME1pOHlNREJmTURJd01EQXdNR1l3TURBeE1qTmxZakF3TURFd01HSTJYMFJGTG1wd1p3fDk5MTNiZDEwOThhODgzMGI2YzMwNGQxMGQxNjc2ZDZlZTlkMTY1NmM2OWNiZWM4NzA4MDZmODc4NDIwMjhhZDA","altText":"200_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMzfGltYWdlL2pwZWd8YURNekwyZzBaUzh4TlRBMk56VXlNemMzTmpVME1pOHlNREJmTURJd01EQXdNR1l3TURBeE1qTmxZakF3TURFd01HSTJYMFJGTG1wd1p3fDk5MTNiZDEwOThhODgzMGI2YzMwNGQxMGQxNjc2ZDZlZTlkMTY1NmM2OWNiZWM4NzA4MDZmODc4NDIwMjhhZDA","altText":"200_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjMzfGltYWdlL2pwZWd8YURNekwyZzBaUzh4TlRBMk56VXlNemMzTmpVME1pOHlNREJmTURJd01EQXdNR1l3TURBeE1qTmxZakF3TURFd01HSTJYMFJGTG1wd1p3fDk5MTNiZDEwOThhODgzMGI2YzMwNGQxMGQxNjc2ZDZlZTlkMTY1NmM2OWNiZWM4NzA4MDZmODc4NDIwMjhhZDA","altText":"200_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f000123eb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000f000123eb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2NDMzfGltYWdlL2pwZWd8YUdRMkwyZ3daQzh4TlRBMk56VXlORE0yTmpNMk5pOHhNakJmTURJd01EQXdNR1l3TURBeE1qTmxZakF3TURFd01HSTJYMFJGTG1wd1p3fGM0ZmVkZDJkMmI4YmY1YWI4MzRjMTNlOWMzNjhmY2MyYTMxNDM1MTIxMGJmMDI4ZDQxZjdiZWMyYTY3ZjkzMTU","altText":"120_0200000f000123eb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000f000123eb000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"753-667/000-003","stock":null,"url":"/io-systems/fail-safe-4-4-channel-digital-input-output/p/753-667_000-003","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["753-667/000-003"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821038757","primaryCategoryName":"I/O Systems","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":true,"status":"CANCELLED","cancelDate":1688076000000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["I/O Systems"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"familyCategoryContentPages":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Fail-safe 4/4 channel digital input/output","primaryImageUrl":null,"productGroup":null,"nameEn":"Fail-safe 4/4 channel digital input/output; 24 VDC; 2 A; PROFIsafe V2.0 iPar","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51227095","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"showFamily":false,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Digital output","productColor":null,"highlightStatus":null,"downloadData":null,"contentPageData":null,"eventData":null,"pointOfServiceData":null,"faqQuestionData":null,"hideGenerateDatasheetAsPdf":true,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"jobAdvertisementTileData":null,"productVideos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false}]

WAGO at Work

Customer Applications: Process Engineering

As a partner and innovation leader, WAGO implements many interesting projects. Learn about the creative, efficient solutions we make possible in the process engineering area.

Aircraft Fueling and Automation

Finally failsafe: Thanks to the switch to spring pressure connection technology from WAGO, the aircraft tankers at Brazil’s airports are safer than ever before.

process_referenz_rucker_flughafen_flugzeug_tankewagen_2000x1500.jpg

Automation for Pipelines

Trace heating prevents pipelines from freezing in Siberian temperatures. Explosion-protected components from WAGO play an important role.

process_landschaft_brunnen_schnee_2000x1500.jpg

Absolutely Reliable Quality

The requirements for the technical equipment aboard vessels are extraordinarily stringent. The WAGO I/O-System fulfills all of them.

marine_siem-pride_tatt_oktober_2000x1500.jpg
Your WAGO Contact

Additional service offerings: