Topics
Guidelines and Regulations

WAGO products are developed, tested, produced and marked in accordance with the applicable standards and laws. In addition, they are subjected to numerous inspections and tests in the development process and ongoing production. Below we present some guidelines and regulations so that you, as our customer, will agree:
WAGO meets all standards.

WAGO Information:

  • CE Marking and EC Directives
  • Standards
  • Test Procedures

WAGO Guidelines and Regulations

Statement on CE Marking

WAGO GmbH & Co. KG products are developed, tested and marked in accordance with legally valid international standards and laws. The CE mark is applied to products intended for the European domestic market; with it, manufacturers declare that the marked electrical equipment is in conformity with the applicable requirements set out in the Community harmonization legislation (EU Directives), which allows such equipment to carry this mark. The original intention of this mark was to support the authorities in the EU member states in their market supervision, with the mark acting as a symbol of free movement of products within the EU. According to EC Directive 765/2008, a product can only be given the CE mark if the product requirements are defined in at least one appropriate EU directive. Examples of such directives are the Low Voltage Directive, the EMC Directive, the ATEX Directive, the Building Products Directive and the Machinery Directive. If more than one directive applies to a product, the product must comply with all applicable directives. Only the basic requirements for achieving the defined aim of the directive are laid out in each respective directive. The individual technical details are specified according to the New Approach using lists with cross references to applicable standards (so-called harmonized standards).

1. Low Voltage Directive
The safety of electrical equipment is guaranteed by the Low Voltage Directive (LVD). The LVD covers all electrical equipment operating with a voltage between 50 VAC and 1000 VAC and between 75 VDC and 1500 VDC.
Products falling within the scope of the Low Voltage Directive that are designed in such a way that they can be used in other electrical devices, and whose safety, for the most part, is dependant on how these components were built into the end product and what features the end product has, are defined as basic components in accordance with the Low Voltage Directive.
The LVD doesn’t apply to basic components.
The RoHS Directive also applies to electrical equipment covered by the Low Voltage Directive. This directive regulates the use of hazardous substances in electrical devices and components, with the aim of reducing the quantity of problematic components in electrical waste. Details about the materials used by WAGO are available in our catalogs, on our product packaging and on our Web page.

2. EMC Directive
The EMC Directive stipulates that a product must meet the limits on radiated electromagnetic disturbance and also requires that a product must be immune to electromagnetic interference.
Electromagnetic passive components or components with no direct function, such as terminal blocks, resistors, diodes, capacitors, switching relays and cables (in the form of passive printed circuit boards) are not considered apparatuses within the meaning of the EMC Directive.

3. ATEX Directive on Explosion Protection
The ATEX Directive defines the rules for products (devices and protective systems) intended for use in hazardous locations. A number of products from WAGO are designed for use in hazardous areas.
Based on potential hazards, the ATEX Directive makes a distinction between three different equipment groups, of which Group II and III are subdivided into further zones. Suitability of WAGO products for the different groups and zones is elucidated in the specific product documents (catalogs, Internet site, data sheets and product inserts).
These may be either devices that can be used as equipment in these types of areas, or components that are required for safe operation, but which do not fulfill a dedicated function. Such components include rail-mount terminal blocks for use in hazardous areas.
Products in both groups must comply with the ATEX Directive.

4. Radio Communications Directive
The Radio Communications Directive applies to all devices that properly transmit or receive radio waves for wireless communications and/or radio orientation. The basic safety requirements apply to the protection of health for humans and animals and to electrical safety in line with the Low Voltage Directive, but without the application of the voltage limit. In addition, the EMC protection goals of the EMC Directive must also be fulfilled and efficient use of radio frequencies ensured. WAGO products covered by the Radio Communications Directive indicate, in compliance with applicable laws, only the Radio Communication Directive in their EU Declaration of Conformity, as fulfillment of the Low Voltage Directive and of the EMC Directive is implicit in this declaration.

5. Construction Products Regulation
The Construction Products Regulation demands that structures be designed and constructed such that the safety of humans, property and animals is not endangered and that all applicable environmental protection requirements be taken into account. Here, building products are defined as products or construction sets which are produced to be built permanently into structures and which make a significant contribution to fulfilling the basic requirements for the structure.
In the unanimous opinion expressed by the German electrical industry, and also by WAGO GmbH & Co. KG, products used in general installation technology are not included among these types of building products and are therefore not covered by this directive.

6. Machinery Directive
The Machinery Directive applies to machines (complete or incomplete) which perform their functions by means other than direct human or animal work, or safety components for these types of machines.
Therefore, this directive usually does not apply to WAGO products.
The manufacturers of machines or systems are required by this directive to use safe products and components in their machines and systems. Directive-compliant production and safe operation is facilitated by the use of WAGO products, with their standard-compliant, up-to-date design.

Significance of CE Mark for WAGO Products
One, several or none of the EU Directives may apply to the various WAGO products. If none of the directives apply, the CE marking will not be affixed to the product, in line with applicable laws. Furthermore, a declaration of conformity must not be issued. All other products are provided with the CE mark – either directly on the product, on its packaging or in the documents included with the product – and a declaration of conformity is issued, or made accessible to the customer.
The data sheets of the technically sound products that, according to the regulations, are not CE marked will refer to the standards used in the development and type and manufacturing testing wherever possible.

IEC/EN Standards

You can find additional information on the standards that apply to WAGO products in the following PDF file:

Tests and Testing Procedures per IEC/EN Standards

There are specific test specifications for each of our products, from connectors to rail-mount terminal blocks.

The following sections describe the most important tests and are limited to a description of the test procedures and an explanation of the test purpose.

Mechanical Tests
WAGO products are developed and produced to withstand the mechanical loads that arise in the application without suffering damage. This is demonstrated on the one hand by the tests according to following tests, some of which are required by standards:

  • Connectability of all conductors indicated in the data sheet
  • Pull-out test of the connected conductors (per IEC/EN 60947-7-1, IEC/EN 60998-2-2, IEC/EN 60999-1)
  • Shock test per IEC/EN 60068-2-27, 60068-2-30; IEC/EN 61373 (railway applications)
  • Vibration test (per IEC/EN 60068-2-6; DNV GL (marine applications); LR; EN 61373 (railway applications))

Electrical Tests
WAGO products meet requirements for the following electrical tests:

  • Temperature-rise test per IEC/EN 60947-7-1, IEC/EN 60947-7-4, IEC/EN 61984
  • Current-carrying capacity curve (derating curve) per IEC/EN 60512-5-2
  • Voltage drop test per IEC/EN 60947-7-1, IEC/EN 60999-1
  • Short-time withstand current test (short-circuit withstand capacity) per IEC/EN 60947-7-1, IEC/EN 60947-7-4
  • Insulation parameters per IEC/EN 60664-1
  • Power-frequency withstand voltage test per IEC/EN 60998-1, IEC/EN 60947-7-1, IEC/EN 60947-7-4
  • Rated impulse withstand voltage test per IEC/EN 60664-1, IEC/EN 60947-7-1
  • IP ratings for electrical equipment per IEC/EN 60529


Material Tests
WAGO products meet the requirements of the following material tests:

  • Needle flame test per IEC/EN 60947-7-1, IEC/EN 60695-11-5
  • Glow-wire test per IEC/EN 60998-1, IEC/EN 60695-2-11


Environmental Tests
The following tests show how a product reacts when exposed to an aggressive environment. Climatic chambers simulate standard atmospheres that could impact long-term constancy of clamping units. All WAGO products meet the requirements of the following environmental tests:

  • Temperature cycling test per IEC/EN 60947-7-1, IEC/EN 60998-2-2
  • Industrial atmospheres per EN ISO 6988, IEC 60068-2-42, IEC/EN 60068-2-60
  • Salt spray test per IEC/EN 60068-2-11; DNV GL (marine applications); LR
  • Quick change of temperature per IEC/EN 60068-2-14
  • Damp heat, cyclic (12 + 12 Hour Cycle) per IEC/EN 60068-2-30, DNV GL, LR (marine applications)

Know What’s Inside and What Needs to Be Done

We will be happy to tell you about the materials we use for our products and everything you need to consider in order to connect solid aluminum conductors to our spring clamps.

Certificates and Approvals

Constructed, tested, approved: WAGO’s products are certified for use in a great variety of industries and sectors worldwide. And all of the certificates are available for download.

kundenservice_zertifikate_zulassungen_gettyimages-533837347_2000x2000.jpg

Catalogs

Download our catalogs so you have an overview of everything, even without an Internet connection, and can readily access important information at any time.

WAGO6369_23-elektronische-kataloge_2000x1500.jpg