Customer application 21 May 2021
New Brilliance for the Stadiums of Tomorrow

Following general renovations started in August 2020, the Helsinki Olympic Stadium now gleams with new light – literally. The SIRIUS® floodlight fixtures from SITECO, a lighting manufacturer, are responsible for this change. The company from Traunreut in Upper Bavaria, which is known for its tradition of quality, has set a new standard with these floodlights, now in use in stadiums around the world. SITECO integrates quality holistically. Because of this, the company relies on high-grade lighting connection technology from WAGO, which can be easily and intuitively operated due to the levers.

The SIRIUS® floodlight fixtures from SITECO will clearly spotlight future major events at the Helsinki Olympic Stadium – both for the 36,000 spectators in the stadium and the millions watching on their TVs. The especially precise lighting control is achieved through high-efficiency silver reflectors. Specialized Cut-Off variants trim superfluous light scatter and, at 96 points on the “Television Lighting Consistency Index” (TLCI), focus it precisely where it is needed – down into the arena, instead of up at the night sky.

WAGO PCB terminal blocks with levers provide:

  • Comfortable and secure connection in the field without tools – thanks to WAGO’s lever technology

  • High current carrying capacity in a compact construction, as well as flexible design-in potentials

  • Reliable, high-quality spring connection technology for numerous conductor cross sections – available worldwide

Connecting Function, Lighting Quality and Efficiency

“The SIRIUS® floodlight fixture exceeds the requirements of the large governing bodies in sports, like FIFA and UEFA in soccer/football or IAAF in Track and Field. It offers excellent lighting quality at low current consumption, and also commands DMX controlled, dynamic light scenes,” states Michaela Plank, Product Manager at SITECO. In the times of Ultra HD and 8K, SIRUIS® offers an ideal foundation for exciting moments in sports that includes flicker-free lighting for super slow motion viewing. This is also confirmed by Tero Männikkö, Project Manager for the city of Helsinki, “The main benefits of the new lighting solution are improved light output, lighting quality and energy efficiency.”

MM-8686  new website page PCB Terminal Block 2604 series_sirius_siteco_2_2000x1125.jpg

In the times of Ultra HD and 8K, SIRIUS® offers an ideal foundation for exciting moments in sports that includes flicker-free lighting for super slow motion viewing.

Photo: SITECO

Consistent quality – Inside and Outside

The one is quality that you can see. The second important factor in quality is somewhat hidden, deep inside the SIRIUS® power supply unit. In order for the spotlights to flood arenas, like the Helsinki Olympic Stadium, with light, they must have supply units. “It forms the core of the floodlight. It generates 2000 watts of LED output and distributes it on the light sail, as per customer request,” explains Mathias Loipfinger, electronics designer at SITECO. This makes the use of high-quality, reliable connection technology even more important, specifically maintenance-free and vibration-proof. “WAGO offers this, and over the entire lifespan of the LED floodlight.” The Wire-to-Board connectors of the 2604 Series, which are installed in the floodlights, function for the mains-side connection at the customer’s location and also to terminate installation cables during remote assembly of the supply unit.

The power supply unit forms the core of each SIRIUS® floodlight fixture. WAGO PCB terminal blocks from the 2604 Series, concealed within this core, ensure reliable connection technology.

Photo: SITECO

» Wire-to-Board connectors of the 2604 Series function for the mains-side connection at the customer’s location and also to terminate installation cables during remote assembly of the supply unit. «

Easy handling, short installation times, due to the levers

The terminal blocks have to be both mechanically robust and stable, and also provide fast conductor termination, without tools, independent of operator skill. The solution is found in the lever technology developed by WAGO. This offers a clear connection for all kinds of connectors, both with and without ferrules, from large cross-sections to the smallest, with different pole numbers, and which is so self-explanatory that it is understood worldwide.

“The lever functionality allows for fast and simple connections for SIRIUS®,” says Mathias Loipfinger. “Because tools are not needed for the connections, customers also see several benefits during installation: it is faster and significantly more comfortable.” In addition, this connection technology satisfies common standards for lighting manufacturers and also for electricians. Furthermore, SITECO has found WAGO to be a reliable partner, with whom they have collaborated for many years in the search for professional lighting solutions. “Three selection criteria count here: quality, price and performance,” concludes Loipfinger.

The Wire-to-Board connectors of the 2604 Series, which are installed in the supply units, function for the mains-side connection at the customer’s location. The straightforward lever connection technology, which requires no tools, also offers time savings and a high degree of comfort for customers during installation.

Photo: WAGO

» Because tools are not needed for the connections, customers also see several benefits during installation: it is faster and significantly more comfortable. «

Mathias Loipfinger, electronics developer at SITECO

Balancing Act between Historical Inheritance and Current Technical Demands

International sporting events, concerts and other events: Michael Jackson, the Rolling Stones, and Tina Turner have performed in the Helsinki Olympic Stadium. It hosted the summer Olympic games in 1952, world championship track and field events in 1971 and 1994, the Women's World Cup in 2009, and the European championships for track and field in 2012. The UEFA Super Cup will be played here in 2022. The past and the future both lay claim to the Olympic Stadium in Helsinki, which makes it something truly special.

Constructed from 1934 to 1938 in the Finnish Functionalistic style and operated by the Stadion-säätiö support society, it was listed as a historic monument in 2006. The latter complicated conditions for the ninth and largest renovation in its history, a complete refurbishment that began in 2016. The lighting, using SIRIUS® floodlight fixtures from SITECO, which in turn employ WAGO connection technology, is an important part of these renovations, and represents, like the Helsinki Olympic Stadium itself, outstanding quality features for the brilliance of the stadiums of tomorrow.

International sporting events, concerts and other events: constructed in 1938 and renovated in 2020, the Helsinki Olympic Stadium will host the UEFA Super Cup in 2022 – perfectly illuminated for more than 36,000 spectators in the stadium and millions watching on TV.

Photo: SITECO

» WAGO offers reliable high-quality connection technology, and over the entire lifespan of the LED floodlight. «

Mathias Loipfinger, electronics developer at SITECO

Product Recommendations

This May Also Interest You

Compatible Products

Get Connected Reliably with WAGO's PCB Terminal Blocks and Pluggable Connectors

buehne_leiterplattenanschluss_ad_2000x2000.jpg

PCB Terminal Blocks and Pluggable Connectors with Lever