[{"term":"Libraries_BA","id":0,"type":"QUICKLINKS"},{"term":"Instructions","id":1,"type":"QUICKLINKS"},{"term":"WAGO-I/O-PRO","id":2,"type":"QUICKLINKS"},{"term":"Building","id":3,"type":"QUICKLINKS"},{"term":"221","id":4,"type":"QUICKLINKS"}]
[{"url":"/products","name":"Products","linkClass":null,"categoryCode":null},{"url":"/interface-electronics","name":"Interface Electronics","linkClass":null,"categoryCode":null},{"url":"/interface-electronics/discover-relays-optocouplers","name":"Relay Modules/Optocoupler Modules","linkClass":null,"categoryCode":null},{"url":"/interface-electronics/discover-relays-optocouplers/customer-application-adls-deutsche-windtechnik","name":"Customer Application ","linkClass":"active","categoryCode":null}]
Customer application 20 October 2022

On-Demand Night-Time Marking (ADLS) for Wind Turbines with Deutsche Windtechnik Control and WAGO

To reduce light pollution in the night sky, wind turbines in Germany will soon only illuminate when approached by aircraft. Deutsche Windtechnik Steuerung offers a solution for this “on-demand night-time marking (ADLS)” with a transponder-based ADLS system. The WAGO Relay, Item No. 857-304 is also used in this project.

Deutsche Windtechnik Steuerung, headquartered in Husum-Ostenfeld, has taken the leadership in wind farm maintenance. The company has maintenance contracts in Germany for around 2,400 turbines, with more worldwide. In addition to standard maintenance of land-based and offshore wind turbines, the team from Deutschen Windtechnik Steuerung conducts research into developing and expanding their services. In 2018, when a draft law for on-demand night-time marking (ADLS) of wind turbines was proposed, Deutschen Windtechnik Steuerung’s technicians and engineers began developing a solution to switch on the red flashing lights at the top of wind turbines, but only when they were needed. At that time, no finished industrial product could satisfy the legislators’ lofty safety requirements.

Merely switching the lights off is simply not a solution here, as the lights fulfill a necessary safety function: they warn any approaching aircraft about the wind turbines. Therefore, the solution must monitor the air space and emit a signal that allows the night-time marking to illuminate as soon as helicopters, airplanes, etc., approach within a radius of four kilometers. Wind turbine operators must legally implement ADLS on land by 31 December 2022 and at sea by 31 December 2023. The law applies to wind turbines starting at a height of 100 meters, meaning that most wind turbines in Germany are affected.

Deutsche Windtechnik Steuerung Relies on WAGO

There are currently a mere handful of solutions to implement ADLS. Three vendors rely on WAGO – Deutsche Windtechnik Steuerung is among them. They have developed a so-called ADLS Box that operators can retrofit on their wind turbines.

“During the development of our ADLS Box, we had to overcome several obstacles. It wasn’t a sure-fire success,” recalls Karl Keusgen, CEO at Deutschen Windtechnik Steuerung. “ADLS represents an intervention in air traffic safety. We had to provide a lot of supporting evidence. This included, for example, that the lights must illuminate within a specific time – something that had to be guaranteed. Another obstacle was the variety of wind energy systems as well as geographic challenges, like mountains and valleys,” continues Keusgen.

The solution from Deutschen Windtechnik Steuerung provides an independent, transponder-based system that can be integrated into existing wind farms. There are three different configuration levels. The complete solution equips the entire wind farm. A transponder receiver functions as the master box, which is centrally located in the wind farm and operated by Deutschen Windtechnik Steuerung. Each individual wind turbine receives an ADSL Box – a slave box that can control the night-time marking system. That box is installed in the turbine’s nacelle.


Starting in January 2023, wind turbines are legally obligated to feature a system for on-demand night-time marking in order to reduce light pollution.

Photo: Udo Hallstein/vor-ort-foto.de

Independent ADLS System

Communication between the boxes occurs via a local, proprietary wireless solution, developed by Deutsche Windtechnik Steuerung, which functions independently from other infrastructure, the wind farm boundaries and the system technology. A transponder receiver module monitors the air space and generates switching signals for illuminating the wind turbine. It detects aircraft within a distance of ten kilometers at an altitude of 600 meters or less. If aircraft comes within a radius of four kilometers around the wind farm, the module transmits a signal to the wind turbines, causing the marking lights to illuminate and flash red. Sixty-three slave boxes can be installed per transponder.

The transponder receiver transmits a signal to the ADLS Boxes every five milliseconds. If the boxes don’t receive any signal for 20 milliseconds, then the night-time marking lights turn on automatically for safety reasons. The same thing occurs if a fault occurs in the transponder box. In this case, the marking lights on all wind turbines connected to the transponder box will illuminate. If there is a fault in the ADLS Box, only the affected wind turbine lights up. The lights are, therefore, only switched off if everything is functioning perfectly and no aircraft is approaching.

{"container":false,"catalogVersion":"sg-wagoContentCatalog/Online","lastExportedVersion":3,"type":"Quote Component","dynamicVisibility":true,"cloneable":true,"uuid":"eyJpdGVtSWQiOiJjb21wX2RlXzAwMDBGVjFCIiwiY2F0YWxvZ0lkIjoic2ctd2Fnb0NvbnRlbnRDYXRhbG9nIiwiY2F0YWxvZ1ZlcnNpb24iOiJPbmxpbmUifQ==","ignoreOnTransfer":false,"uid":"comp_de_0000FV1B","quote":"The design appealed to us. Due to the clamping system, mounting is easy and fast, saving time and reducing costs. We are completely satisfied with the relay.","modifiedtime":"2026-04-22T00:34:31+0000","children":[],"onlyOneRestrictionMustApply":true,"image":{"code":"Karl Keusgen 2000 x2000","altText":null,"imageFormats":[{"imageType":null,"format":"2000","url":"/medias/2000-Karl-Keusgen-2000-x2000?context=bWFzdGVyfGltYWdlc3w0NTk1NDZ8aW1hZ2UvanBlZ3xhR1F5TDJnNVpTOHhNelU0TXpVMk1UYzFNall3Tmk4eU1EQXdYMHRoY213Z1MyVjFjMmRsYmlBeU1EQXdJSGd5TURBd3w0Mjg5ZWFiNzBhNTBhZjNiM2QxZTlhNmM1MGZkZjRiY2QwNmNmY2VhYmI1M2E2NGNjZTdiMzBjZjZkY2EzNDM4","altText":null,"galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":null},{"imageType":null,"format":"1600","url":"/medias/1600-Karl-Keusgen-2000-x2000?context=bWFzdGVyfGltYWdlc3wyODAzMTd8aW1hZ2UvanBlZ3xhR001TDJnME1pOHhNelU0TXpVMk1qTTBNalF6TUM4eE5qQXdYMHRoY213Z1MyVjFjMmRsYmlBeU1EQXdJSGd5TURBd3xkNTRlODA4MmU0NGQ4M2ZiMTg1YmM0YzBkMjBjZjMxODE0NjYyYmQxNTQ1N2FjYWY0OTQxMjQwNmM5YTMzOGMx","altText":null,"galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":null},{"imageType":null,"format":"1280","url":"/medias/1280-Karl-Keusgen-2000-x2000?context=bWFzdGVyfGltYWdlc3wxODAzMDd8aW1hZ2UvanBlZ3xhREV6TDJnNVlpOHhNelU0TXpVMk1UZzRNelkzT0M4eE1qZ3dYMHRoY213Z1MyVjFjMmRsYmlBeU1EQXdJSGd5TURBd3w0NTUwZjUzYWJkMzJhYTRiZWJmYzY1MTY2ZTNmYTVmODBhM2IxOWNkOWUxZTMzNGFiMzQ2Y2U1MDQzODE1NGMx","altText":null,"galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":null},{"imageType":null,"format":"1024","url":"/medias/1024-Karl-Keusgen-2000-x2000?context=bWFzdGVyfGltYWdlc3wxMjAzOTR8aW1hZ2UvanBlZ3xhREUxTDJnNU9DOHhNelU0TXpVMk1UazBPVEl4TkM4eE1ESTBYMHRoY213Z1MyVjFjMmRsYmlBeU1EQXdJSGd5TURBd3xlYTYxNjk5Yzk3ZDRiODBhYTA1NGY5ZGZlZmNlNWVmNzI5OTU4NzQ3Y2E1YjNhODM1OTM2ODRiZjAyZGRlYThj","altText":null,"galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":null},{"imageType":null,"format":"768","url":"/medias/768-Karl-Keusgen-2000-x2000?context=bWFzdGVyfGltYWdlc3w3Mzc3NnxpbWFnZS9qcGVnfGFEVTVMMmcwWkM4eE16VTRNelUyTWpBeE5EYzFNQzgzTmpoZlMyRnliQ0JMWlhWeloyVnVJREl3TURBZ2VESXdNREF8MTJhY2U5MTI0ZDViNGM0MmY2MzU4MmM3OGI3MTY4OTFmMWI2OWQ4YmQ1YTYwNTFlZmRlMGI3NTA5N2M1NDkxZQ","altText":null,"galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":null},{"imageType":null,"format":"480","url":"/medias/480-Karl-Keusgen-2000-x2000?context=bWFzdGVyfGltYWdlc3wzNTQ5MHxpbWFnZS9qcGVnfGFEazNMMmcwWXk4eE16VTRNelUyTWpBNE1ESTROaTgwT0RCZlMyRnliQ0JMWlhWeloyVnVJREl3TURBZ2VESXdNREF8MzRhYTk5ZDRhNzY4MDJlZGU3NWU5OWFlZWRjZmJiODNkYWYyZjFhNzNhZGY5OGQ1NjU1NzgyZDk4ZmM4Y2U2NQ","altText":null,"galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":null},{"imageType":null,"format":"200","url":"/medias/200-Karl-Keusgen-2000-x2000?context=bWFzdGVyfGltYWdlc3w1MTM5fGltYWdlL2pwZWd8YUdSaEwyZzBOUzh4TXpVNE16VTJNakkzTmpnNU5DOHlNREJmUzJGeWJDQkxaWFZ6WjJWdUlESXdNREFnZURJd01EQXw4ODJjZmQxYzlhYjU0OTk5NmQzZTc5N2ZlOTdlOWVkZDVhMTI2OGM0MGRjMzVmOWJlZTg1OTczYjgzMDg5OTE0","altText":null,"galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":null}],"description":null},"lastLoad":1776818071179,"visible":true,"wagoColumnComponent":[],"imagePosition":"LEFT","availableLanguages":"AVAILABLE","passepartout":true,"restrictions":[],"searchable":true,"lead":"<p>Karl Keusgen, CEO of Deutsche Windtechnik Steuerung</p>","typeCode":"WagoQuoteTeaserComponent","slots":["eyJpdGVtSWQiOiJjc19kZV8wMDAwRVQ3SiIsImNhdGFsb2dJZCI6InNnLXdhZ29Db250ZW50Q2F0YWxvZyIsImNhdGFsb2dWZXJzaW9uIjoiT25saW5lIn0="],"itemtype":"WagoQuoteTeaserComponent","restricted":false,"name":"WagoQuoteTeaserComponent","synchronizationBlocked":false,"containers":[],"creationtime":"2025-09-26T07:19:58+0000","actions":[],"contentVersion":3,"parents":[]}