[{"term":"Libraries_BA","id":0,"type":"QUICKLINKS"},{"term":"Instructions","id":1,"type":"QUICKLINKS"},{"term":"WAGO-I/O-PRO","id":2,"type":"QUICKLINKS"},{"term":"Building","id":3,"type":"QUICKLINKS"},{"term":"221","id":4,"type":"QUICKLINKS"}]
{ "@context": "https://schema.org", "@type": "BreadcrumbList", "itemListElement": [ { "@type": "ListItem", "position": 1, "name": "Homepage", "item": "https://www.wago.com/us" }, { "@type": "ListItem", "position": 2, "name": "Industries", "item": "https://www.wago.com/us/industries" }, { "@type": "ListItem", "position": 3, "name": "Marine", "item": "https://www.wago.com/us/marine-offshore" }, { "@type": "ListItem", "position": 4, "name": "Interview", "item": "https://www.wago.com/us/marine-offshore/interview-energy-saving-shipping" } ] } [{"url":"/industries","name":"Industries","linkClass":null,"categoryCode":null},{"url":"/marine-offshore","name":"Marine","linkClass":null,"categoryCode":null},{"url":"/marine-offshore/interview-energy-saving-shipping","name":"Interview","linkClass":"active","categoryCode":null}]
Interview

“You can only save a limited amount of energy from land.”

It comes down to the crew: Interview with Hannah Ohorn, Superintendent for the Hamburg Süd shipping company.

Some 10,500 containers in total – then the Cap San Raphael is fully loaded. The ship has traveled the world’s oceans for the Hamburg Süd shipping company for five years. According to load, route, and weather conditions, this ship and its five sisters burn between 90 and 100 tonnes of fuel per day. They are the largest of the 46 ships in Hamburg Süd’s bright red fleet. Hannah Ohorn, Superintendent at the Hamburg Süd shipping company, sees substantial potential for savings in this number, without sacrificing convenience. At more than 400 dollars per tonne, the work quickly pays for itself. We spoke with Hannah Ohorn in Hamburg to learn which measures the shipping company – a new member of the Danish Maersk Group – will implement and how they plan on including the vessel’s crew.

We are currently standing on the bridge of a container ship, which is considered one of Hamburg Süd’s most modern vessels. Are there any possibilities left for increasing efficiency in shipping?

Ohorn: Oh, yes, of course there are. One goal of our energy efficiency projects is, for example, to save one tonne of fuel per ship every day. This can be implemented in a relatively easy way if everyone on board looks closely at things and makes an effort.

Where exactly should people be looking?

Ohorn: Let’s use the seawater cooling pumps as an example. These supply the necessary amounts of cooled water to the engines over multiple circuits when the ship is in motion. If the ship is docked, or if the primary engine is running at a reduced load, then the cooling requirements are reduced significantly to the point where it makes sense to switch pumps off. However, this means that after docking, someone has to think about this and go down and turn off the pumps. Then, it also becomes necessary to close this valve or that one in order to prevent pressure losses.

It that a lot of work?

Ohorn: No, but it is additional work and that can irritate the crew sometimes. I know this myself from my time on board. If a shipping company stipulates these types of activities as necessary for increasing energy efficiency, then the crew must also understand the reasoning behind them. The company has to calculate how much the crew saves by switching off the pumps in the harbor. These types of small actions can quickly add up over the day to fuel savings of more than a tonne.

Does your shipping company reward crews that think about such activities?

Ohorn: We are considering a bonus program at Hamburg Süd and have held discussions about it. The people backing this include the captains, chief engineers, first officer and the second engineer.

How has that turned out as a whole?

Ohorn: We have jointly decided against a monetary program of bonuses, because we feel a moral obligation to save energy. We have agreed that at Hamburg Süd, we are ultimately paid to bring ships safely and efficiently into harbor. In general, however, the question remains as to how we can correctly configure such a bonus system. We have discussed this internally for a long time.

Do you have another example for effective efficiency measures?

Ohorn: Yes, the diesel generators. There are five installed on this ship, each with an output of 4500 kW. Now, let us assume that the actual load is 3600 kW. I see it all the time: Two generators are running, even though the need could easily be covered by one system. An optimal operating level for a generator is an 85 percent load. Due to undefined safety considerations, when one generator is running at an 80 percent load, then a second is often switched on; this means that both will run at just a 40 percent load. This gains nothing, because fuel consumption exorbitantly increases due to the poor efficiency. And we are precisely interested in specifically optimizing fuel consumption.

For that, you need to measure and evaluate everything. How do you collect the data?

Ohorn: We collect the data available on board using a Bluetracker and provide this to the crew. In additional, we run an evaluation at the office so that we can compare different ships with each other. We are currently at the beginning of the evaluation and validation phase.