MM-400936_new-website-page_open_for-the-industrial-iot_2000x1125

Open Automation with WAGO

For Easy Connection to the World of the Industrial IoT

The basis of successful digitization and automation is a comprehensively networked infrastructure in which all the data is integrated into the IT. To ensure successful conversion of data to digitized, networked processes, we’ve developed an open automation platform for easy connection of both new and existing technologies.

Under the motto “open to the Industrial IoT,” our components’ connectivity options go beyond the field level and build a bridge to the IT infrastructure. This allows smooth, continuous communication from the field level to the cloud.

Open Automation with WAGO

For Easy Connection to the World of the Industrial IoT

The basis of successful digitization and automation is a comprehensively networked infrastructure in which all the data is integrated into the IT. To ensure successful conversion of data to digitized, networked processes, we’ve developed an open automation platform for easy connection of both new and existing technologies.

Under the motto “open to the Industrial IoT,” our components’ connectivity options go beyond the field level and build a bridge to the IT infrastructure. This allows smooth, continuous communication from the field level to the cloud.

WAGO Cloud

WAGO Cloud allows you to collect and analyze data from different machines and systems in a central location. In addition, you can manage and monitor all your WAGO controllers, including your data and applications. With its simple, user-friendly operating concept, WAGO Cloud was developed for users without extensive IT know-how.

Loesungen_Offene_Automatisierung_Controllerbild_DE-SAPCloud_2000x2000.jpg

Cloud Connectivity

It’s all about data: In the past, technical data from the field only made it as far the control and management level at best. The situation is different now – thanks to modern information technology, important information from production is no longer limited to the conventional automation pyramid and is available anytime and anywhere. However, this has certain technical requirements. The WAGO PFC Controllers and Touch Panels 600 feature cloud connectivity and transfer data to WAGO Cloud – or any other MQTT broker.

MM-17122 website update IoT-Box_iot-box-frontalansicht-seitlich_2000x2000.png

WAGO IoT Box

With the IoT Box, WAGO takes the first step, offering an easy-to-use, practical solution with concrete added value. The box is universal and ideal for machine, device and property connection, as well as asset management. It is completely pre-assembled in a solid housing and equipped with WAGO’s pioneering automation technology.

Related to the Topic

Customer Applications on the Cloud

energy_referenz_stadtwerke-osnabrueck_christian-dreckstraeter_digitalisierung_verteiler3_2000x1125.jpg

Distribution Network in Real Time

SWO Netz GmbH, an incorporation of the Osnabrück municipal utility, is preparing for electrical distribution in the future by establishing a cloud project. The company, which is based in Lower-Saxony, uses WAGO technology to manage and analyze their data.

WDE_1802_WAGO_avacon-0371_2000x1125.jpg

Digitization as the Basis for Sector Coupling

Sector coupling, digitization and customer centricity – these are the cores of energy service provider Avacon Natur’s business! All of this increases the efficiency of power plants and district heating networks and provides information as needed. Above all, sector coupling – integrated control for heat, electricity and electromobility – requires digital data acquisition.

energy_referenz_stadtwerke-osnabrueck_christian-dreckstraeter_digitalisierung_leitwarte12_2000x1125.jpg

Distribution Network in Real Time

SWO Netz GmbH, an incorporation of the Osnabrück municipal utility, is preparing for electrical distribution in the future by establishing a cloud project. The company, which is based in Lower-Saxony, uses WAGO technology to manage and analyze their data.

digitalisierung_referenz_fort-knox_cybersecurity_istock_172776360_2000x1125.jpg

Highest Level of Security for Computer Centers Thanks to Cloud-Based Power Data Analysis

If hackers or a technical malfunction paralyze the servers of a corporation, the failures can lead to millions in damage. One company, Correct Power Institute, has developed a method for monitoring computer centers that quickly traces faults in the power supply and thus ensures high availability of the IT systems.

Your WAGO Contact

Additional service offerings: