Customer application

Cornerstone of the Energy Transition

Automation for Modular Hydrogen Generation

Hydrogen will play an important role as an energy storage system in the sustainable energy landscape of the future. The collaboration between WAGO and FEST demonstrates how this production can be carried out in the present using modular concepts and the interplay of sophisticated automation technology.

MM-458419_GWA_Referenz-FEST_X1A1765_2000x2000

The potential for green hydrogen is enormous – both today and in the future as it continues to grow.

Christian Perplies
Senior Sales and Business Development Manager for Hydrogen Technology at FEST GmbH

A Collaboration between FEST and WAGO

Innovation through Cooperation

MM-458419_GWA_Referenz-FEST_X1A1038_2000x1125.jpg

Hydrogen: A Key Element in the Future Energy Mix

Electric vehicles, heat or hot water generation: wind and sun now drive more electrons through electrical conductors – without detours, directly from the generator to the consumer. Indeed, it seems that the future of energy supply can’t manage without molecules. Energy must be stored. Some consumers also have an unquenchable desire for more energy in the tank than, for example, their batteries currently offer.

Thus, the energy cocktail of the future requires a little addition for its success, that is, hydrogen, the smallest molecule. When produced with excess electricity generated from renewable sources, it forms both a potent energy storage system, and also an alternative energy supply for aviation, long-distance, heavy-duty and marine traffic.

FEST Converts Excess Energy into Green Hydrogen

However, as convincing as the concepts appear on paper, there are still questions regarding the source of green hydrogen.

One solution may already be close to home: electrolyzers can exploit their full potential when located near wind farms or solar parks. Instead of throttling wind turbines or decoupling solar cells from the grid in the event of an oversupply of energy, the green current that is not being consumed can instead be used to split water into oxygen and hydrogen.

FEST, headquartered in Goslar, provides these types of systems. The company, part of the Schmidt Kranz Group, plans, develops, builds, and installs custom hydrogen electrolysis systems and supply systems for Power-to-X applications.

Due to their size, these systems are not continuously monitored on-site – a concept that only succeeds when engineering, system technology, and automation work seamlessly together.



Want to read more? You can download the entire story from us for free!

Want to read more?

Download the complete customer application report here and discover the many possibilities our solutions offer.

Components from WAGO

Details of the WAGO Products Installed in the Project

MM-16046  3D product pictures  IO system Field EthernetIP and EtherCAT variants_2000x2000 (2).jpg

WAGO I/O System Field

Decentralization with extended connectivity – the WAGO I/O System Field for IP67-rated cabinet-free automation features an impressive range of functions.

Your Benefits:

  • Integrated load management

  • Extended network connectivity

  • Functionality and aesthetics in one system

  • All-in-one solution thanks to IO-Link

Power Supplies

Power supplies are the core of any automation solution. WAGO offers a broad portfolio of different series and performance classes for virtually any application.

Your Benefits:

  • Highly efficient devices with up to 96.3% efficiency

  • Numerous approvals for a wide range of applications

  • CAGE CLAMP® connection technology for nearly all devices

Your WAGO Contact

kontaktmodul_kundenservice_zentrale_300x300_1

Main Office

Monday -Thursday 8:45 am – 5pm Friday: 8:45 am – 4pm

Additional service offerings: