Customer application

Building Automation on the iPad

  • 7/21/2020
  • Low energy consumption was one of the main goals that Günther Heumann pursued when he was planning his new corporate headquarters. At the same time, he wanted to demonstrate modern building automation to his customers. A WAGO ETHERNET Controller and an app for the iPad form the basis of the building automation.

    The new corporate headquarters for Elektro-Service Heumann GmbH offers CEO Günther Heumann and his ten employees 400 m² of office and storage space. During planning, special focus was placed on providing optimal comfort in the space while keeping energy costs low. For example, the south-facing facade is nearly all glass, allowing the sun to warm up the rooms during the colder seasons. Blinds ensure that the temperature does not climb too high in the summer. A wood-fired furnace with an output of 14.5 kW provides the building with warm-air heat if the solar radiation alone is not sufficient.

    In cold weather, a cross-stream heat exchanger uses the exhaust air to warm the supply air so that very little energy is required for heating. COMFORT AND ENERGY EFFICIENCY Building Automation on the iPad It is also possible to cool the rooms using the supply air. To accomplish this, ground heat collectors were situated under the parking garage; these use a brine pipeline and a heat exchanger to cool the supply air.

    building_referenz_heumann_ipad_1_2000x1500.jpg

    Central Air-Conditioning Control

    Günther Heumann uses the WAGO-I/O-SYSTEM with the 750-881 ETHERNET Controller to automate the air-conditioning system. The ETHERNET Controller adjusts the supply and exhaust air flaps in the individual rooms, the cross-stream heat exchanger, the ventilator motors, the heating, the pump for cooling and the SMI drives for the blinds. Temperature sensors in the rooms provide the current actual value; the controller compares this to the setpoint specified by the user in order to adjust the ventilation flaps accordingly. The WAGO-I/O-SYSTEM thus automatically controls the entire air-conditioning system. Günther Heumann and his team created the CODESYS programming themselves in accordance with IEC 61131-3.

    building_referenz_heumann_ipad_2_2000x1500.jpg

    Light, Sound and Video Monitoring

    The building automation at Elektro-Service Heumann was also designed to meet another important requirement: The company would like to demonstrate to customers what is possible using this type of solution. To achieve this, all systems were to be incorporated into the central automation if possible. Thus, in addition to HVAC for individual rooms, the WAGO controller regulates the lighting via DMX bus, and also controls video monitoring and a Bose multi-room sound system. Touch-panel controls in the individual rooms transmit user inputs to the automation technology using EnOcean wireless technology. Special sensors in the window handles also communicate via EnOcean; signaling the controller whether the window is open, tipped or closed.

    Operation via iPad

    However, the highlight of the entire automation system is the user interface on the Apple iPad. The user can program all automation settings centrally and access all functions individually. At the same time, the “AmbientRC” app, created by Günther Heumann, provides an overview of the current status of the building automation – it displays the current electrical power consumption for the entire building, among other things. Reduction of lighting energy consumption Parameterization and visualization of building automation via iPad Control of HVAC, lighting, video monitoring and a Bose multi-room sound system

    To display the building automation information on the iPad, the controller generates the appropriate XML files and stores them on the internal Webserver. The app then visualizes the information on the iPad. Company owner Heumann is completely satisfied: “From the lighting control, to the blinds, to the incorporation of sound systems, the WAGO ETHERNET Controller offers a lot of possibilities that we’ve used here in our own building.”

    By Detlef Holfeder | 2013-03-19

    Image sources: Elektro-Service Heumann, WAGO

    Product Overview

    Controller ETHERNET; 3rd Generation
    Item no. 750-881

    Controller ETHERNET; 3rd Generation

    Configuration cable; USB connector; Length: 2.5 m
    Item no. 750-923

    Configuration cable; USB connector; Length: 2.5 m

    The Right Automation Technology Products

    buehne_io-system_2000x1500.jpg

    I/O Systems – Ready to Use Anywhere

    Whether inside or outside the control cabinet, WAGO’s I/O Systems provide automation right where you need it – even under harsh conditions.

    WAGO at Work

    Customer Applications: Building Technology

    As a partner and innovation leader, WAGO implements many interesting projects. Learn more about our creative and efficient building technology solutions.

    building_referenz_schulte_elektrotechnik_buero_2000x1500.jpg

    Sustainable Networking

    With its administration building, Schulte Elektrotechnik GmbH shows how intelligent and flexible building and room automation can be.

    systemgrafik-hlk-aufbau-einer-bacnet-steuerung_2000x1500.jpg

    BACnet Controller Setup

    With our solution, it is possible to wire the fieldbuses in a line topology. This eliminates additional elements such as switches or hubs.

    Your Contact Person at WAGO

    kontaktmodul_kundenservice_zentrale_300x300_1

    Main Office

    Monday -Thursday 8:45 am – 5pm Friday: 8:45 am – 4pm

    Additional service offerings: