Customer Application

A Watchful Eye for Maintenance

Early detection of anomalies enables condition-based maintenance.

Air Liquide, a specialist in industrial gases, has invested nearly €40 million at its site in Stade, Lower Saxony, to decarbonize synthesis gas production. As part of this initiative, continuous monitoring of the new high-temperature reactor was implemented. WAGO provided the ideal solution: a combination of a thermal camera, a WAGO IoT Gateway, and seamless integration into the process control system. This setup enables early detection of anomalies and supports condition-based maintenance when needed.

The great advantage of the WAGO and TTS system is that it functions like an early warning system. Damage in the reactor tends to develop gradually, allowing us to inform our customers in advance. They can then adjust their production, and we can shut down in a controlled manner, make repairs, and quickly restart.

Hendrik Gollek, Project Engineer, Cluster Central Europe, Düsseldorf, Air Liquide

Innovation Through Cooperation — A Collaboration between Air Liquide and WAGO

Automated Monitoring in a High-Temperature Reactor

The core of the Air Liquide system in Stade is the new high-temperature reactor. Preventing unplanned downtime was a top priority. Detecting damage to the masonry surrounding the reactor — damage that inevitably occurs over time — offers limited technical options. Air Liquide sought a method to reliably assess the reactor’s condition without relying on scheduled or suspicion-based shutdowns. Experts recommended industrial thermal cameras for early hazard detection. TTS Automation selected Prometheus, a solution that identifies temperature anomalies regardless of environmental conditions. It is based on intelligent control technology from WAGO, including the PFC200 from the 750 Series.

Seamless Integration into the Automation Landscape

For uninterrupted inspection, three cameras are positioned radially around the reactor in two layers, with an additional camera mounted above the container. These cameras transmit all relevant data to the control system, including maximum and minimum values segmented by sector. Fixed alarm thresholds are configured to trigger alerts only when values exceed or fall below defined limits. The camera software operates on the WAGO IoT Box, which integrates seamlessly into process industry environments as an interface to the control system. This setup enables Air Liquide to utilize the full functionality of the cameras and process raw data efficiently. Managing and calculating anomaly data at the PLC level reduces system load. Operators can communicate directly with the camera electronics from within the control system.

Want to learn more? Download the full story for free!

Want to Learn More?

Download the complete customer application report here — and discover the many possibilities our solutions offer.

Components from WAGO

Details of the WAGO Products Installed in the Project

MM-370198_GWA_Steuerungen_16_2000x2000.jpg

Controllers

The WAGO PFC200 Controller enables efficient design, control, and visualization of your projects. It is widely used in process industries, building automation, and mechanical engineering — particularly benefiting complex applications.

Key Benefits:

  • Linux® operating system and CODESYS (CODESYS V3) programming

  • High cybersecurity standards

  • Remote access via mobile communication with integrated web visualization

Untitled Post (GWA Formats) (2000x1125) (2) (1).png

Digitalization Out of the Box: WAGO IoT Boxes

The company of the future is fully networked. What is not yet integrated into IT must be connected — especially in production. However, many companies are not yet prepared for this challenge. Their machines and systems are unable to transmit data. WAGO offers the solution: the IoT Box.

Key Benefits:

  • Complete solution for the digitalization of machines and systems

  • Custom control cabinet solutions available

  • Unlock the advantages of Industry 4.0

kontaktmodul_kundenservice_zentrale_300x300_1

Main Office

Monday -Thursday 8:45 am – 5pm Friday: 8:45 am – 4pm

Additional service offerings: