Customer application

Small Terminal Blocks Lead to Big Advancements

  • 8/27/2021
  • OSRAM contributes to the progress of the global lighting market with its new LED driver, which is a mere 11 millimeters thick. A vital component of this innovation is the extremely compact, easy-to-use 2060 Series SMD PCB Terminal Blocks from WAGO.

    As thousands of visitors strolled around the exhibitions at Light+Building 2016, a crowd formed around the OSRAM booth. “We’ve already attracted quite a bit of attention with our new LED driver,” says Nicolai Heber, product manager for LED Drivers & Industrialization at OSRAM, recalling the trade fair. This is a bit of an understatement, considering OSRAM’s new innovation nearly stole the show from the other producers.

    And no wonder – the new linear driver from the “OPTOTRONIC Intelligent” series is called “UltraFlat,” and at only 11 millimeters thick, the reason is clear. But despite its miniature design, the driver provides up to 75 watts, is equipped with a corresponding temperature management system, supports DALI and can also be programmed using Near Field Communication (NFC) wireless technology – though not via DALI or LEDset.

    The Munich-based lighting specialist is opening up whole new dimensions with its new driver. Whereas the standard thickness of LED units was once 30millimeters, about 15 years ago this shrank to 21 or 22 millimeters – and that’s where the standard has remained up to now. In other words, while LED modules were getting flatter and flatter, the shape of the control gear hardly changed.

    OSRAM is now injecting new dynamism into the market – and creating great competitive advantages for lighting manufacturers. From the very beginning, our idea was to provide an ultra-flat LED driver for the high-end lighting segment. “Above all, our goal is to impress customers with attractive designs, even more than costs and energy efficiency” says Heber, outlining the market demands from the manufacturers’ point of view. After all, it was the manufacturers who told OSRAM they wanted a thinner driver. However, at the beginning of the development process, it was not at all clear how thin the new driver could actually be, says Heber. OSRAM’s light designers wanted to offer clear added value, so they set a target of cutting driver thickness in half. After more than a year of exploring possibilities, it became clear that the target thickness of 11 millimeters would be feasible. But there was a further constraint: The thin design could not be allowed to compromise the functionality. Even in a flat enclosure, high standards had to be upheld concerning service life, temperature resistance, light quality and other technical details.

    LED-Treiber.jpg

    Easy Connection Technology

    Half the thickness for twice the design freedom – achieving that presented enormous challenges for the individual components of the driver. However, there was one area where the R&D team did not have to worry much: the connection technology. The OSRAM engineers could rely on the 2060 Series SMD PCB Terminal Blocks from WAGO for their ultra-flat drivers. Introduced around four years ago, these terminal blocks from Minden in North Rhine-Westphalia are among the smallest available on the market. “WAGO terminal blocks were essential for making this product design a reality,” says Heber. As he explains: “They combine two vital advantages: They are extremely small and also enable practical, convenient wiring.”

    osram logo.jpg

    Automated Wiring Is a Must

    Five single-pole terminal blocks are installed on the internal side of the OSRAM driver, with two three-pole terminal blocks on the external side. WAGO’s 2060 Series Terminal Blocks are only 4.5 millimeters thick. They are designed for conductor cross-sections from 0.2 to 0.75 millimeters. “That’s ideal for keeping PCBs extremely flat. The terminal blocks also allow automated wiring. These days, that’s an absolute must,” explains Heinz-Werner Hilgenberg, Market Manager for PCB Applications & Lighting at WAGO. As in other projects, the WAGO expert was closely involved in the development of the new driver. “It’s vital for the connection technology to offer a high degree of flexibility so manufacturers have the freedom they need for product design,” says Hilgenberg, summarizing the essence of his experience. Numerous manufacturers have already come to appreciate the benefits of the small terminal blocks and use them to produce innovative LED modules, for example. Now, the 2060 Series is also playing a leading role in the further development of LED units.

    Drivers Will Offer Even More Functions in the Future

    Under strict secrecy, other completely new components for the new OSRAM driver were created in close cooperation with both suppliers and several lighting manufacturers. The central control chip, for example, although smaller than usual, offers even more functions, and the coil has also been specially adapted. The initial pre-production models of the new driver were ready just in time for Light+Building. A number of OSRAM partners were able to present unusually flat LED lights at Light+Building. These companies also attracted a great deal of attention. The drivers are currently undergoing tests in different countries to obtain corresponding certification. The driver has been available since August 2016. In the months to come, an 11-millimeter-thick daylight harvesting and presence sensor will also be added to the ultra-flat system. Heber thinks LED drivers will become even more intelligent in the near future. “With this product in its current form, it’s already possible to read out data such as hours of consumption. We will definitely see more and more functions like this, especially with a view toward smart grid applications.” And Heber also foresees NFC becoming a standard feature on certain markets in the medium term. “This shows just how big a step forward we’ve taken in terms of module size,” says Heber in summary. But we have not heard the last word on this topic either.

    Product Overview

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white
    Item no. 2060-402/998-404

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 1-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white
    Item no. 2060-451/998-404

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 1-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white

    THR PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white
    Item no. 2060-1452/998-404

    THR PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white

    THR PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 3-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white
    Item no. 2060-1453/998-404

    THR PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 3-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white

    THR PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 1-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white
    Item no. 2060-1451/998-404

    THR PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 1-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 8 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; light gray
    Item no. 2060-802/998-404

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 8 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; light gray

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 3-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white
    Item no. 2060-453/998-404

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 3-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; white

    Board-to-Board Link; Pin spacing 4 mm; 1-pole; Length: 28 mm; white
    Item no. 2060-951/028-000

    Board-to-Board Link; Pin spacing 4 mm; 1-pole; Length: 28 mm; white

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; black
    Item no. 2060-472/998-404

    SMD PCB terminal block; push-button; 0.75 mm²; Pin spacing 4 mm; 2-pole; Push-in CAGE CLAMP®; in tape-and-reel packaging; black

    WAGO at Work

    Customer Applications from Lighting Technology

    building_referenz_nordeon_3_2000x1500.jpg

    Economical LED Technology

    Because of outmoded lighting technology, street lighting is an energy cost trap. The modular light system from Nordeon changes all this – with WAGO technology.

    Your WAGO Contact

    kontaktmodul_kundenservice_zentrale_300x300_1

    Main Office

    Monday -Thursday 8:45 am – 5pm Friday: 8:45 am – 4pm

    Additional service offerings: