building_licht_lagerhalle_2_istock_000014092815_2000x2000.jpg

Lighting Installation and Automation that Proves its Worth

Modern lighting is demand-oriented, convenient and energy-saving. This assumes that your skilled planning, an optimum installation and intelligent lighting control fully exploit the potentials your system offers. When all is properly implemented, you protect the environment, lower energy costs and improve your work environment and atmosphere in the building. This also gains points for commissioning, maintenance and conversions, because, for example, modern lighting management solutions are easily configured through a graphic interface. Elaborate installations and complicated programming are thereby consigned to the past.

Good reasons for WAGO:

  • Ideal lighting quality

  • Greater user convenience

  • Energy-efficient operation

  • Simple commissioning without any programming

  • Fast, simple maintenance and conversions

WAGO Lighting Management

Future-Proof Solutions for Your Building, Too

lighting_potential-energy-savings_2000x2000.jpg

Lighting Management – Leveraging Greater Efficiency

Artificial light illuminates living spaces, office buildings and manufacturing halls; it lights up the streets at night and puts landmarks into the limelight. In fact, lighting currently accounts for some 19% of worldwide electricity consumption. From the business side, however, another aspect is always under consideration: system efficiency. The largest influencing factor here is the cost of energy, which, at around 70% of the total costs of a lighting system, is reflected in the budget. Energy optimization of each lighting system, whether through upgrades or purchased new, will be apparent in future savings.

building_licht_b161125_22-kelvinkurve_finale_2000x2000.jpg

People Are Our Focus

Human-Centric Lighting
Initially, “Human-Centric Lighting” (HCL) means nothing more than placing people and their needs for good lighting up front and center whenever lighting systems are planned. In the context of lighting management, this especially includes the individual adjustment of color temperatures and lighting intensity throughout the day. Thus, the character of the room changes as natural lighting conditions are brought into the building's interior.


This is based on the knowledge that not only is light required for visual acuity, it also sets our internal clocks. If the lighting conditions are adapted corresponding to daily rhythms in a room, well-being and motivation rise, fatigue is prevented and performance increases.

Improved Work with Good Lighting

Lighting is a critical factor in industrial and manual labor. Optimal production results depend on the performance of the employees. The correct lighting helps increase motivation, reduce fatigue, maintain health and prevent accidents. Poor visual conditions have the opposite effect: If it is too dark, productivity drops, we tire easily and errors quickly accrue.

Optimal Production Facility Lighting at Lower Costs

WAGO Lighting Management is the intelligent solution for lighting control in large spaces such as production facilities or warehouses. Using a combination of predefined hardware and user-friendly, web-based software, WAGO Lighting Management facilitates the design and commissioning of new lighting systems and also offers numerous advantages for their operation.

Pluggable Room Installations

The WINSTA® Pluggable Connection System easily meets the strict requirements of building installations. The system provides simple pluggable electrical connections, making electrical installations fast, safe and error-free. You benefit from quality-tested components that ensure installations are error-free and completed on time.

Your Contact Person at WAGO

Additional service offerings: