icon_ex_kennzeichnung_ex_produkte_2000x2000.jpg

Zone Division per ATEX and NEC 500

Depending on the type of materials that occur, hazardous locations are not equally at risk. The frequency and duration of occurrence of one of these substances give rise to the different protective requirements for operating equipment.


According to CENELEC and IEC, hazardous locations in Europe are divided into six different danger zones. The higher the probability that a potentially explosive atmosphere occurs, the more rigorous the requirements on operating equipment to prevent, for example, origination of sparks or hot surfaces.

WAGO in Explosion Protection

Principles of Explosion Protection

Everything worth knowing about Ex protection at a single glance.

Device Categories and Groups

Which resources are permitted for use in a zone can be derived from the specific operating equipment and in dependence on the zone allocation. In order to specify for which zone specific operating equipment may be used, the device group and category are relevant. The explosion protection zone in which the operating equipment may be operated is defined based on temperature classes and explosion groups.

Zone Divisions in North America

In North America, a different classification system based on the standards NEC 500 and NEC 505 is applied. Here, flammable substances are divided into three classes (Classes I to III). Explosive gases, vapors and mists of Class I are subdivided into the gas groups A, B, C and D; flammable dusts of Class II into the groups E, F and G.

Depending on the frequency or duration of occurrence of these materials, the hazardous locations are divided into so-called divisions. Division 1 corresponds to Zones 0 and 1 and Division 2 to Zone 2. In addition to the division of the explosive areas, the construction of the operating equipment and installation of the electrical systems are also differentiated.

Read More Here

What happens during an explosion, which factors are important, and what protective measures are available? Everything you need to know about ATEX, Ex zones, ignition protection categories, etc.

icon_ex_normen_rechtliches_2000x1125.jpg

Directives, Standards and Regulations

The requirements for electrical equipment for hazardous locations are multi-layered: National and international determinations, guidelines and standards must be complied with to achieve the highest possible level of safety. We give you an overview of the most important regulations and recommendations, such as the ATEX directive.

icon_ex_geraetegruppen_geraetekategorien_2000x1125.jpg

Device Groups

Like the devices, gases, vapors, and dust are divided into various groups according to their properties. This division simplifies the right selection of devices for the various gases, vapors, and dusts.

icon_ex_explosionsschutz_2000x1125.jpg

Ex Protection Measures

Who needs explosion protection? To whom does explosion protection apply? What must be noted here? And what is constructive explosion protection? WAGO has compiled answers to the most important questions for you.

icon_ex_zuendschutzarten_2000x1125.jpg

Ignition Protection Categories

Only equipment protected against explosion is permitted in Ex areas. Ignition protection categories are constructive and electrical measures for equipment and qualify as secondary explosion protection.

icon_ex_zuendquelle_2000x1125.jpg

Ignition Sources

If an atmosphere subject to explosion cannot be prevented in a work area, secondary explosion protection is brought to bear. Secondary measures include prevention of any ignition sources in the Ex area.

icon_ex_explosion_2000x1125.jpg

What Is an Explosion?

Ex|plo|si|on; -s <lat.> (explosio) means "escaping under pressure." What happens during an explosion, which factors are important and what protective measures are available? You will learn everything you need to know about explosion protection right here.

WAGO Products for Explosion Protection

titel_0750_XTR_Knoten_017_2000x1500px.jpg

Ready for the Ex Area

Automation under adverse environmental conditions? WAGO products and solutions are made for this.

durchgangsklemmen_2000x1500px.jpg

Inclusive Explosion Protection

Approved for the Ex area: WAGO products form secure connections even under the most extreme conditions

Your Contact Person at WAGO

Additional service offerings: