Efficient System Integration Through Service-Oriented Software in Automation

Today, shipyards are essentially forced to meet delivery dates, and do so in the most optimal way. Mastering complex processes and systems thus becomes an important challenge. In fact, automation and software are already determining the complexity of a ship. The shipyard must work very closely with the supplier of a higher-level monitoring and control system. Ultimately, this total system integrator has a key function during commissioning. The integrator is required to make changes as well as perform the integration test on board. Work is sometimes only possible with one job being performed right after the other, and the working hours are generally more expensive than those in the workshop. For their part, shipping companies must now concentrate on their core business, the mapping of a global logistics chain, unlike ever before. If they need data from their ships, they rely heavily on the integrator who provides the ship's integrated monitoring and control system. Changes in subsystems, such as the bunker system or the boiler, mean that the boiler supplier has to come aboard, for example. In addition, the integrator must also enter the additional variables or measured value ranges into the higher-level system.
The boiler supplier, as an example of any sub-system manufacturer, must be permanently involved in the extensive coordination with many monitoring and control system manufacturers to ensure a viable and standard-compliant visualization of the boiler circuits. If there is any doubt, even the regulation of subsystems will be performed at the management level.