Interview

« Le câblage frontal demande trop d'espace »

  • 2/14/2022
  • Nous sommes convaincus de la polyvalence et des opportunités de notre programme Topjob-S. Mais qu'en pensent les personnes qui l'utilisent à l'extérieur quotidiennement pour leur travail? Entretien avec Michael Bieri, directeur de Bieri Elektrotechnik AG à Uetendorf.

    The terminal blocks are available with different cross-sections. To what extent do you benefit from this variety?

    Since we’re not exclusively a controller manufacturer, we need the complete width from the smallest to the largest cross-section. On the high current terminal blocks, we connect up to 160 A with stranded wires and single conductors.

    The range also includes double- and triple-deck terminal blocks, as well as various specialty terminal blocks. Which of these solutions are you familiar with?

    We’re familiar with the different variants, but we avoid them ourselves as far as possible, since they make the connection situation worse for the electricians. So, when planning the switchgear combination, we always use the normal terminal block to calculate the terminal block space and really only use double-deck terminal blocks in exceptional situations.

    The three-phase power set with lever and operating slot is rarely used in electrical installations, telecommunications network setup and controller manufacturing. Could you imagine using this lever terminal block for the control cabinet supply cable?

    I think that’s basically a good solution. However, with the larger input modules, I find the sealing problematic, since it takes up too much space for terminal blocks with front-entry wiring. From my point of view, side-entry wiring would be a significant improvement, since it’s easier to seal the line entry from the front. For this reason, we run the supply cables to a screw-clamp terminal block so we don’t lose too much space in the depth dimension. Besides that, we don’t use screw-clamp terminal blocks.

    How could you see yourself benefiting from such an optimized terminal block if you could use one?

    From not needing a second product, as we clearly only want pluggable connection.

    A push-in type jumper bar allows many taps in a small space.

    Michael Bieri

    So the two jumper slots that come standard with the terminal blocks are just what you need, right?

    That’s true! For expansion, we use the second slot and simply leave the existing jumper plugged in. That’s great, because it lets us expand easily even while the system is running. If we had to remove the inserted jumper, it wouldn’t be as easy.

    Clean terminal block marking is like a control cabinet builder’s business card. How do you guarantee clear identification of the installed conductors?

    Almost exactly the way you show in your catalogs! Our labeling spans three lines. On the bottom line we number the terminal blocks, on the middle one we indicate the X number and on the top one the load. We now have almost ten smart printers in use. We use a separate printer for each medium so we don’t have to adjust it.

    _SPR4989.jpg

    WAGO’s thermal transfer Smart Printer can be used to quickly check whether the calculated terminal block space is sufficient.

    Michael Bieri

    Why don’t you give us two or three specific examples of how you use the Smart Printer?

    We use a printer for labeling the terminal blocks, for example. Another example is the labeling of individual markers; we even use those to mark third-party products. We print the silver labels for door installations on an additional Smart Printer. In my opinion, there’s no better way to clearly label terminal blocks. You’ve provided a fantastic solution, and your marking system is also the reason we switched to WAGO.

    You sound really convinced!

    I also like the fact that, with the Smart Printer, we can check whether the calculated terminal block space is really sufficient within a few seconds. To do this, we just leave the marking strip off before assembly. Then whoever’s in charge can just hold the strip up to the control cabinet and immediately see whether the planning was correct. In the past, sometimes we’d place the terminal blocks, and after 80 percent of the work was done, we’d realize that the available space was insufficient. And this verification mechanism involves no extra effort for us, since we’d have to print out the marking strip anyway.

    How do you get the data from the circuit diagram to the Smart Printer? Do you use a CAE system, or maybe even the Excel import function?

    We use the Excel import function, but only to a very limited extent, since we often don’t get the data from the planning stage at all. When we’re the ones drawing the diagram, that’s all set and works just fine. But with most of the circuit diagrams we get from outside sources, we have to copy it manually in the workshop.

    Personne de contacte

    Remo Marti

    Area Sales Manager Building
    Region Suisse centrale
    +41 (0)26 676 73 85

    Adresse e-mail: remo.marti@wago.com

    WAGO en pratique

    RÉFÉRENCES ISSUES DE LA TECHNOLOGIE DE BÂTIMENT

    En tant que partenaire et leader de l'innovation, WAGO met en œuvre de nombreux projets intéressants. Découvrez ce que nous pouvons faire pour des solutions créatives et efficaces dans le domaine de la technologie du bâtiment.

    L'imagination est la seule limite

    Avec ses trois succursales, l’entreprise Burtscher Elektro- und Gebäudetechnik AG est un partenaire de choix dans le secteur de la construction dans l’agglomération de Saint-Gall. Grâce à son expertise, elle soutient ses clients dans la planification et la mise en oeuvre de systèmes électriques, donne des conseils en matière d’électrobiologie ou apporte son aide dans l’intégration des systèmes d’automatisation de bâtiments. Au siège de la société à Flawil, Patric Burtscher démontre aux parties intéressées les nombreuses possibilités d’automatisation des bâtiments et la facilité d’utilisation des systèmes proposés par Wago Home Automation.

    Casa_Clara.PNG

    C'est la Champions League !

    Un contrôleur principal, trois sous-contrôleurs, plusieurs centaines de relais, ainsi que tous les appareils de terrain cartographiés directement dans le BIM. Ce sont les dimensions du plus grand projet WAGO Home Automation jamais réalisé en Suisse. Compte tenu de ces paramètres, la vue sensationnelle que la Casa "Clara" offre sur le Gotschna est presque un peu perdue.

    Your Contact at WAGO

    Additional service offerings: