Electrical Power Supply
Imtech GmbH & Co. KG was awarded the contract to work on the electrical installations in the central area of Building 23. This power and building technology company has more than 5,000 employees and constructs its own control cabinets at its facility in Illingen, Germany. The Imtech facilities in Frankfurt and Illingen collaborated closely on the University Hospital project. In all, 200 distribution boards were built, installed on site and connected to the hospital’s systems. Design and construction of the distribution boards occurred at Imtech’s Illingen manufacturing facility. The connection-ready distribution boards were delivered, installed and connected by the workers from Imtech’s Frankfurt office. In addition to the distribution boards that were installed in specialized utility rooms, nearly 80 ceiling-mounted distribution boxes were required for integration into the building’s suspended ceilings. These were also manufactured in Illingen, then installed and cabled on site.
Every device in the building is supplied with electrical power from these wiring distribution boards. In addition to general facilities, like administrative offices and doctors’ and nurses’ offices, these also include patient rooms, as well as operating rooms and treatment rooms. The latter areas include X-ray machines, lasers and other medical devices that need electricity. The ceiling-mounted distribution boards are equipped with WAGO’s 2002-3217 TOPJOB® S Through Terminal Blocks, which enable a change in conductor size from 4 mm2 (12 AWG) to 2.5 mm2 (14 AWG). With a conductor size of 2.5 mm2 (14 AWG), the maximum permissible conductor length is only 25 m. Since the distances between the distribution boards and loads are often longer, the conductor size must be adjusted in the ceiling-mounted distribution boards. This highlights an important benefit: ease of wiring. Since the electricians must perform overhead cabling work while standing on scaffolding, rail-mount terminal blocks equipped with push-in connection technology are extremely advantageous.