Customer application

A Climate in Tune With the Art

building_referenz_augusteum_landesmuseum-kunst-kulturgeschichte_2000x1125
  • 3/31/2021
  • Old works of art require a stable room climate. To optimally maintain them, the correct temperature and humidity must be fastidiously observed. This applies in particular when temporary exhibits are displayed with loaned pieces, because no one will provide art works if they are not assured that they will be returned in the original state.

    Therefore, in the course of substantial modernization work at the Oldenburg Augusteum, an indoor air system including individual room monitoring was installed, controlled using the WAGO 750 I/O-SYSTEM. This automated solution guarantees optimal conditions and additionally helps with energy savings. Narrow spatial relationships and monument protection requirements provided challenges for the planners.

    Automation Ensures Stable Conditions

    Previously, stationary humidifiers served to make the dry furnace air more palatable for the works of art. Now, the Augusteum relies on an automated solution that satisfies international museum standards and protects the exhibited art works. The necessary technology was installed over the course of comprehensive modernization work, and has functioned without fault since the re-opening of the museum in December 2015. Nossol Automatisation GmbH was selected by the state museum to install the automation systems along with designers from the engineering firm Ahrens GmbH. They had to accommodate specific conditions guaranteeing the requirements for temperature, humidity, and noise level, which are based on guidelines for HVAC systems developed by the Association of Mechanical and Electrical Engineers in 2011. The margin of error is quite low. Specifically, the room temperature should average 20 °C. A maximum hourly deviation of 1 C, a maximum short-term deviation of 2 C, and a maximum long-term deviation of 5 C are allowed. The relative humidity must remain at 50%. In this case, maximum deviations of 2.5% per hour and 5% per day are permissible. The specification for sound pressure level permits a maximum of 45 decibels. The designers assumed an average number of visitors to be 70 persons per day.

    building_referenz_augusteum_landesmuseum-kunst-kulturgeschichte_technik_schaltschrank_2000x1500.jpg

    Central HVAC System Creates the Desired Conditions

    To fulfill these requirements, and to guarantee a hygienic, pre-conditioned proportion of external air, a central HVAC system was installed in the basement. In addition, the exhibit rooms were decoupled from the open stair case by pairs of self-closing doors, forming air locks. The HVAC system has an output of up to 2,400 m3 per hour and provides the functions of heating, cooling, dehumidifying, and air circulation. It is equipped with a high efficiency rotating heat exchanger which has a heat recovery factor of around 75% in heating operation. The air humidity is carried out by a separate steam generator in a downstream humidifying chamber. The air is transported via the building’s primary duct system into the intermediate floor area between the ground floor and upper storey, and from there via air ducts into the exhibit rooms.

    Using Building Technology from WAGO

    The new ICA system from Nossol Automatisation was equipped with the modular 750 I/O-SYSTEM from WAGO. Nine subdistributors are used in the Augusteum in addition to the information node, which is equipped with a touch panel. They communicate with one another via an ETHERNET network per Modbus/TCP. “By using the open source communication standard, the WAGO controllers can be easily and efficiently connected to one another. Even configuration is no problem due to the user-friendly software,” agree Arne Meyer and Lukas Vorwerk from Nossol Automatisation, which was responsible for the programming.

    building_referenz_augusteum_landesmuseum-kunst-kulturgeschichte_touch-panel_heizungskeller_2000x1500.jpg

    Space Limitations and Monument Protection as Challenges

    Decentralized air treatment modules (ATMs) were also installed in the exhibit rooms. These cover cooling loads and enable individual room monitoring. The ATMs function exclusively in air circulation mode and generate around 350 to 400 m3 of air per hour. They heat, cool, dehumidify, and transport the air in the rooms. The accommodation of the devices and the necessary supply routes were anything but easy. After all, the exhibit rooms are accessible for visitors. The HVAC technology should not distract from the exhibits and should be as close to invisible as possible. Locating the technology under the ceilings was not practical from maintenance or operational stand points, due to their height. Therefore, the technology had to be concealed in the walls. Because the Augusteum is under monument protection, any changes were highly restricted. Therefore, the building was provided with false walls, which provided 40 cm of space – not a great amount. It is thus good that WAGO products require little space. “Since the PLC already has two integrated ETHERNET interfaces and a switch, we could omit additional infrastructure elements,” according to Stefan Behrens from Ahrens. “When there's not much space, that is worth its weight in gold.”

    Significantly Increased Energy Efficiency

    Even though the main focus was on air quality, a nice side effect of the modernization is a substantial improvement in energy efficiency. Contributors to greater efficiency include the new building technology, a hydraulic balance, which was installed at the same time, and the replacement of the the heating units valves.

    Text: Stephan Lampe, | WAGO

    Photo: Till Werhan | BILDSCHÖN

    Product Heading

    Coupleur de bus de terrain ETHERNET; 3ème génération
    Réf. 750-352

    Coupleur de bus de terrain ETHERNET; 3ème génération

    Entrée analogique à 4 canaux; 4 à 20 mA; Single-Ended
    Réf. 750-455

    Entrée analogique à 4 canaux; 4 à 20 mA; Single-Ended

    Coupleur de bus de terrain PROFIBUS DP; 2ème génération; 12 MBd
    Réf. 750-333

    Coupleur de bus de terrain PROFIBUS DP; 2ème génération; 12 MBd

    Entrée analogique à 2 canaux; Pour capteurs de résistance Pt100-/RTD
    Réf. 750-461

    Entrée analogique à 2 canaux; Pour capteurs de résistance Pt100-/RTD

    Coupleur de bus de terrain PROFINET IO; 3ème génération; Avancé
    Réf. 750-375

    Coupleur de bus de terrain PROFINET IO; 3ème génération; Avancé

    Entrée analogique à 2 canaux; 4 à 20 mA; Single-Ended
    Réf. 750-466

    Entrée analogique à 2 canaux; 4 à 20 mA; Single-Ended

    Entrée analogique à 4 canaux; DC 0 … 10 V; Single-Ended
    Réf. 750-459

    Entrée analogique à 4 canaux; DC 0 … 10 V; Single-Ended

    WAGO at Work

    Additional Solution and References from Building Automation

    building_referenz_voestalpine_gebaeude_nacht_1_2000x1500.jpg

    More Light, Lower Costs

    If the ecological aspects of lighting are a concern, then energy efficient illumination must be combined with an intelligent lighting management system.

    Votre interlocuteur chez WAGO

    Additional service offerings: