Early detection of anomalies enables condition-based maintenance
Air Liquide, a specialist in industrial gases, has invested nearly €40 million at its site in Stade, Lower Saxony, to decarbonize synthesis gas production. As part of this initiative, continuous monitoring of the new high-temperature reactor was implemented. WAGO provided the ideal solution: a combination of a thermal camera, a WAGO IoT Gateway, and seamless integration into the process control system. This setup enables early detection of anomalies and supports condition-based maintenance when needed.
In This Article, You Will Learn:
Why seamless integration into the process control system is more sustainable than a stand-alone solution.
The importance of the interface to the control system, especially when retrofitting existing machines and systems.
How managing and calculating anomaly data at the PLC level already reduces system load.