Customer application

A Match for Even the Harshest Weather Conditions

  • 9/21/2017
  • Wind, waves and salt water: The prevailing conditions at sea are rough for humans and machines alike. This is why the marine industry has special requirements for the technical equipment aboard vessels. The equipment must be covered by a marine approval, as well as explosion-proof certification, to ensure it can survive such use – like WAGO’s I/O System can.
    Communication solutions, such as fieldbus connections, I/O modules and boards, must have marine approval, as well as an Ex-proof certification, to ensure that they can be used to control hydraulic valves. And this is where the problem starts: In the past, the worldwide market offered products that only fulfilled one of the two requirements. The WAGO-I/O-SYSTEM was the first to combine two approvals in one system. However, this is not the only reason PG Flow Solutions AS relies on WAGO.

    The WAGO-I/O-SYSTEM only need half as much space as conventional modules, leaving plenty of room for installation.

    The function modules of the WAGO-I/O-SYSTEM only need half as much space as conventional modules, leaving plenty of room for installation.

    Signal and Voltage Transmission in One System

    “The requirements that we have pertaining to Ex-proof certification, as well as marine approval, are special,” explains Odd Sverre Pedersen of PG Flow Solutions AS. PG delivers controllers for hydraulic aggregates and load pumps for a series of special ships, including supply ships for oil production operations. The company wanted to develop an automation system that would supply the hydraulic system’s controller with the voltage of the communication solution. This configuration would ensure that PG could offer an effective and competitive solution to its customers, explains Pedersen. “We evaluated the currently available I/O systems from different suppliers that included both approvals,” says Pedersen. “Two renowned manufacturers made it through our analysis.”

    WAGO got the contract because it had made significant progress with the development of a prototype that transmits the voltage in addition to the signal transmission. Pedersen continues: “The WAGO solution met PG Flow Solutions AS’s requirements to a high degree.” Therefore, WAGO was the obvious choice. PG recognized that prototype development required time, but in the end there were no unexpected delays, despite the fact that the customer wanted some changes. “Actually, we got the impression that WAGO would improve the product,” says Pedersen, especially
    with respect to the firmware for the boards.

    Our experience with WAGO was very good. We had excellent follow-up support whenever we needed help.

    Odd Sverre Pedersen
    PG Flow Solutions AS
    Tom Jonas Lauritsen of PG Flow Solutions AS appreciates the compact design of the WAGO-I/O-SYSTEM.

    Tom Jonas Lauritsen of PG Flow Solutions AS appreciates the compact design of the WAGO-I/O-SYSTEM.

    Space for User-Friendly Installation

    The fact that they are one of the smallest modules on the market was very much appreciated by PG’s skilled workers, because a small module needs less space in the control cabinet. Compared to conventional modules, the WAGO modules only need half as much space. This means that the automation technicians and control cabinet manufacturers have more space for carrying out technically challenging installations. While this was one reason the PG experts considered the WAGO components user-friendly, there was also another: WAGO provides push-in technology. They knew the installation of most of these WAGO products would be fast and efficient. In addition, pluggable components make it easier to prevent errors during wiring. Therefore, the time needed for testing automation systems and possibly fixing errors was almost completely eliminated.

    Adaptable – Even under Challenging Conditions

    In addition to the requirements that must be fulfilled regarding Ex-proofness and marine approval, it was critical for PG to develop solutions that would be modular – and this applies to the drawing phase as well as the installation! WAGO has its own programs for the configuration of I/O modules and other products. PG has a comprehensive machine manufacturing operation and typically uses an open drawing and configuration system. PG also used this tool for the configuration of the WAGO products. In this case, the configuration of the I/O modules encountered no problems, says Pedersen. “Our experience with WAGO was very good,” he says in summary. “We had excellent follow-up support whenever we needed help. And for the Norwegian organization and its parent company, this was important if significant technical help was required.”

    The combination of robust WAGO equipment and sophisticated installation by PG results in control cabinets that exceed the qualifications required for the rough conditions aboard a supply ship. The DNV-GL certification for Class D certifies that the equipment can also withstand vibrations, which occur onboard a ship traversing the North Sea under the challenging conditions normally found there.

    Author: Benjamin Böhm

    Product Overview

    8-channel digital input; 24 VDC; 3 ms
    Item no. 750-430

    8-channel digital input; 24 VDC; 3 ms

    Fieldbus Coupler ETHERNET; 3rd Generation
    Item no. 750-352

    Fieldbus Coupler ETHERNET; 3rd Generation

    4-channel analog input; 4 … 20 mA; Single-ended
    Item no. 750-455

    4-channel analog input; 4 … 20 mA; Single-ended

    Fieldbus Coupler PROFIBUS DP; 2nd Generation; 12 MBd
    Item no. 750-333

    Fieldbus Coupler PROFIBUS DP; 2nd Generation; 12 MBd

    2-channel analog input; For Pt100/RTD resistance sensors
    Item no. 750-461

    2-channel analog input; For Pt100/RTD resistance sensors

    4-channel analog output; 0 ... 10 VDC
    Item no. 750-559

    4-channel analog output; 0 ... 10 VDC

    Fieldbus Coupler PROFINET IO; 3rd Generation; Advanced
    Item no. 750-375

    Fieldbus Coupler PROFINET IO; 3rd Generation; Advanced

    2-channel analog input; 4 … 20 mA; Single-ended
    Item no. 750-466

    2-channel analog input; 4 … 20 mA; Single-ended

    2-channel analog output; 4 … 20 mA
    Item no. 750-554

    2-channel analog output; 4 … 20 mA

    4-channel analog input; 0 ... 10 VDC; Single-ended
    Item no. 750-459

    4-channel analog input; 0 ... 10 VDC; Single-ended

    WAGO at Work

    Further Customer Applications from the Area of Tank Ballast and Cargo Management

    WAGO has completed many interesting projects in the marine and offshore sectors. Learn more about the most recent ones here.

    marine_containerschiff_hafen_2000x1500.jpg

    Fill Level Measurement without Compromises

    Krohne Marine develops cargo monitoring and management systems with an international reputation. Its “Cargomaster” works with WAGO’s standard controller technology.

    marine_thor_hochtief_hubinsel_2000x1500.jpg

    Reliable Flow and Tank Management

    For monitoring and control of such important liquids as ballast and bilge water, BESI Marine Systems relies on WAGO’s solutions.

    marine_marine-platforms_african-inspiration_offshore-service-schiff_2000x1500.jpg

    Precise Monitoring

    XTronica AS builds systems for monitoring fill levels in tanks and relies on the flexible and reliable WAGO-I/O-SYSTEM 750 for them.

    Learn more

    More Marine Applications

    Whether Maritime 4.0, propulsion control or tank ballast and cargo management, WAGO offers solutions for every maritime challenge.

    marine_steuerraum_1_gettyimages-169263598_2000x1500.jpg

    Reliable Signal Processing

    Collect, condition and visualize data and, when necessary issue alarms: WAGO-equipped alarm and monitoring systems get the job done.

    marine_motorboot_segelyacht_gettyimages-556376575_2000x1500.jpg

    Ready for Whatever Comes Next

    Intelligent automation solutions also belong to future marine applications. Stay on the safe side with WAGO’s solutions.

    marine_schlepper_seil_2000x1500.jpg

    Safe around the Clock

    Proven under even the most demanding conditions, WAGO’s maintenance-free, safe solutions keep tugboats and cranes ready for action at any time.

    marine_kreuzfahrtschiff_1_2000x1500.jpg

    Safety and Comfort

    WAGO’s cost-effective, reliable connection solutions are the electrical basis for onboard amenities.