The Founding of WAGO

2020-Today

WAGO Drives the Energy Transition Forward

In challenging times, WAGO focuses even more intently on sustainable business activity and incorporates this approach into its vision, summarized by the motto: “We are the backbone of a sustainable and smart connected world.” To rise to this challenge, WAGO has established sustainability as a central goal in its corporate strategy. With its new SOLUTIONS business unit, WAGO relies on customer-specific solutions and focuses on applications that drive the energy transition. In 2021, the company broke €1 billion in sales for the first time. In the same year, Dr. Heiner Lang joined the company as its new CEO. Sven Hohorst switched to the advisory board of the WAGO Group.

Product Developments and Events from the 2020s

  • 2021: SOLUTIONS business unit established

  • 2021: WAGO breaks €1 billion in sales

  • 2021: Dr. Heiner Lang becomes CEO of the WAGO Group

  • 2021: WAGO Inline Splicing Connector with Levers

  • 2022: WAGO Compact Controller 100 for smaller automation solutions

Milestones in the 2020s

New SOLUTIONS Business Unit

With the founding of the new SOLUTIONS business unit, WAGO relies on solutions that are tailored precisely to customer requirements and applications, simultaneously saving resources, time and money through efficiency and sustainability.

Focus on the Energy Transition

With its new business unit, WAGO is expanding its portfolio to include complete system solutions for the building technology, energy distribution, infrastructure networking, mechanical and systems engineering, industrial production systems and the railway industry markets. The focus is on applications from smart energy, smart buildings and smart factories that help drive the energy transition.

WAGO Inline Splicing Connector with Levers

WAGO expands its 221 Series Splicing Connectors with a trend-setting conductor connection for all conductor types from 0.2 to 4 mm². The inline splicing connector with levers allows universal conductor termination in the feedthrough direction.

All the Benefits of the 221 Series with a Slim Design

Unparalleled simplicity, speed and reliability – that’s what the new WAGO Inline Splicing Connector stands for. WAGO's Inline Splicing Connector condenses the industry-leading 221 Series Splicing Connectors’ advantages into a slim design. Offering unsurpassed simplicity, speed and reliability, the 221 Series’ levers provide tool-free universal conductor connections and a transparent housing for confirming conductor contact at a glance. As a universal connection technology, it is not only suitable for familiar installation applications in tight spaces but also opens up many new and different ones, such as the inline connection of installation lines in distribution boxes or flying leads. It is ideal for lab and test setups or production test stands, requires no tools and provides visible confirmation of conductor contact.

From Then to Now

Get insight into other decades of WAGO corporate history here

The WAGO Story Begins

Ready for the Global Market

Spring Pressure Connection Technology Conquers the Markets

The CAGE CLAMP® Breakthrough

The Dawn of a New Era

Exciting Times

MM-17598_Unternehmenshistorie_Dekade_Intro_Picture_2010_new.jpg

WAGO Shapes the Future

Driving the Energy Transition Forward