Chemical Reactions Possible at Any Time
One thing is for certain: It is almost impossible to predict the composition of the effluents arriving in wastewater plants. Contaminations, flammable compositions or chemical reactions can occur at any time due to accidents or unauthorized discharges. These may result in outgassing, which must be classified as a hazardous atmosphere. If highly flammable liquids, such as gasoline, get into the sewer system, they will float on the surface due to their lower density. As volatile materials, they evaporate quickly; depending on their concentration, they can create a harmful or even explosive mixture. Since the vapors that are generated are often heavier than air, they inevitably collect at the lowest point of the sewer network. Therefore, the sewer network and its structures, such as enclosed storage basins for wastewater, stowage canals, pumps or inverted siphon structures, are classified as Zone 1 or Zone 2 depending on their design.