Building Lighting under Scrutiny
One such measure also carefully scrutinizes the existing lighting technology in the production facilities, even though substantial optimization had already been achieved in this sector using a new central control system. This included, among other improvements, switching off the main lighting in the production facilities during idle times. Furthermore, BMW was already taking advantage of the possibility of switching off individual phases in the three-phase current bars as needed. However, without additional technical changes to the installed current bars with traditional control gears, the savings potential was soon exhausted.
A quick glance at the lighting plan from that time demonstrated to management how far from ideal the system was – all lights had indeed been planned based on the reduction in luminosity that occurs as lights age, but, because the expenses for frequent manual adjustment would have been too high, and the technology necessary for automatic adjustment had not yet been developed, the lights were installed from the beginning with significantly over-designed luminosity. This was the only means of ensuring that the lighting intensity required by the pertinent standards would still be achieved at the predefined time for maintenance. This concept inevitably resulted in inefficient lighting, as energy consumption was unnecessarily high.
A User-Friendly and Area-Oriented Concept
The next logical step, after upgrading the central control system, was to modernize the hardware at the automation level. In fact, this required a solution that could both be installed in newly constructed production facilities that are equipped in the field with DALI and EnOcean, and also retrofitted to projects that retained the existing conventional technology. The fact that the two technologies – both old and new – could be easily combined was one reason that Jörg Tratzl, the electrical systems designer in charge, ultimately decided on components from WAGO. Another reason: the exceptionally user-friendling handling that WAGO developed for BMW for control of operating devices for lighting technology.
The new lighting distribution system not only boasts up-to-date technology, it also puts a special focus on the needs of the end customer. In contrast to the lighting distribution systems used previously, with this system, the electrical installation specialist does not have to perform any complicated programming during commissioning or during everyday work. Instead, the area-oriented software can be adapted to individual needs using only the parameter settings – made in the graphical user interface of any Internet browser. This saves time while eliminating the need for additional expertise, which significantly reduces both energy costs and the expenses associated with engineering. The basis of this system is WAGO-I/O-SYSTEM 750’s ETHERNET Controllers, which are installed in control cabinets in the production facilities with I/O modules for DALI and EnOcean, as well as standard analog/digital inputs and outputs. From there, they control each and every control gear.
This allows the lighting to be automatically dimmed based on a lighting schedule. This achieved the first noticeable savings on energy costs – while simultaneously meeting the stringent operating standards. DALI provides additional advantages: For example, instead of having to activate entire circuits, short addresses are used to control each individual light. The individual targeting this achieves allows the short addresses to be assembled into groups. Thus, virtual rooms can be depicted on the display using WAGO’s Web visualization, and – just like physical rooms – can be regulated autonomously. For BMW’s production facilities, this means that lighting can be adapted to structural modifications or building repurposing with only a few clicks of the mouse.
750 Series Ethernet Controllers:
Controllers for all prominent fieldbus systems
Expandable with the comprehensive WAGO-I/O-SYSTEM 750 product range
Extensive IT integration possibilities
Automated and Integrated Workflows
The lighting distribution boards standardized by BMW have proven themselves in more than 100 installations at a wide range of locations within this group of companies. Simple configuration of the WAGO controller via Internet browser has reduced the commissioning time for each lighting distribution board from several days to only a few seconds. Relays can be installed or removed with just a few manual operations using pluggable sockets. “This, of course, also reduces costs during ongoing operations, as maintenance can be performed much more quickly,” explains Jörg Tratzl.
Replacement of the hardware is, however, the only activity that still needs to be performed manually at BMW, stresses the electrical systems designer. “Since the WAGO ETHERNET Controllers communicate directly with the plant management software, we have been able to perfect this workflow: The exact position of defective lighting is reported, operating hours counters are reset after replacement of the components, and the brightness levels are adjusted automatically.”
Why WAGO?
- More than 30 % reduction of lighting energy
- Commissioning and adjustment without any programming
- Parameterization via Internet browser saves time and requires no additional expertise
By Jürgen Pfeifer | 2013-03-19
[{"code":"750-881","name":"Controller ETHERNET; 3rd Generation","url":"/plcs-controllers/controller-ethernet/p/750-881","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w4MDQ1NDd8aW1hZ2UvanBlZ3xhR1UxTDJobE1pOHhOalUyT1RRek56QXlPRE00TWd8MTc2ZGE1ZDRiMDc3ZjkxMmRiZmZhNTBlYWNkZDc5NThiZWRhMWUwOTczNzFhNDZhY2I2YmFmNzAwMWZhZGJjMg","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzQ2NzN8aW1hZ2UvanBlZ3xhRGMxTDJobFpDOHhOalUyT1RRek56TTFOakEyTWk4eU1EQXdYekF5TURBd01EQmxNREF3TVdObFpEWXdNREF4TURCaU5sOUVSUzVxY0djfGI4M2Y3Y2QzZjk3NmEzMWY2YTA1ZDZkY2ViNzIyOTNlNDYzNzNmMmM2M2ExMGVjOTdhOTNjZTY5N2MyZGQxMjU","altText":"2000_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzQ2NzN8aW1hZ2UvanBlZ3xhRGMxTDJobFpDOHhOalUyT1RRek56TTFOakEyTWk4eU1EQXdYekF5TURBd01EQmxNREF3TVdObFpEWXdNREF4TURCaU5sOUVSUzVxY0djfGI4M2Y3Y2QzZjk3NmEzMWY2YTA1ZDZkY2ViNzIyOTNlNDYzNzNmMmM2M2ExMGVjOTdhOTNjZTY5N2MyZGQxMjU","altText":"2000_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzQ2NzN8aW1hZ2UvanBlZ3xhRGMxTDJobFpDOHhOalUyT1RRek56TTFOakEyTWk4eU1EQXdYekF5TURBd01EQmxNREF3TVdObFpEWXdNREF4TURCaU5sOUVSUzVxY0djfGI4M2Y3Y2QzZjk3NmEzMWY2YTA1ZDZkY2ViNzIyOTNlNDYzNzNmMmM2M2ExMGVjOTdhOTNjZTY5N2MyZGQxMjU","altText":"2000_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzQ2NzN8aW1hZ2UvanBlZ3xhRGMxTDJobFpDOHhOalUyT1RRek56TTFOakEyTWk4eU1EQXdYekF5TURBd01EQmxNREF3TVdObFpEWXdNREF4TURCaU5sOUVSUzVxY0djfGI4M2Y3Y2QzZjk3NmEzMWY2YTA1ZDZkY2ViNzIyOTNlNDYzNzNmMmM2M2ExMGVjOTdhOTNjZTY5N2MyZGQxMjU","altText":"2000_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzQ2NzN8aW1hZ2UvanBlZ3xhRE0wTDJobU1TOHhOalUyT1RRek56UTROekV6TkM4eE5EUXdYekF5TURBd01EQmxNREF3TVdObFpEWXdNREF4TURCaU5sOUVSUzVxY0djfGJmOTJkMWE4NDk3OWRmY2Y2OTc1NWFhNGIzOTc0NzM3OTJmOTMwMTU4OTg2OWE1ZTNhZDQ0NmJiNTliNDBkNTM","altText":"1440_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzQ2NzN8aW1hZ2UvanBlZ3xhREEwTDJobU9DOHhOalUyT1RRek56WTRNemMwTWk4eE1qZ3dYekF5TURBd01EQmxNREF3TVdObFpEWXdNREF4TURCaU5sOUVSUzVxY0djfGNlM2M0YTZlOGIzYmVhN2MwOWU1MThhMmM5MTE1ODRmZTY3OTg2MGEwNGEzY2Y2ZjIyMTE0OWViOTJjZTJmMTc","altText":"1280_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5OTkwNnxpbWFnZS9qcGVnfGFERXpMMmhtWlM4eE5qVTJPVFF6TnpneE5EZ3hOQzh4TURJMFh6QXlNREF3TURCbE1EQXdNV05sWkRZd01EQXhNREJpTmw5RVJTNXFjR2N8ODU1ZjY2M2MyODRlMDJjNDE1ZTNmYjQ3YzA2MGYwOGEwNWUzMDZhZDcyZjQwZmY2NWJlM2Q1Yzc0YmNkYzY3Yg","altText":"1024_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2NzY2NHxpbWFnZS9qcGVnfGFHTXlMMmhpTWk4eE5qVTJPVFF6T0RBM05qazFPQzgzTmpoZk1ESXdNREF3TUdVd01EQXhZMlZrTmpBd01ERXdNR0kyWDBSRkxtcHdad3wyMjllZGU2MWNiNjQ1ZTJiYTRiY2M1MzgwZWI4ZjQwZWI3MGZkMjM0ZDFmNDg5YzE4ZTBkODk0OGEyN2RjMzk3","altText":"768_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNTc4NXxpbWFnZS9qcGVnfGFHSXhMMmhoWmk4eE5qVTJPVFF6T0RFME1qUTVOQzgwT0RCZk1ESXdNREF3TUdVd01EQXhZMlZrTmpBd01ERXdNR0kyWDBSRkxtcHdad3xmMjJlMmM1YzVkYmM5ZGIyZjYwNjY4YWFkOGJlNWExNzFkZTliNjUyNGZkNjQwODA4ZDMyOGFiMTUyYzExZTVh","altText":"480_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyOTQ5fGltYWdlL2pwZWd8YUdVekwyaGhOUzh4TmpVMk9UUXpPRFF3TkRZek9DOHlNREJmTURJd01EQXdNR1V3TURBeFkyVmtOakF3TURFd01HSTJYMFJGTG1wd1p3fDkxNmVjZDFkMjI4YTcyYTk3NmYzZDllYjg0YWE0MjA3ZjQzNTAxOGY4MDI3MmZmMzU3OThlNGQwYjZiYTZkNTA","altText":"200_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyOTQ5fGltYWdlL2pwZWd8YUdVekwyaGhOUzh4TmpVMk9UUXpPRFF3TkRZek9DOHlNREJmTURJd01EQXdNR1V3TURBeFkyVmtOakF3TURFd01HSTJYMFJGTG1wd1p3fDkxNmVjZDFkMjI4YTcyYTk3NmYzZDllYjg0YWE0MjA3ZjQzNTAxOGY4MDI3MmZmMzU3OThlNGQwYjZiYTZkNTA","altText":"200_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyOTQ5fGltYWdlL2pwZWd8YUdVekwyaGhOUzh4TmpVMk9UUXpPRFF3TkRZek9DOHlNREJmTURJd01EQXdNR1V3TURBeFkyVmtOakF3TURFd01HSTJYMFJGTG1wd1p3fDkxNmVjZDFkMjI4YTcyYTk3NmYzZDllYjg0YWE0MjA3ZjQzNTAxOGY4MDI3MmZmMzU3OThlNGQwYjZiYTZkNTA","altText":"200_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000e0001ced6000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000e0001ced6000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0NTg0fGltYWdlL2pwZWd8YURrMEwyZzVOeTh4TmpVMk9UUXpPRGcyTXpNNU1DOHhNakJmTURJd01EQXdNR1V3TURBeFkyVmtOakF3TURFd01HSTJYMFJGTG1wd1p3fGFmMDE5OWRjZjM4MjVhZjY1NjYwYWFkYjcyM2NjMzBhY2JmNzkzZjlhMDY5NjY5OGU1ZTk4MmVhMTExMTBkYWM","altText":"120_0200000e0001ced6000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000e0001ced6000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-881","stock":null,"url":"/plcs-controllers/controller-ethernet/p/750-881","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["ec000236","fieldbus system","fieldbus components","io controller","fieldbus controller","distributed i/o","ip20","remote i/o","bus controller","750-881","wago io system","controller","programmable","codesys","fieldbus","plc","cpu","pfc","master","ethernet","27-24-26-07","head station","modbus","fieldbus technology","io system","gateway"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821086826","primaryCategoryName":"Controller","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":true,"status":"CANCELLED","cancelDate":1576364400000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["Controller"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Controller ETHERNET","primaryImageUrl":null,"productGroup":null,"nameEn":"Controller ETHERNET; 3rd Generation","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"7500881","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Controller 750","productColor":null,"downloadData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"videos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-880","name":"Controller ETHERNET; 3rd Generation; SD Card Slot","url":"/plcs-controllers/controller-ethernet/p/750-880","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w4NzkxMDR8aW1hZ2UvanBlZ3xhR0l5TDJnME1pOHhOalUzTVRFNE9UVTVNakE1TkF8MTVjNTk2MTc3NjYyODBkMzRiYmRlYzc4MjUzY2RhNzY3MzRjZThjNDQ4MGJhMjE4Yjc3NDA1ZjI5Y2RkMTAzMw","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDA1MTJ8aW1hZ2UvanBlZ3xhRGRrTDJnMFppOHhOalUzTVRFNE9Ua3hPVGMzTkM4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbE5qa3dNREF4TURCaU5sOUVSUzVxY0djfDkwYWJiYzI1YWE3MmRiZDJkZGRkMDJhOTA4NjI2NWI0MWZjZjdiZjU0NDZiYzAyY2M1NWZhY2Q4MTc0OTcxNDQ","altText":"2000_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDA1MTJ8aW1hZ2UvanBlZ3xhRGRrTDJnMFppOHhOalUzTVRFNE9Ua3hPVGMzTkM4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbE5qa3dNREF4TURCaU5sOUVSUzVxY0djfDkwYWJiYzI1YWE3MmRiZDJkZGRkMDJhOTA4NjI2NWI0MWZjZjdiZjU0NDZiYzAyY2M1NWZhY2Q4MTc0OTcxNDQ","altText":"2000_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDA1MTJ8aW1hZ2UvanBlZ3xhRGRrTDJnMFppOHhOalUzTVRFNE9Ua3hPVGMzTkM4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbE5qa3dNREF4TURCaU5sOUVSUzVxY0djfDkwYWJiYzI1YWE3MmRiZDJkZGRkMDJhOTA4NjI2NWI0MWZjZjdiZjU0NDZiYzAyY2M1NWZhY2Q4MTc0OTcxNDQ","altText":"2000_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDA1MTJ8aW1hZ2UvanBlZ3xhRGRrTDJnMFppOHhOalUzTVRFNE9Ua3hPVGMzTkM4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbE5qa3dNREF4TURCaU5sOUVSUzVxY0djfDkwYWJiYzI1YWE3MmRiZDJkZGRkMDJhOTA4NjI2NWI0MWZjZjdiZjU0NDZiYzAyY2M1NWZhY2Q4MTc0OTcxNDQ","altText":"2000_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDA1MTJ8aW1hZ2UvanBlZ3xhR1U1TDJoaU15OHhOalUzTVRFNU1ERTBPVEUxTUM4eE5EUXdYekF5TURBd01EQm1NREF3TXpKbE5qa3dNREF4TURCaU5sOUVSUzVxY0djfDNmMzgzYmIxODE0ODhkNmIwYjAxYzgyNDU2MjMxNDEyYWRlZTlkZDUyYzQ4ZjBmNTUwNTMwMWUwZmU1YTE5NjI","altText":"1440_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDA1MTJ8aW1hZ2UvanBlZ3xhRGN3TDJoaFpDOHhOalUzTVRFNU1ETXhNams1TUM4eE1qZ3dYekF5TURBd01EQm1NREF3TXpKbE5qa3dNREF4TURCaU5sOUVSUzVxY0djfGY5ODU4NGZlZjI5MGY5MWJkNTdlOGE2NTA2YWI3ZTY0NDI4MTljNDcwZDFjNmFhYWZkZDQ4ZTM4ZjE3NjBlNjU","altText":"1280_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMDM3MzJ8aW1hZ2UvanBlZ3xhR0l5TDJoaE5pOHhOalUzTVRFNU1EVXdPVFU1T0M4eE1ESTBYekF5TURBd01EQm1NREF3TXpKbE5qa3dNREF4TURCaU5sOUVSUzVxY0djfGRiYjFhYmZkMzg2NWU0MDUyMzBjNGExMjhiYWUyYjUxNTc4ZjBkODc1OGJmOWU4NjM4ZGMxNGYzM2IxMjBhMjU","altText":"1024_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w3MDE5MHxpbWFnZS9qcGVnfGFESXhMMmc1Wmk4eE5qVTNNVEU1TURjM01UYzBNaTgzTmpoZk1ESXdNREF3TUdZd01EQXpNbVUyT1RBd01ERXdNR0kyWDBSRkxtcHdad3wyMDU4MGVlNjA1OTQ0YjRlNmZhYmM4ZTA3ZjlmMWYyNjFkMmIxZTllMDMzODg0MDk0ODIxZjgwODRmYWQ1MTZk","altText":"768_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNTk3OXxpbWFnZS9qcGVnfGFHRTNMMmcwWkM4eE5qVTNNVEU1TVRBek16ZzROaTgwT0RCZk1ESXdNREF3TUdZd01EQXpNbVUyT1RBd01ERXdNR0kyWDBSRkxtcHdad3xjZTMwODY1OTE1YjRjZDYxNDM2YzRjYjRlMzJjMzI5OWE3ZGYwYzkxYWFjMTM4NmZiZjFmNmM4ZDE2NTI4MzVh","altText":"480_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyNjMxfGltYWdlL2pwZWd8YURreEwyZzBPUzh4TmpVM01URTVNVEU1TnpjeU5pOHlNREJmTURJd01EQXdNR1l3TURBek1tVTJPVEF3TURFd01HSTJYMFJGTG1wd1p3fDg2YzI5ODM4ZGI5NmQ0YjNlZGI1MWRhZDI0MGQzZTVmMWNmZWEzODNhYjMyNDIxYWQ0Y2YyZGYzZDFhNTIxMjc","altText":"200_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyNjMxfGltYWdlL2pwZWd8YURreEwyZzBPUzh4TmpVM01URTVNVEU1TnpjeU5pOHlNREJmTURJd01EQXdNR1l3TURBek1tVTJPVEF3TURFd01HSTJYMFJGTG1wd1p3fDg2YzI5ODM4ZGI5NmQ0YjNlZGI1MWRhZDI0MGQzZTVmMWNmZWEzODNhYjMyNDIxYWQ0Y2YyZGYzZDFhNTIxMjc","altText":"200_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyNjMxfGltYWdlL2pwZWd8YURreEwyZzBPUzh4TmpVM01URTVNVEU1TnpjeU5pOHlNREJmTURJd01EQXdNR1l3TURBek1tVTJPVEF3TURFd01HSTJYMFJGTG1wd1p3fDg2YzI5ODM4ZGI5NmQ0YjNlZGI1MWRhZDI0MGQzZTVmMWNmZWEzODNhYjMyNDIxYWQ0Y2YyZGYzZDFhNTIxMjc","altText":"200_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00032e69000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000f00032e69000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0Mjk2fGltYWdlL2pwZWd8YURjNUwyZ3pNaTh4TmpVM01URTVNVGd5TURNeE9DOHhNakJmTURJd01EQXdNR1l3TURBek1tVTJPVEF3TURFd01HSTJYMFJGTG1wd1p3fGM4NDY5Mjg2ZmNhYWZmMjkyMzBlZWYwYWYwNzE0MGY0YzE0ODQ0ZjZkM2U1NmQ0MWMzZWY4ZTliZjUwODExMWQ","altText":"120_0200000f00032e69000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000f00032e69000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-880","stock":null,"url":"/plcs-controllers/controller-ethernet/p/750-880","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["ec000236","fieldbus system","fieldbus components","io controller","fieldbus controller","distributed i/o","ip20","750-880","remote i/o","bus controller","wago io system","controller","codesys","programmable","fieldbus","plc","cpu","pfc","master","ethernet","27-24-26-07","head station","modbus","fieldbus technology","io system","gateway"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821134053","primaryCategoryName":"Controller","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":true,"status":"CANCELLED","cancelDate":1576364400000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["Controller"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Controller ETHERNET","primaryImageUrl":null,"productGroup":null,"nameEn":"Controller ETHERNET; 3rd Generation; SD Card Slot","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"7500880","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Controller 750","productColor":null,"downloadData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"videos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-852","name":"Controller ETHERNET; 3rd Generation; ECO","url":"/controller-ethernet/p/750-852","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w4MjQ5ODR8aW1hZ2UvanBlZ3xhR1l6TDJnMFlTOHhOalUwT1RnNE9ETTVNekkwTmd8Yzk0ZDZkMjIxODkyNDk1NGIxY2Q5ZDI0OThkMTBkYjVkZDE0ZWI0YTRkZTMxZjIxZWE2NjgwOTU1NzM3MDViMQ","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzkzNjV8aW1hZ2UvanBlZ3xhRFUxTDJnellTOHhOalUwT1RnNE9EZzFNVGs1T0M4eU1EQXdYekF5TURBd01ERTRNREF3TVRWak0yRXdNREF4TURCaU5sOUVSUzVxY0djfDg5Mzg4NjVkZjI2YzY4NWQ1ZjRhNjMyZjQ3OTY0Yjc1OWRhODY5ZTMzYjU4N2ExMjI2MjBjNWYyNDgyYzIwYjY","altText":"2000_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzkzNjV8aW1hZ2UvanBlZ3xhRFUxTDJnellTOHhOalUwT1RnNE9EZzFNVGs1T0M4eU1EQXdYekF5TURBd01ERTRNREF3TVRWak0yRXdNREF4TURCaU5sOUVSUzVxY0djfDg5Mzg4NjVkZjI2YzY4NWQ1ZjRhNjMyZjQ3OTY0Yjc1OWRhODY5ZTMzYjU4N2ExMjI2MjBjNWYyNDgyYzIwYjY","altText":"2000_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzkzNjV8aW1hZ2UvanBlZ3xhRFUxTDJnellTOHhOalUwT1RnNE9EZzFNVGs1T0M4eU1EQXdYekF5TURBd01ERTRNREF3TVRWak0yRXdNREF4TURCaU5sOUVSUzVxY0djfDg5Mzg4NjVkZjI2YzY4NWQ1ZjRhNjMyZjQ3OTY0Yjc1OWRhODY5ZTMzYjU4N2ExMjI2MjBjNWYyNDgyYzIwYjY","altText":"2000_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzkzNjV8aW1hZ2UvanBlZ3xhRFUxTDJnellTOHhOalUwT1RnNE9EZzFNVGs1T0M4eU1EQXdYekF5TURBd01ERTRNREF3TVRWak0yRXdNREF4TURCaU5sOUVSUzVxY0djfDg5Mzg4NjVkZjI2YzY4NWQ1ZjRhNjMyZjQ3OTY0Yjc1OWRhODY5ZTMzYjU4N2ExMjI2MjBjNWYyNDgyYzIwYjY","altText":"2000_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzkzNjV8aW1hZ2UvanBlZ3xhREV6TDJneE5DOHhOalUwT1RnNE9UQTBPRFl3Tmk4eE5EUXdYekF5TURBd01ERTRNREF3TVRWak0yRXdNREF4TURCaU5sOUVSUzVxY0djfDMzYjRlMGQzYjY0MmEyYmRmODhjZDkzMzUxNjg1ZTNlYWNiYTI3ZGI3NjY3ZDE5YWRjYjhjNzA5YzZiYWYxNzA","altText":"1440_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzkzNjV8aW1hZ2UvanBlZ3xhR1F5TDJneE55OHhOalUwT1RnNE9URTNPVFkzT0M4eE1qZ3dYekF5TURBd01ERTRNREF3TVRWak0yRXdNREF4TURCaU5sOUVSUzVxY0djfDgwZDBiMWFmMDg2N2FiMWE1ZDEzYzlkMTJhOTQyMmFjYTcyM2I2Mjc3NDU3ZjNlMDQ5MGM1YmUzODk3Y2RkNmE","altText":"1280_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMDM2MDB8aW1hZ2UvanBlZ3xhR0V6TDJneFpTOHhOalUwT1RnNE9UTTNOakk0Tmk4eE1ESTBYekF5TURBd01ERTRNREF3TVRWak0yRXdNREF4TURCaU5sOUVSUzVxY0djfDIwOTdkYjMxYmE2ODMxYTNkNDY5YmZjMjFkYzUxZTEwZTkzMzM3NjI4NjY0Njc4M2I1YmZmODVjYjc4MWNiMjE","altText":"1024_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w3MTA0M3xpbWFnZS9qcGVnfGFHSXpMMmd5TVM4eE5qVTBPVGc0T1RRME1UZ3lNaTgzTmpoZk1ESXdNREF3TVRnd01EQXhOV016WVRBd01ERXdNR0kyWDBSRkxtcHdad3wzNzc0ODE4ZTlhZDg0MjUxMGM2NmI0MWI1YjBjYTY1NTFhZjg1MmIwYzdmZGQwYTZjMjkwOTM5ZGZjMGY2NWRj","altText":"768_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNzk4MXxpbWFnZS9qcGVnfGFEY3lMMmd5TlM4eE5qVTBPVGc0T1RVM01qZzVOQzgwT0RCZk1ESXdNREF3TVRnd01EQXhOV016WVRBd01ERXdNR0kyWDBSRkxtcHdad3xmYTkwMDE0YmIxZWIxYmU1N2VjNzUwNDk5MDRkZWE5ODgzZjVjNmQ4NGIwM2NiZDNkODA3M2QyNzNmOWE2MGUz","altText":"480_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTcxfGltYWdlL2pwZWd8YURneEwyZ3lZaTh4TmpVME9UZzRPVGN3TXprMk5pOHlNREJmTURJd01EQXdNVGd3TURBeE5XTXpZVEF3TURFd01HSTJYMFJGTG1wd1p3fDQxYzYxNzdhMzg3YTgyYWYzZjM1NGUwNDcwYzNkNTM3NjQ5ZmYxZDA1OTRlZjdkZjY4OTIzNjA3ZTNiYWU2YTI","altText":"200_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTcxfGltYWdlL2pwZWd8YURneEwyZ3lZaTh4TmpVME9UZzRPVGN3TXprMk5pOHlNREJmTURJd01EQXdNVGd3TURBeE5XTXpZVEF3TURFd01HSTJYMFJGTG1wd1p3fDQxYzYxNzdhMzg3YTgyYWYzZjM1NGUwNDcwYzNkNTM3NjQ5ZmYxZDA1OTRlZjdkZjY4OTIzNjA3ZTNiYWU2YTI","altText":"200_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTcxfGltYWdlL2pwZWd8YURneEwyZ3lZaTh4TmpVME9UZzRPVGN3TXprMk5pOHlNREJmTURJd01EQXdNVGd3TURBeE5XTXpZVEF3TURFd01HSTJYMFJGTG1wd1p3fDQxYzYxNzdhMzg3YTgyYWYzZjM1NGUwNDcwYzNkNTM3NjQ5ZmYxZDA1OTRlZjdkZjY4OTIzNjA3ZTNiYWU2YTI","altText":"200_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200001800015c3a000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200001800015c3a000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0OTI2fGltYWdlL2pwZWd8YUdabEwyaGpZeTh4TmpVME9UZzVNREk1TXpjNU1DOHhNakJmTURJd01EQXdNVGd3TURBeE5XTXpZVEF3TURFd01HSTJYMFJGTG1wd1p3fDNmYmIxNzY0OThiNjA5ZDUyYTk0OWM1ZmIzMjFkYmE1ZDEzNWVmNDkzNTFjYWU0YmI4MmI2OTViNGRlYjFjZDE","altText":"120_0200001800015c3a000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200001800015c3a000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-852","stock":null,"url":"/controller-ethernet/p/750-852","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["ec000236","fieldbus system","fieldbus components","io controller","fieldbus controller","ip20","distributed i/o","remote i/o","bus controller","wago io system","controller","codesys","programmable","fieldbus","plc","cpu","pfc","master","ethernet","27-24-26-07","head station","modbus","fieldbus technology","750-852","io system","gateway"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821753940","primaryCategoryName":null,"numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":false,"status":"INACTIVE","cancelDate":1576364400000,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":null,"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":false,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Controller ETHERNET","primaryImageUrl":null,"productGroup":null,"nameEn":"Controller ETHERNET; 3rd Generation; ECO","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"7500852","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Controller 750","productColor":null,"downloadData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"videos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-842","name":"Controller ETHERNET; 1st Generation","url":"/plcs-controllers/controller-ethernet/p/750-842","description":null,"purchasable":true,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w1ODg0NTZ8aW1hZ2UvanBlZ3xhR1kwTDJnM1l5OHhOalUxTnpZMk9USTFNekUxTUF8YmNjMTI0NTdhMTgyYmQ5MTA5YjA2ODg3ZDNjNjE3NmFkZGZlMGJiN2ZkNDExN2VjM2M2ODE0MjMyMzk4MzJiOA","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzk4M3xpbWFnZS9qcGVnfGFHWm1MMmcyWWk4eE5qVTFOelkyT1RjME5EWTNNQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwTTJVd01EQXhNREJpTmw5RVJTNXFjR2N8MDM2M2RmNTlkZTJlY2E5ZjMxNjc0NDJmNmE0ZjI0NDc1Njg3MjRkMTkyZTA5ZDU2ZTk3NWUzZWJlODIwYjkyYQ","altText":"2000_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzk4M3xpbWFnZS9qcGVnfGFHWm1MMmcyWWk4eE5qVTFOelkyT1RjME5EWTNNQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwTTJVd01EQXhNREJpTmw5RVJTNXFjR2N8MDM2M2RmNTlkZTJlY2E5ZjMxNjc0NDJmNmE0ZjI0NDc1Njg3MjRkMTkyZTA5ZDU2ZTk3NWUzZWJlODIwYjkyYQ","altText":"2000_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzk4M3xpbWFnZS9qcGVnfGFHWm1MMmcyWWk4eE5qVTFOelkyT1RjME5EWTNNQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwTTJVd01EQXhNREJpTmw5RVJTNXFjR2N8MDM2M2RmNTlkZTJlY2E5ZjMxNjc0NDJmNmE0ZjI0NDc1Njg3MjRkMTkyZTA5ZDU2ZTk3NWUzZWJlODIwYjkyYQ","altText":"2000_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzk4M3xpbWFnZS9qcGVnfGFHWm1MMmcyWWk4eE5qVTFOelkyT1RjME5EWTNNQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwTTJVd01EQXhNREJpTmw5RVJTNXFjR2N8MDM2M2RmNTlkZTJlY2E5ZjMxNjc0NDJmNmE0ZjI0NDc1Njg3MjRkMTkyZTA5ZDU2ZTk3NWUzZWJlODIwYjkyYQ","altText":"2000_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzk4M3xpbWFnZS9qcGVnfGFEazNMMmcyT0M4eE5qVTFOelkyT1RnME1qazNOQzh4TkRRd1h6QXlNREF3TURCak1EQXdNVEEwTTJVd01EQXhNREJpTmw5RVJTNXFjR2N8YjQ3MjUyMjM4YTA1YzZmZWY0YTIxZjIxMWEyNGIyYTgzYjQzYTU5ZGFkOTg4ZGIyMjg0YWE4YTJmZjcxMmIzOQ","altText":"1440_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzk4M3xpbWFnZS9qcGVnfGFEUXdMMmc1TXk4eE5qVTFOelkzTURBd05qZ3hOQzh4TWpnd1h6QXlNREF3TURCak1EQXdNVEEwTTJVd01EQXhNREJpTmw5RVJTNXFjR2N8YmM2NzVkNGUzMzNkNmY2NjI0OTczN2E4MjcyZmEyYTE5MGNmMzQ4ZDgxMDBjNGZlNGQ0YjM4NjE0ZTUwMjA0Zg","altText":"1280_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w3MTQ5OHxpbWFnZS9qcGVnfGFEWTNMMmc1WVM4eE5qVTFOelkzTURJek5qRTVNQzh4TURJMFh6QXlNREF3TURCak1EQXdNVEEwTTJVd01EQXhNREJpTmw5RVJTNXFjR2N8N2ExYzJiNTNkMDJhOWM0NWI1ZTY5MTVjNDYwMDQzYTZjYmExNDlhYjQxZTc1YWUwYzU1NjIyNDNmOTM5YTQyOA","altText":"1024_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0Nzg1NXxpbWFnZS9qcGVnfGFHWTNMMmhoTkM4eE5qVTFOelkzTURVMk16ZzNNQzgzTmpoZk1ESXdNREF3TUdNd01EQXhNRFF6WlRBd01ERXdNR0kyWDBSRkxtcHdad3w3OWRlY2ViY2M4OGQyNGQ0MmY0NmFkZTMzOWFiNDA0MDIyMGEyZmY4MDdmOWM4NzQ5OWYyM2RjMDk1MjkyYmE1","altText":"768_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyNDgzNXxpbWFnZS9qcGVnfGFHSTJMMmhoT0M4eE5qVTFOelkzTURZNU5EazBNaTgwT0RCZk1ESXdNREF3TUdNd01EQXhNRFF6WlRBd01ERXdNR0kyWDBSRkxtcHdad3w5YjA1OGJmMGE0MTEwMmE3YWQyZTQ0MmIxMDk2YTc4MTk1MzU5NDEzMTZjMWZjMWEzMzBjMDY1ZGQ2Mzk2Yzhh","altText":"480_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMTcxfGltYWdlL2pwZWd8YURnMUwyaGlNaTh4TmpVMU56WTNNRGsxTnpBNE5pOHlNREJmTURJd01EQXdNR013TURBeE1EUXpaVEF3TURFd01HSTJYMFJGTG1wd1p3fDE1MzUzZTA3MDAzYTdiNTJlZTkyZThmNjUwMmVhZDAzNmJmZDJiODQyMTk2Zjg5ZDg4YzEyY2U4OWM3MjUzY2M","altText":"200_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMTcxfGltYWdlL2pwZWd8YURnMUwyaGlNaTh4TmpVMU56WTNNRGsxTnpBNE5pOHlNREJmTURJd01EQXdNR013TURBeE1EUXpaVEF3TURFd01HSTJYMFJGTG1wd1p3fDE1MzUzZTA3MDAzYTdiNTJlZTkyZThmNjUwMmVhZDAzNmJmZDJiODQyMTk2Zjg5ZDg4YzEyY2U4OWM3MjUzY2M","altText":"200_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMTcxfGltYWdlL2pwZWd8YURnMUwyaGlNaTh4TmpVMU56WTNNRGsxTnpBNE5pOHlNREJmTURJd01EQXdNR013TURBeE1EUXpaVEF3TURFd01HSTJYMFJGTG1wd1p3fDE1MzUzZTA3MDAzYTdiNTJlZTkyZThmNjUwMmVhZDAzNmJmZDJiODQyMTk2Zjg5ZDg4YzEyY2U4OWM3MjUzY2M","altText":"200_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000c0001043e000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000c0001043e000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMjYyfGltYWdlL2pwZWd8YUdJeUwyaGxaQzh4TmpVMU56WTNNVFkzTnprNE1pOHhNakJmTURJd01EQXdNR013TURBeE1EUXpaVEF3TURFd01HSTJYMFJGTG1wd1p3fGJkODFmMWI1OTQ0YmE5ZmUzNTM4NWY4MGRmNzQ5ZGNiMTg2ZDFhMGEwNzRkODFmYzFiMjZiMjBmNTU3MTg3MWY","altText":"120_0200000c0001043e000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000c0001043e000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-842","stock":null,"url":"/plcs-controllers/controller-ethernet/p/750-842","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["ec000236","fieldbus system","fieldbus components","io controller","fieldbus controller","ip20","distributed i/o","remote i/o","bus controller","750-842","wago io system","controller","programmable","codesys","fieldbus","plc","cpu","pfc","master","27-24-26-07","ethernet","head station","modbus","fieldbus technology","io system","gateway"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4045454527198","primaryCategoryName":"Controller","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":false,"status":"RELEASED","cancelDate":null,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["Controller"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Controller ETHERNET","primaryImageUrl":null,"productGroup":null,"nameEn":"Controller ETHERNET; 1st Generation","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"51189365","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Controller 750","productColor":null,"downloadData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"videos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-882","name":"Controller ETHERNET; 3rd Generation; Media Redundancy","url":"/plcs-controllers/controller-ethernet/p/750-882","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w4MTAyODV8aW1hZ2UvanBlZ3xhR0l4TDJneU5DOHhOalUzTmpZeU56STBOVEE0Tmd8ZDdhMTk4YzZkY2FiMmY3NjIzYzU2Zjc3Njg3ZmY0NDdkOWY4MDEzNzcxNGFhMmU3YTNjNGZkYmNiOTk2ZjNjZg","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzY4NDl8aW1hZ2UvanBlZ3xhRGhoTDJneFpDOHhOalUzTmpZeU56UTNORFEyTWk4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbU9ETXdNREF4TURCaU5sOUVSUzVxY0djfDFmYzBkYzkzZWY5ODlkNTc3ZDMwYzc0NmM3YzMwOTNhOTIzY2IyNGU3OGMxMTg2ZmI3MzRmYTg0N2FjYmIxN2I","altText":"2000_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzY4NDl8aW1hZ2UvanBlZ3xhRGhoTDJneFpDOHhOalUzTmpZeU56UTNORFEyTWk4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbU9ETXdNREF4TURCaU5sOUVSUzVxY0djfDFmYzBkYzkzZWY5ODlkNTc3ZDMwYzc0NmM3YzMwOTNhOTIzY2IyNGU3OGMxMTg2ZmI3MzRmYTg0N2FjYmIxN2I","altText":"2000_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzY4NDl8aW1hZ2UvanBlZ3xhRGhoTDJneFpDOHhOalUzTmpZeU56UTNORFEyTWk4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbU9ETXdNREF4TURCaU5sOUVSUzVxY0djfDFmYzBkYzkzZWY5ODlkNTc3ZDMwYzc0NmM3YzMwOTNhOTIzY2IyNGU3OGMxMTg2ZmI3MzRmYTg0N2FjYmIxN2I","altText":"2000_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzY4NDl8aW1hZ2UvanBlZ3xhRGhoTDJneFpDOHhOalUzTmpZeU56UTNORFEyTWk4eU1EQXdYekF5TURBd01EQm1NREF3TXpKbU9ETXdNREF4TURCaU5sOUVSUzVxY0djfDFmYzBkYzkzZWY5ODlkNTc3ZDMwYzc0NmM3YzMwOTNhOTIzY2IyNGU3OGMxMTg2ZmI3MzRmYTg0N2FjYmIxN2I","altText":"2000_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzY4NDl8aW1hZ2UvanBlZ3xhR0k1TDJneE5pOHhOalUzTmpZeU56WTNNVEEzTUM4eE5EUXdYekF5TURBd01EQm1NREF3TXpKbU9ETXdNREF4TURCaU5sOUVSUzVxY0djfDFiODY1ZjQyOWMxZGQyZjA3ZDM0NzNjNTEyYTM5M2IxNTJjZDBhNzMwYmU1ZmU4M2IwYTc3MzU4MWEzZTlmM2E","altText":"1440_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMzY4NDl8aW1hZ2UvanBlZ3xhR0ZoTDJneE1DOHhOalUzTmpZeU56Z3dNakUwTWk4eE1qZ3dYekF5TURBd01EQm1NREF3TXpKbU9ETXdNREF4TURCaU5sOUVSUzVxY0djfGQzZDg3ZDUwYjYzNDMwZDhlMjM1ODEwNTlmOGFmYzlhZWZmMTViOTM2OGJhOTllZDA4MzYwMmFkZGYyZTQ2Njk","altText":"1280_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMDE4MzB8aW1hZ2UvanBlZ3xhRGRtTDJnelpTOHhOalUzTmpZeU9EQTJOREk0Tmk4eE1ESTBYekF5TURBd01EQm1NREF3TXpKbU9ETXdNREF4TURCaU5sOUVSUzVxY0djfGZlYWZlYWJiZGU5ZDJkODhiYTdjMmQ3NWZhMjI4MWVkMTBkMjhhNWExN2M5Yjc1NjVkOGQzODA3NTA2NGQ4MzI","altText":"1024_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w2OTcxNnxpbWFnZS9qcGVnfGFETmxMMmcwTWk4eE5qVTNOall5T0RFNU5UTTFPQzgzTmpoZk1ESXdNREF3TUdZd01EQXpNbVk0TXpBd01ERXdNR0kyWDBSRkxtcHdad3w1NDM5ZjhlNzYxZDIwMTY3N2MxMzY0MzBhM2EwZmQyYjliYTE4YTViYzU3Y2ZjYWYyMmQ5ZmNkM2E0MzkxN2Nj","altText":"768_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzNjk2NXxpbWFnZS9qcGVnfGFEQmpMMmcwWXk4eE5qVTNOall5T0RRMU56VXdNaTgwT0RCZk1ESXdNREF3TUdZd01EQXpNbVk0TXpBd01ERXdNR0kyWDBSRkxtcHdad3wyMDQzNzMwZDkzZjhkYWRkMzAxZmU1MGZiNThkNGQ4YmIzZDFhNzU3NGQ3Yzg2MTY1M2Y3M2QyMWRlZDUwNTRh","altText":"480_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMDY0fGltYWdlL2pwZWd8YUdSa0wyZzFNaTh4TmpVM05qWXlPRFkxTkRFeE1DOHlNREJmTURJd01EQXdNR1l3TURBek1tWTRNekF3TURFd01HSTJYMFJGTG1wd1p3fDVjNmM3NmU2YzVhMGM1MTU2NjExZjRiN2ZiM2FlNzg2YzUyZTEyMzcyNzEzZmQxZTM3ZWVmNmNhYTUyYmM4MTY","altText":"200_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMDY0fGltYWdlL2pwZWd8YUdSa0wyZzFNaTh4TmpVM05qWXlPRFkxTkRFeE1DOHlNREJmTURJd01EQXdNR1l3TURBek1tWTRNekF3TURFd01HSTJYMFJGTG1wd1p3fDVjNmM3NmU2YzVhMGM1MTU2NjExZjRiN2ZiM2FlNzg2YzUyZTEyMzcyNzEzZmQxZTM3ZWVmNmNhYTUyYmM4MTY","altText":"200_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMDY0fGltYWdlL2pwZWd8YUdSa0wyZzFNaTh4TmpVM05qWXlPRFkxTkRFeE1DOHlNREJmTURJd01EQXdNR1l3TURBek1tWTRNekF3TURFd01HSTJYMFJGTG1wd1p3fDVjNmM3NmU2YzVhMGM1MTU2NjExZjRiN2ZiM2FlNzg2YzUyZTEyMzcyNzEzZmQxZTM3ZWVmNmNhYTUyYmM4MTY","altText":"200_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000f00032f83000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000f00032f83000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0ODE4fGltYWdlL2pwZWd8YURobUwyaGhaUzh4TmpVM05qWXlPVEl4TVRFMk5pOHhNakJmTURJd01EQXdNR1l3TURBek1tWTRNekF3TURFd01HSTJYMFJGTG1wd1p3fGNkYzFkMjAwZjY5MTQxYTMyMTBmNzBiYWJjOWE3NmI2ZWJlMjAzZTVmZjQ1ZmQwZjJkZDAxNmNjMDhmYzgzMDg","altText":"120_0200000f00032f83000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000f00032f83000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-882","stock":null,"url":"/plcs-controllers/controller-ethernet/p/750-882","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["ec000236","fieldbus system","fieldbus components","io controller","fieldbus controller","distributed i/o","ip20","remote i/o","750-882","bus controller","wago io system","controller","programmable","codesys","fieldbus","plc","cpu","pfc","master","ethernet","27-24-26-07","head station","modbus","fieldbus technology","io system","gateway"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821174929","primaryCategoryName":"Controller","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":false,"status":"RELEASED","cancelDate":null,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["Controller"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":true,"purchasableFrom":null,"customerSpecific":false,"priceVisible":false,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Controller ETHERNET","primaryImageUrl":null,"productGroup":null,"nameEn":"Controller ETHERNET; 3rd Generation; Media Redundancy","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"7500882","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Controller 750","productColor":null,"downloadData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"videos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-843","name":"Controller ETHERNET; 1st Generation; ECO","url":"/plcs-controllers/controller-ethernet/p/750-843","description":null,"purchasable":true,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w1ODc2NTJ8aW1hZ2UvanBlZ3xhR0ZtTDJnMVppOHhOalUzT0RReE1EQTFNelkyTWd8MjkxYjE5MTYxMzYzZjk3ZjBkYmY4ZmVjZTk0YTE1ODVhYTkzYmEwMmU4ZDI0OTE0M2Q1Nzg5NWU4M2EwNjRkZA","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzg3OXxpbWFnZS9qcGVnfGFESXlMMmcxTWk4eE5qVTNPRFF4TURRME5qZzNPQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwWTJJd01EQXhNREJpTmw5RVJTNXFjR2N8YTE1NjM0ODAwODNhMGY5OWE3YjYyNDkyZmQ4OTRmOWU3NmFjMDk3OTRlNTQwYzc2MjNiY2Q3MDUxM2YwNGU0Mg","altText":"2000_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzg3OXxpbWFnZS9qcGVnfGFESXlMMmcxTWk4eE5qVTNPRFF4TURRME5qZzNPQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwWTJJd01EQXhNREJpTmw5RVJTNXFjR2N8YTE1NjM0ODAwODNhMGY5OWE3YjYyNDkyZmQ4OTRmOWU3NmFjMDk3OTRlNTQwYzc2MjNiY2Q3MDUxM2YwNGU0Mg","altText":"2000_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzg3OXxpbWFnZS9qcGVnfGFESXlMMmcxTWk4eE5qVTNPRFF4TURRME5qZzNPQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwWTJJd01EQXhNREJpTmw5RVJTNXFjR2N8YTE1NjM0ODAwODNhMGY5OWE3YjYyNDkyZmQ4OTRmOWU3NmFjMDk3OTRlNTQwYzc2MjNiY2Q3MDUxM2YwNGU0Mg","altText":"2000_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzg3OXxpbWFnZS9qcGVnfGFESXlMMmcxTWk4eE5qVTNPRFF4TURRME5qZzNPQzh5TURBd1h6QXlNREF3TURCak1EQXdNVEEwWTJJd01EQXhNREJpTmw5RVJTNXFjR2N8YTE1NjM0ODAwODNhMGY5OWE3YjYyNDkyZmQ4OTRmOWU3NmFjMDk3OTRlNTQwYzc2MjNiY2Q3MDUxM2YwNGU0Mg","altText":"2000_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzg3OXxpbWFnZS9qcGVnfGFHVTVMMmcwTnk4eE5qVTNPRFF4TURjME1UYzVNQzh4TkRRd1h6QXlNREF3TURCak1EQXdNVEEwWTJJd01EQXhNREJpTmw5RVJTNXFjR2N8MzkzMmFhMWIyZWQ4OTJiMmVjYmVkMDNkYTEwNTVlZDdkMTZjNGIxMTBjYzI0OTU2ZGUxMTZlYjMwMjgzYTk0Mg","altText":"1440_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w5Nzg3OXxpbWFnZS9qcGVnfGFEZ3pMMmcwTVM4eE5qVTNPRFF4TURrd05UWXpNQzh4TWpnd1h6QXlNREF3TURCak1EQXdNVEEwWTJJd01EQXhNREJpTmw5RVJTNXFjR2N8ODU4NjA4ZTNmMDYyNjk2NjM5NDZlY2Q4MDgwYjJiMWM1ZmI4MWJhNTY0NDIyYzU3MDk4M2RkNTU3YjE3MGI4MA","altText":"1280_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w3MTYxNnxpbWFnZS9qcGVnfGFEUm1MMmd3WkM4eE5qVTNPRFF4TVRFek5UQXdOaTh4TURJMFh6QXlNREF3TURCak1EQXdNVEEwWTJJd01EQXhNREJpTmw5RVJTNXFjR2N8MWExOWUyZjE4YzVmMmU4ZGY0NDJjMWQ1MTU5OWQ5M2RmMTJhMWRkMjc1MjBjMzA5ZGNlMThiZDk5NmI2MWNhNw","altText":"1024_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0Nzc5OXxpbWFnZS9qcGVnfGFEYzBMMmd4Tnk4eE5qVTNPRFF4TVRReU9Ua3hPQzgzTmpoZk1ESXdNREF3TUdNd01EQXhNRFJqWWpBd01ERXdNR0kyWDBSRkxtcHdad3w3NmE5NWMxNDU4ZTkwOWEyOWNjM2RhNWVkODZhMjZiNzQwMTRmNjRmNjJlOWYxOTA2ODE0Mjg1YTEyOGM0ZWJk","altText":"768_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyNDc3MnxpbWFnZS9qcGVnfGFHUmpMMmd4WVM4eE5qVTNPRFF4TVRVeU9ESXlNaTgwT0RCZk1ESXdNREF3TUdNd01EQXhNRFJqWWpBd01ERXdNR0kyWDBSRkxtcHdad3w2NWE5NzMwZWRiMmYxY2FiZWNjNDhiMmU0N2YxNzI0ZjJhZGNiZTg2MTIwYWFlNDczYjc4YjZiMWUwOWRjNDIz","altText":"480_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMTg0fGltYWdlL2pwZWd8YURBMkwyZ3haaTh4TmpVM09EUXhNVFk1TWpBMk1pOHlNREJmTURJd01EQXdNR013TURBeE1EUmpZakF3TURFd01HSTJYMFJGTG1wd1p3fDkwYjcyNzI0MmJlMzYyNjQ3ODBiODhkZjY2NWMzNzJkYzJjNzMyNWYzYWQ4NWRhYjk4ZTMzMTY1MDIyZGNkM2Q","altText":"200_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMTg0fGltYWdlL2pwZWd8YURBMkwyZ3haaTh4TmpVM09EUXhNVFk1TWpBMk1pOHlNREJmTURJd01EQXdNR013TURBeE1EUmpZakF3TURFd01HSTJYMFJGTG1wd1p3fDkwYjcyNzI0MmJlMzYyNjQ3ODBiODhkZjY2NWMzNzJkYzJjNzMyNWYzYWQ4NWRhYjk4ZTMzMTY1MDIyZGNkM2Q","altText":"200_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wyMTg0fGltYWdlL2pwZWd8YURBMkwyZ3haaTh4TmpVM09EUXhNVFk1TWpBMk1pOHlNREJmTURJd01EQXdNR013TURBeE1EUmpZakF3TURFd01HSTJYMFJGTG1wd1p3fDkwYjcyNzI0MmJlMzYyNjQ3ODBiODhkZjY2NWMzNzJkYzJjNzMyNWYzYWQ4NWRhYjk4ZTMzMTY1MDIyZGNkM2Q","altText":"200_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200000c000104cb000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200000c000104cb000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMjY1fGltYWdlL2pwZWd8YURVd0wyZzNOeTh4TmpVM09EUXhNakUxTURneE5DOHhNakJmTURJd01EQXdNR013TURBeE1EUmpZakF3TURFd01HSTJYMFJGTG1wd1p3fGM4NmFmN2FhMDdhZDlkODA2YjJiZmE1ZTg1YTZlYTg3NWQzNjUzMTFlNDYyMGQzZjA2YzVkMDk2NjI3NjgyOGI","altText":"120_0200000c000104cb000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200000c000104cb000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-843","stock":null,"url":"/plcs-controllers/controller-ethernet/p/750-843","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["ec000236","fieldbus system","fieldbus components","io controller","fieldbus controller","distributed i/o","ip20","remote i/o","bus controller","wago io system","750-843","controller","programmable","codesys","fieldbus","plc","cpu","pfc","master","ethernet","27-24-26-07","head station","modbus","fieldbus technology","gateway","io system"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4045454897888","primaryCategoryName":"Controller","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":false,"status":"RELEASED","cancelDate":null,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["Controller"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":false,"purchasableFrom":null,"customerSpecific":false,"priceVisible":true,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Controller ETHERNET","primaryImageUrl":null,"productGroup":null,"nameEn":"Controller ETHERNET; 1st Generation; ECO","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"7500843","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Controller 750","productColor":null,"downloadData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"videos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false},{"code":"750-885","name":"Controller ETHERNET; 3rd Generation; SD Card Slot; Media Redundancy","url":"/plcs-controllers/controller-ethernet/p/750-885","description":null,"purchasable":false,"stock":null,"futureStocks":null,"availableForPickup":null,"averageRating":null,"numberOfReviews":null,"summary":null,"manufacturer":null,"variantType":null,"price":null,"baseProduct":null,"images":[{"imageType":"PRIMARY","format":"fallback","url":"/medias/?context=bWFzdGVyfGltYWdlc3w4OTQyNDl8aW1hZ2UvanBlZ3xhRGt6TDJoaE5pOHhOalUyTWpnMU9UTTBNemt3TWd8MDUzOTdlMjc0YjczNjE2OGI3OGVhYTc0NmE0ZjBjNzkzODI2M2EzYTlmOWFmNjc0MGQyMWQ5MmUyNGEwN2QwMA","altText":"","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"2000","url":"/medias/2000-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDcxNDZ8aW1hZ2UvanBlZ3xhR1V3TDJoaU55OHhOalUyTWpnMU9UZzJPREU1TUM4eU1EQXdYekF5TURBd01ERTJNREF3TVRGaFltRXdNREF4TURCaU5sOUVSUzVxY0djfGU2YjRkZTY3MTdiZThjMzBiZGNjOTI1MTZjMzAzMmRkMzk3MTljODQ3ODRiZTU2Mjk4YzNmMzk4M2RjYTU2M2E","altText":"2000_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"superZoom","url":"/medias/2000-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDcxNDZ8aW1hZ2UvanBlZ3xhR1V3TDJoaU55OHhOalUyTWpnMU9UZzJPREU1TUM4eU1EQXdYekF5TURBd01ERTJNREF3TVRGaFltRXdNREF4TURCaU5sOUVSUzVxY0djfGU2YjRkZTY3MTdiZThjMzBiZGNjOTI1MTZjMzAzMmRkMzk3MTljODQ3ODRiZTU2Mjk4YzNmMzk4M2RjYTU2M2E","altText":"2000_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"zoom","url":"/medias/2000-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDcxNDZ8aW1hZ2UvanBlZ3xhR1V3TDJoaU55OHhOalUyTWpnMU9UZzJPREU1TUM4eU1EQXdYekF5TURBd01ERTJNREF3TVRGaFltRXdNREF4TURCaU5sOUVSUzVxY0djfGU2YjRkZTY3MTdiZThjMzBiZGNjOTI1MTZjMzAzMmRkMzk3MTljODQ3ODRiZTU2Mjk4YzNmMzk4M2RjYTU2M2E","altText":"2000_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"product","url":"/medias/2000-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDcxNDZ8aW1hZ2UvanBlZ3xhR1V3TDJoaU55OHhOalUyTWpnMU9UZzJPREU1TUM4eU1EQXdYekF5TURBd01ERTJNREF3TVRGaFltRXdNREF4TURCaU5sOUVSUzVxY0djfGU2YjRkZTY3MTdiZThjMzBiZGNjOTI1MTZjMzAzMmRkMzk3MTljODQ3ODRiZTU2Mjk4YzNmMzk4M2RjYTU2M2E","altText":"2000_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"2000_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1440","url":"/medias/1440-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDcxNDZ8aW1hZ2UvanBlZ3xhREZtTDJnME9DOHhOalUyTWpnMk1ERTVOVGczTUM4eE5EUXdYekF5TURBd01ERTJNREF3TVRGaFltRXdNREF4TURCaU5sOUVSUzVxY0djfGY0MDc1ZDk0ZDQzYmJiMDczNDVhY2Y2ZDJhNTQ5ZTgxMmEwZTIwZTlhM2RlZTZiZDgxY2UyMGY5NjcwNDVmNjE","altText":"1440_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1440_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1280","url":"/medias/1280-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxNDcxNDZ8aW1hZ2UvanBlZ3xhRFV3TDJnelpTOHhOalUyTWpnMk1EUTFPREF4TkM4eE1qZ3dYekF5TURBd01ERTJNREF3TVRGaFltRXdNREF4TURCaU5sOUVSUzVxY0djfDM1Y2ZlYTdkMmZhN2RmNTViMDEyZGQ3YTExNDIwZDMzYWQxODYxMTNhZTNiNjA0NTNhYzZmMjZkODJlY2IxZTk","altText":"1280_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1280_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"1024","url":"/medias/1024-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wxMDkwNjF8aW1hZ2UvanBlZ3xhRFpsTDJnek5DOHhOalUyTWpnMk1EY3lNREUxT0M4eE1ESTBYekF5TURBd01ERTJNREF3TVRGaFltRXdNREF4TURCaU5sOUVSUzVxY0djfGU1NTUwM2YwNWY3NDJhYmUxYWU5NzYyOTZhYzM4Mzk3MmRkYzk5MjJmYjczYmM0Y2MyYmFmMWFlNjA0M2FkMDU","altText":"1024_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"1024_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"768","url":"/medias/768-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w3MzkwM3xpbWFnZS9qcGVnfGFEVmhMMmd5WkM4eE5qVTJNamcyTURrME9UVXpOQzgzTmpoZk1ESXdNREF3TVRZd01EQXhNV0ZpWVRBd01ERXdNR0kyWDBSRkxtcHdad3xhZmNhZGQwYTI3MGI0MDQ5ZmI5ZTZkMzNhZjIzM2EyZDM4MDg0MzFmNGYwNDI2MGVkYzRmZDAzZGQ1YWY3MmFl","altText":"768_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"768_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"480","url":"/medias/480-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzODcwN3xpbWFnZS9qcGVnfGFESXlMMmd4WlM4eE5qVTJNamcyTVRBNE1EWXdOaTgwT0RCZk1ESXdNREF3TVRZd01EQXhNV0ZpWVRBd01ERXdNR0kyWDBSRkxtcHdad3w4YjYxNjI2NjZjNDk4M2U0MjA5N2VlM2JhOGJiMTYzNDI3YzUwNGVlYWRlYTliZTQwNmQzYTNmNWRiZjhlMmFi","altText":"480_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"480_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"200","url":"/medias/200-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTE1fGltYWdlL2pwZWd8YURnMkwyZ3lOeTh4TmpVMk1qZzJNVE13T1RrNE1pOHlNREJmTURJd01EQXdNVFl3TURBeE1XRmlZVEF3TURFd01HSTJYMFJGTG1wd1p3fGJkZDU4MDYwZTBhNzU1NzNkMjI2NTQ3ZjQ0NWYyYmM0MWFiZGE5NGY0ZDExMTYyMjZhZmQ1Y2JhZTVhODg3ODU","altText":"200_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"thumbnail","url":"/medias/200-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTE1fGltYWdlL2pwZWd8YURnMkwyZ3lOeTh4TmpVMk1qZzJNVE13T1RrNE1pOHlNREJmTURJd01EQXdNVFl3TURBeE1XRmlZVEF3TURFd01HSTJYMFJGTG1wd1p3fGJkZDU4MDYwZTBhNzU1NzNkMjI2NTQ3ZjQ0NWYyYmM0MWFiZGE5NGY0ZDExMTYyMjZhZmQ1Y2JhZTVhODg3ODU","altText":"200_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"cartIcon","url":"/medias/200-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3wzMTE1fGltYWdlL2pwZWd8YURnMkwyZ3lOeTh4TmpVMk1qZzJNVE13T1RrNE1pOHlNREJmTURJd01EQXdNVFl3TURBeE1XRmlZVEF3TURFd01HSTJYMFJGTG1wd1p3fGJkZDU4MDYwZTBhNzU1NzNkMjI2NTQ3ZjQ0NWYyYmM0MWFiZGE5NGY0ZDExMTYyMjZhZmQ1Y2JhZTVhODg3ODU","altText":"200_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"200_0200001600011aba000100b6_DE.jpg"},{"imageType":"PRIMARY","format":"120","url":"/medias/120-0200001600011aba000100b6-DE.jpg?context=bWFzdGVyfGltYWdlc3w0Nzk4fGltYWdlL2pwZWd8YURobUwyZ3pPQzh4TmpVMk1qZzJNVGd3TVRVd01pOHhNakJmTURJd01EQXdNVFl3TURBeE1XRmlZVEF3TURFd01HSTJYMFJGTG1wd1p3fDMzOTg3ZmY3OGQ1OWRkNjA1ZTg1NmQ4MTMyZjcwMTJhNzRhMTIzNjk4OWE3Yzg3OGMyYzVjMmQ5ZmQ2YTAzZTM","altText":"120_0200001600011aba000100b6_DE","galleryIndex":null,"width":null,"description":null,"mediaType":null,"code":"120_0200001600011aba000100b6_DE.jpg"}],"categories":null,"reviews":null,"classifications":null,"potentialPromotions":null,"variantOptions":null,"baseOptions":[{"variantType":"GenericVariantProduct","options":null,"selected":{"code":"750-885","stock":null,"url":"/plcs-controllers/controller-ethernet/p/750-885","priceData":null,"variantOptionQualifiers":null}}],"volumePricesFlag":null,"volumePrices":null,"productReferences":null,"variantMatrix":null,"priceRange":null,"firstCategoryNameList":null,"multidimensional":null,"configurable":false,"configuratorType":null,"addToCartDisabled":null,"addToCartDisabledMessage":null,"tags":null,"sapUnit":null,"keywords":["ec000236","fieldbus system","fieldbus components","io controller","fieldbus controller","distributed i/o","ip20","remote i/o","bus controller","750-885","wago io system","controller","programmable","codesys","fieldbus","plc","cpu","pfc","master","ethernet","27-24-26-07","head station","modbus","fieldbus technology","io system","gateway"],"dataType":null,"resultType":null,"productReferencesSearchUrl":null,"customsNumber":null,"availableFrom":null,"homeCountry":null,"ean":"4050821572206","primaryCategoryName":"Controller","numberContentUnits":null,"numberPackageUnits":null,"unit":null,"edelmetall":null,"netPrice":null,"positionValue":null,"contentUnit":null,"downloads":null,"cancelled":false,"status":"RELEASED","cancelDate":null,"announced":false,"infoText":null,"containsDownloads":true,"categoryNames":["Controller"],"variantLevels":null,"listPrice":null,"productAvailability":null,"categoryClassifications":null,"infoArticle":true,"purchasableFrom":null,"customerSpecific":false,"priceVisible":false,"cadenasCAD":true,"ultralibrarianCAD":false,"published":true,"customsCode":null,"wholesalerNumber":null,"approvals":null,"familyCategory":null,"familyName":null,"descriptionMetadataPattern":null,"titleMetadataPattern":null,"shortName":"Controller ETHERNET","primaryImageUrl":null,"productGroup":null,"nameEn":"Controller ETHERNET; 3rd Generation; SD Card Slot; Media Redundancy","useableInProductConfigurator":true,"compilantToRoHS":true,"materialId":"7500885","stockArticle":false,"customerArticleNumbers":null,"maxOrderQuantity":null,"currentOrderedQuantity":null,"cartContentQuantity":null,"hasCounterparts":false,"counterpartMainFunction":null,"mainFunction":"Controller 750","productColor":null,"downloadData":null,"hideGenerateDatasheetAsPdf":false,"sampleProduct":false,"hasFollowUpProduct":false,"newProduct":false,"representativePicture":false,"videos":[],"uuid":null,"productFilterCategories":null,"variantData":null,"taxes":null,"matrixValues":null,"safetyAdvice":null,"safetyAdviceDownloadUrl":null,"thermosimulation":false,"hideWhereToBuy":false}]