Customer Application

Control Cabinet Manufacturing at Ford Using WAGO Terminal Blocks

With the introduction of the assembly line, Henry Ford left an indelible mark and it made him one of the most important pioneers in the automotive industry. The ambition of his company has always been to improve the production process. At their production facility in Cologne, Germany, they rebuilt their entire press line that manufactures chassis parts for the Ford Fiesta. One of the stars in this overhaul: WAGO’s rail-mount terminal block.

Nearly 19,000 employees help produce one of Ford’s most successful compact car models. Since 1976, up to 1,400 Ford Fiestas roll off the assembly line on a daily basis. Ford utilizes big equipment in their production facilities, but sometimes it’s the small details that really matter. For instance, the large punching machines and presses used to produce chassis components have a lifespan of several decades. However, many of the internal components and systems in the press line do not last near that long. To help this, Ford regularly installs new assemblies, updates the electronics and expands safety technology in their press lines. During this process that control and automation technology along with energy distribution within control cabinets are also updated and optimized.

Your Benefits with the WAGO smartDESIGNER:

  • No installation

  • Runs exclusively on cloud server (no updating)

  • Accessible anywhere

  • Create custom assemblies with WAGO products

  • Customizable parts libraries for common components

  • Add custom labels that can be sent directly to WAGO's smartPRINTER



Product Highlights

TOPJOB®S feedthrough terminal block with Lever and Push-buttons; rail mount; 3-conductor; 5.2 mm wide; gray
Item no. 2102-5301

TOPJOB®S feedthrough terminal block with Lever and Push-buttons; rail mount; 3-conductor; 5.2 mm wide; gray

TOPJOB®S feedthrough terminal block with Lever and Open Tool Slots; rail mount; 3-conductor; 5.2 mm wide; gray
Item no. 2102-1301

TOPJOB®S feedthrough terminal block with Lever and Open Tool Slots; rail mount; 3-conductor; 5.2 mm wide; gray

TOPJOB®S feedthrough terminal block with Lever and Open Tool Slots; rail mount; 3-conductor; 7.5 mm wide; gray
Item no. 2106-1301

TOPJOB®S feedthrough terminal block with Lever and Open Tool Slots; rail mount; 3-conductor; 7.5 mm wide; gray

TOPJOB®S feedthrough terminal block with Push-buttons; rail mount; 2-conductor; 3.5 mm wide; gray
Item no. 2200-1201

TOPJOB®S feedthrough terminal block with Push-buttons; rail mount; 2-conductor; 3.5 mm wide; gray

TOPJOB®S feedthrough terminal block with Lever and Push-button; rail mount; 2-conductor; 5.2 mm wide; gray
Item no. 2102-5201

TOPJOB®S feedthrough terminal block with Lever and Push-button; rail mount; 2-conductor; 5.2 mm wide; gray

TOPJOB®S feedthrough terminal block with Lever and Open Tool Slot; rail mount; 2-conductor; 5.2 mm wide; gray
Item no. 2102-1201

TOPJOB®S feedthrough terminal block with Lever and Open Tool Slot; rail mount; 2-conductor; 5.2 mm wide; gray

The Story

Picture1

A Service Provider within the Company

The grounds of the Ford plant also house the in-house equipment production department. In this department, about 180 employees carry out conversion and retrofitting projects for various equipment in the production plant. The main focus is on control cabinet manufacturing. This department normally covers the entire spectrum, from electrical planning and design, to the mechanical structure and wiring, to programming and commissioning. The orders for in-house equipment production come primarily from the two German Ford plants in Cologne and Saarlouis. But the other European plants have also already implemented projects that have to hold their own against external competition.

Picture2

Project-Based Conversion to Standardized Terminal Block Technology

The various internal customers within the Ford Group sometimes set very different requirements for their projects. This also applies to components for use in control cabinets, for example. As a result, in the past, different terminals blocks from different suppliers were often used in the control cabinets. Two years ago, during the conversion of a press line in the Cologne plant, the idea arose for the first time to standardize terminal blocks by switching to exclusively using WAGO rail-mount terminal blocks for the conversion of the press line. Agreeing on a uniform project-based system leads to enormous advantages for logistics, purchasing and spare parts procurement.

For the people involved at Ford, the choice for WAGO’s rail-mount terminals blocks was based on financial and – above all – technical considerations. The project-specific concentration on one terminal block system reduces warehouse volumes and provides predictability for all employees involved in the planning and production process. WAGO’s innovative push-in CAGE CLAMP® connection technology offers the end customers superior contact quality, even – and especially – under extreme conditions. One of the greatest technical advantages of WAGO’s rail-mount terminals blocks is the push-in connection technology. Not only does it make the wiring quicker than the old terminals blocks using screw technology – the fact that the terminal blocks are maintenance-free is also a great advantage, since screw connections need to be retightened at regular intervals. With WAGO terminals blocks, this work is unnecessary. And this saves significant time on maintenance. Furthermore, faults occur less often. The large presses experience very significant vibrations. This creates a risk of screw connections coming loose. Therefore, two years ago the maintenance department advocated for switching over to WAGO rail-mount terminal blocks, which at that time were already listed as the plant standard, in the conversion of the press line as well.

picture3

Easy Wiring and Clear Marking

Not only does the push-in connection technology of WAGO’s TOPJOB® S Rail-Mount Terminal Blocks make them maintenance-free – the electrical department staff is also able to trim wiring time by nearly 25%. Conductors with crimped ferrules are easy to insert, making wiring very quick and easy compared to screw-type terminal blocks. The marking method also saves time: Standardized marking strips exist for all terminal block sizes, which the Ford employees can print quickly and easily with one of the two printers that were purchased for this purpose. WAGO Smart Printers are controlled online, allowing the markings that are created to be stored and reused in later projects. The marking strips offer plenty of space for clear labeling of connection points. This too saves wiring time, since employees can find the right connection point more quickly. And the clear marking makes maintenance much easier too whenever faults need to be eliminated. Besides the rail-mount terminal blocks, the Smart Printer can also be used to mark conductors with marking sleeves or thread-on wire markers, making it an incredibly versatile solution.

Picture4

The Right Terminal Block for Every Application

The control cabinets built by the in-house equipment production department mostly use TOPJOB® S Rail-Mount Terminal Blocks. They are used to connect a wide variety of signals from sensors and actuators. Ford limits itself to three or four series of rail-mount terminals blocks. That works very well, especially since the terminal blocks accommodate a very wide range of possible conductor sizes. The power distribution with large conductors is connected via high-current rail-mount terminal blocks equipped with POWER CAGE CLAMP. The experts at Ford use WAGO’s terminal blocks for other requirements as well. Recording power consumption has become an important part of many projects. For this purpose, Ford uses current converters and 3-Phase Power Measurement Modules, as well as function modules from WAGO’s 750 Series automation portfolio.

During the recent factory-wide vacation, another press line was also converted – based on past success, the control cabinet was again equipped with WAGO rail-mount terminal blocks. Using the standardized rail-mount terminals blocks for press line conversion projects has since become routine. However, during conversion, it was important for the in-house equipment production unit that WAGO support was always reachable to help Ford’s team get is bearings in a broad product portfolio. The tight integration between the Ford Key Account at WAGO, WAGO’s local sales office and industrial system advisors enabled short response times.

Text: Lena Kalmer | WAGO Photo: Ford