Automation at All Levels

Decentralized Infrastructure Automation

Companies are focusing on decentralized infrastructure automation more and more. When monitoring system systems – whether distributed production facilities, power grids, transport systems or energy systems – remote signals can be recorded in a wide variety of applications and integrated into an IT infrastructure. One example: recording data in waterworks.

MM-459201_GWA_Reference-Netilion-Endress-Hauser_02_2000x1125.jpg

Recording Data in Waterworks

The data is often widely distributed, and certain areas lack reception. Highly qualified employees often spend hours driving just to read out simple measured values, such as levels and volume flows, and record them in government-mandated reports. In a joint project with Endress + Hauser and the Oberzent water supply system, LoRaWAN has provided the communication, thus allowing automated data collection. With the flexible gateway of the WAGO IoT Box, recorded signals can be passed on to an IT infrastructure.

Automation at the Company Site

The infrastructure automation at the company’s site has many different parts and covers many different areas. Discover our solutions for automation in the following domains:

Automation in the Factory

MM-454394_GW_Infrastructure-Automation_02_2000x1125.jpg

Whether in production, logistics or storage – the future of the digital factory is automated! By thinking about the future now, companies can fully exploit the potential of automation.

The possibilities range from improving quality, to saving time and money, to conserving resources for people, machines and the environment.

Automation at the Machine

MM-454394_GW_Infrastructure-Automation_03_2000x1125.jpg

Many factors play a role in production optimization. The first step involves keeping an eye on the current machine status at all times. To perform an analysis for machine optimization, it is also necessary to link to the IT system and use it to provide current information from different user groups.

This is where the WAGO PFC200 comes in: With a wide variety of interfaces on the OT and IT levels, the WAGO PFC200 connects the two worlds. On the OT level, different I/O modules are available on the hardware side for the signal connection to the system. Additional advantages include a compact design and scalability. This allows individual, system-specific, cost-effective hardware data acquisition. As a retrofit solution, it is easy to expand at any later time. The CODESYS programming environment per IEC 61131-3, allows system functions to be programmed specifically so optimization measures can be added to the logic at the system level.

Your WAGO Contact

kontaktmodul_kundenservice_zentrale_300x300_1

Main Office

Monday -Thursday 8:45 am – 5pm Friday: 8:45 am – 4pm

Additional service offerings: