Alter Wall: Automation that Allows Future Expansion
It is the longest historical facade in Hamburg and is being thoroughly renovated and equipped with modern technology. Directly across from the Rathaus, a completely new world is coming into being at the “Alter Wall” (originally part of the old city fortifications). At one time, it formed the imaginary boundary dividing the historical city center from the new districts, which can be seen in the form of the Alsterfleet canal. While the retailers at the Neuer Wall shopping street (the “new fortification”)belong to the exclusive luxury market, the historical city center from Mönckebergstraße to Spitalerstraße offers a diversity of market experiences. But the Alter Wall complex reduces the importance of this boundary – thanks in no small part to a new bridge over the Alsterfleet canal. A lively boulevard filled with upscale retailers, exclusive office properties and fine restaurants: this was the goal pursued by Art-Invest Real Estate, the project developer and investment company. The company, headquartered in Cologne, regularly invests in well-situated commercial properties in Germany’s largest cities. Among them, the “Alter Wall” renovation project stands out due to the technical migration.
Large-Scale Project: “Alter Wall”
The WAGO I/O System 750 coordinates the technology of the office areas and shopping mall.
52 system distributors and 54 WAGO controllers are used in electrical sub-distribution boards for the individual office areas.
In the office areas, 40 additional ETHERNET controllers provide lighting control and automated sun shading based on weather conditions.
Local operation is enabled by touch panels.
On the roof, four weather stations based on WAGO flexROOM® Weather measure the weather conditions to support efficient building operation.