Product FAQ

On the following pages you will find information on the most frequently asked questions. If the question you are looking for is not listed - please contact us by phone or leave your question in the form at the bottom of the page.

According to VDE 0141:2000-01, section 5.3.4, current and voltage transformers must be grounded on the secondary side for nominal voltages of Um 3.6 kV and above. For low voltage up to Um 1.2 kV, grounding can be omitted if the transformer housing does not have any metal surfaces that can be touched over a large area.

Further Technical Information" data-tracking-click='{"category": "faq-item", "label": "Do current transformers need to be grounded on the secondary side?"}' >
Single-phase power supplies are used, for example, in decentralized automation if three phases are not available. In Asia, entire control cabinets are powered by single-phase supplies even at high power.

As a general rule, yes – but please note that the inherent stability of a single-pole PCB terminal block is less than that of a multi-pole terminal strip. Therefore, be sure to protect single-pole terminal blocks against excessive mechanical stress, such as torsional or bending stress, both when connecting the conductor and during subsequent use. For example, use additional supports, ensure short bracing of the connected conductor, and note the corresponding handling instructions for actuation.

Unlike the TOPJOB® S Through Terminal Block, a reduction to smaller cross-sections is not possible with the 2016 Series Supply Terminal Blocks for Distribution Boxes such as the 2016-7601. The jumper slots of the supply terminal blocks for distribution boxes are not located on the same plane as with the TOPJOB® S Through Terminal Blocks, nor can the jumper slots be arranged in a plane by rotating the individual rail-mount terminal blocks.

For a reduction to smaller cross-sections, please use the corresponding 2016 Series Through Terminal Block and the 2016-499 Step-Down Jumper.

According to IEC 60947-7-1, the short-time withstand current simulates a thermal shock. However, there is no information on the pulse dynamics, i.e., how to test this. Therefore, the short-time withstand current indicated must not be considered the dynamic short circuit withstand capacity. For a dynamic short circuit situation, the applicable international standards describe neither requirements profiles nor test procedures.

The short-time withstand current value is determined from a current load of 120 A per wire cross-section, which is applied for one second, once to the clamping unit of the through terminal blocks, and three times to the clamping unit of the ground conductor terminal block. Typical short-time withstand currents for rail-mount terminal blocks according to IEC 60947-7-1 and 60947-7-2 are:

1.5 mm² – 180 A
2.5 mm² – 300 A
4 mm² – 480 A
6 mm² – 720 A
10 mm² – 1,200 A
16 mm² – 1,920 A
25 mm² – 3,000 A
35 mm² – 4,200 A
50 mm² – 6,000 A
70 mm² – 8,400 A
95 mm² – 11,400 A
120 mm² – 14,400 A
150 mm² – 18,000 A
185 mm² – 22,200 A
240 mm² – 28,800 A
300 mm² – 36,000 A

Screwless connection points use clamping springs as compensating elements. Tin-plating conductors is an ideal pre-treatment for conductors in terms of voltage drop constancy and uniformity of the contact surfaces. However, this only applies to stationary installations. Full tin-plating of conductors is generally not permissible for use in equipment with vibrations, such as engines. Tin-plating is only permissible for the tip of a stranded wire as a measure to protect the splice. This has no negative effect on the contact quality or voltage drop.

For use of tin-plated conductor ends in screwless clamp connections, please note the applicable standards: DIN EN 60999-1:2000, Section 7.1, as well asDIN EN 60335-1:2001, Section 23.9. The relevant passages place limits on connectors with screw-type clamping units, but not on connectors with screwless clamping units. DIN EN 60335-1, Section 23.9, explicitly mentions spring clamps as a solution in Note 1.

Different color variants of our rail-mount terminal blocks are available according to their cross-sections. Colored through terminal blocks can be used for all insulated protective ground connections, with the exception of the colors blue and green/yellow. According to IEC 60947-7-2, the green/yellow color combination is only intended for partially insulated ground conductor rail-mounted terminal blocks with a connection to the DIN-rail.

Because of the discontinuation of our 775 to 777 Series Classic Multilevel Installation Terminal Blocks, our customers are now reverting to using the 2003 and 2005 Series TOPJOB® S Multilevel Installation Terminal Blocks. In existing distribution boxes equipped with 10 x 3 mm N-busbars, expansion with the TOPJOB® S Multilevel Installation Terminal Blocks is possible using N-disconnect slide links. The position of the N-busbar for the Classic busbar carrier (777-305) is identical to the TOPJOB® S busbar carrier (2009-305).

However, when expanding an existing distribution box, note that the Classic and TOPJOB® S accessories are incompatible. Connecting the two rail-mount terminal block series – for example, commoming the phase – is not possible.

Our 206 Series Variocrimp Crimping Tool ensures a proper, reproducible, gas-tight square or “WM” format crimp from 0.25 mm² to 50 mm²